<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic imx6sx emmc mode in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6sx-emmc-mode/m-p/1067561#M156863</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;as far as i understand, imx6sx can reach a HS200 mode (controller spec 4.5 max, so no HS400).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Btw, the ref. manual (68.1.1, Rev. 3, 06/2018) is saying:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Card bus clock frequency up to 208 MHz&lt;/P&gt;&lt;P&gt;- Up to 832 Mbps of data transfer for MMC cards using 8 parallel &lt;STRONG&gt;data lines in&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;DDR(Dual Data Rate)&lt;/STRONG&gt; mode&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am miss somthing here, 200Mhz DDR means HS.400.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, 832Mbps seems a max bandwidth of 100Mhz ddr, or, 200 SDR.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any clarification is welcome.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 Jun 2020 07:44:10 GMT</pubDate>
    <dc:creator>angelo_d</dc:creator>
    <dc:date>2020-06-08T07:44:10Z</dc:date>
    <item>
      <title>imx6sx emmc mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6sx-emmc-mode/m-p/1067561#M156863</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;as far as i understand, imx6sx can reach a HS200 mode (controller spec 4.5 max, so no HS400).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Btw, the ref. manual (68.1.1, Rev. 3, 06/2018) is saying:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Card bus clock frequency up to 208 MHz&lt;/P&gt;&lt;P&gt;- Up to 832 Mbps of data transfer for MMC cards using 8 parallel &lt;STRONG&gt;data lines in&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;DDR(Dual Data Rate)&lt;/STRONG&gt; mode&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am miss somthing here, 200Mhz DDR means HS.400.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, 832Mbps seems a max bandwidth of 100Mhz ddr, or, 200 SDR.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any clarification is welcome.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jun 2020 07:44:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6sx-emmc-mode/m-p/1067561#M156863</guid>
      <dc:creator>angelo_d</dc:creator>
      <dc:date>2020-06-08T07:44:10Z</dc:date>
    </item>
  </channel>
</rss>