<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: How to use VPU to encode/decode on imx8qxp (linux)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-VPU-to-encode-decode-on-imx8qxp-linux/m-p/1066107#M156666</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks a lot for your response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How to make sure it is using hw-codec and not the sw-codec?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Wasim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Jul 2020 09:54:31 GMT</pubDate>
    <dc:creator>wasim_nazir</dc:creator>
    <dc:date>2020-07-07T09:54:31Z</dc:date>
    <item>
      <title>How to use VPU to encode/decode on imx8qxp (linux)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-VPU-to-encode-decode-on-imx8qxp-linux/m-p/1066104#M156663</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am currently using&amp;nbsp;imx-L4.14.98_2.3.0 linux yocto build on imx8qxp-B0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to create one application to encode/decode h264.&lt;/P&gt;&lt;P&gt;Is there any user-guide to implement enc-dec on Amphion VPU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am following this doc(&lt;A class="link-titled" href="https://www.nxp.com/docs/en/reference-manual/IMX_VPU_APPLICATION_PROGRAMMING_INTERFACE_LINUX_REFERENCE_MANUAL.pdf" title="https://www.nxp.com/docs/en/reference-manual/IMX_VPU_APPLICATION_PROGRAMMING_INTERFACE_LINUX_REFERENCE_MANUAL.pdf"&gt;https://www.nxp.com/docs/en/reference-manual/IMX_VPU_APPLICATION_PROGRAMMING_INTERFACE_LINUX_REFERENCE_MANUAL.pdf&lt;/A&gt;&amp;nbsp;), which shows way for programming based on RPC but doesn't seems complete.&lt;/P&gt;&lt;P&gt;I have also found end/dec test applications here(&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/imx-test" title="https://source.codeaurora.org/external/imx/imx-test"&gt;imx-test - i.MX Driver Test Application Software&lt;/A&gt;&amp;nbsp;)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any other proper doc or sample code to follow, to implement the same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in Advance,&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Wasim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 05 Jul 2020 16:16:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-use-VPU-to-encode-decode-on-imx8qxp-linux/m-p/1066104#M156663</guid>
      <dc:creator>wasim_nazir</dc:creator>
      <dc:date>2020-07-05T16:16:05Z</dc:date>
    </item>
    <item>
      <title>Re: How to use VPU to encode/decode on imx8qxp (linux)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-VPU-to-encode-decode-on-imx8qxp-linux/m-p/1066105#M156664</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Wasim&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am afraid such nxp publicly available documentation is not available yet,&lt;/P&gt;&lt;P&gt;one can look at third party resources:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://variwiki.com/index.php?title=MX8_GSTREAMER&amp;amp;release=RELEASE_SUMO_V1.1_VAR-SOM-MX8" title="http://variwiki.com/index.php?title=MX8_GSTREAMER&amp;amp;release=RELEASE_SUMO_V1.1_VAR-SOM-MX8"&gt;MX8 GSTREAMER - Variscite Wiki&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://developer.ridgerun.com/wiki/index.php?title=GStreamer_Based_Image_Signal_Processor/Examples/IMX8_Pipelines" title="https://developer.ridgerun.com/wiki/index.php?title=GStreamer_Based_Image_Signal_Processor/Examples/IMX8_Pipelines"&gt;GStreamer Based Image Signal Processor - IMX8 Pipelines&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 05 Jul 2020 23:18:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-use-VPU-to-encode-decode-on-imx8qxp-linux/m-p/1066105#M156664</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-07-05T23:18:56Z</dc:date>
    </item>
    <item>
      <title>Re: How to use VPU to encode/decode on imx8qxp (linux)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-VPU-to-encode-decode-on-imx8qxp-linux/m-p/1066106#M156665</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Wasim,&lt;/P&gt;&lt;P&gt;on 8QM we are using the NXP's gst v4l2decoder to decode H264 frames using the VPU. That's working fine.&lt;/P&gt;&lt;P&gt;The missing part is the display of the decoded Amphion tiled format, that's not included in the gstreamer provided with BSP 4.14.98&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Francesco&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Jul 2020 09:40:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-use-VPU-to-encode-decode-on-imx8qxp-linux/m-p/1066106#M156665</guid>
      <dc:creator>fmonte</dc:creator>
      <dc:date>2020-07-06T09:40:03Z</dc:date>
    </item>
    <item>
      <title>Re: How to use VPU to encode/decode on imx8qxp (linux)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-VPU-to-encode-decode-on-imx8qxp-linux/m-p/1066107#M156666</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks a lot for your response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How to make sure it is using hw-codec and not the sw-codec?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Wasim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jul 2020 09:54:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-use-VPU-to-encode-decode-on-imx8qxp-linux/m-p/1066107#M156666</guid>
      <dc:creator>wasim_nazir</dc:creator>
      <dc:date>2020-07-07T09:54:31Z</dc:date>
    </item>
    <item>
      <title>Re: How to use VPU to encode/decode on imx8qxp (linux)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-VPU-to-encode-decode-on-imx8qxp-linux/m-p/1066108#M156667</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If using HW decoding, in dmesg you will find messages stating that the VPU is opened, the buffers allocated etc.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jul 2020 08:58:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-use-VPU-to-encode-decode-on-imx8qxp-linux/m-p/1066108#M156667</guid>
      <dc:creator>fmonte</dc:creator>
      <dc:date>2020-07-16T08:58:46Z</dc:date>
    </item>
  </channel>
</rss>