<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX8MM EVK Type C connector</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-EVK-Type-C-connector/m-p/1065337#M156570</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="direction: ltr;"&gt;Hi,&lt;/P&gt;&lt;P style="direction: ltr;"&gt;&lt;/P&gt;&lt;P style="direction: ltr;"&gt;any ideas?&lt;/P&gt;&lt;P style="direction: ltr;"&gt;&lt;/P&gt;&lt;P style="direction: ltr;"&gt;Thanks,&lt;/P&gt;&lt;P style="direction: ltr;"&gt;Dudi.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 May 2020 13:42:40 GMT</pubDate>
    <dc:creator>dudisasson</dc:creator>
    <dc:date>2020-05-05T13:42:40Z</dc:date>
    <item>
      <title>IMX8MM EVK Type C connector</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-EVK-Type-C-connector/m-p/1065334#M156567</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="direction: ltr;"&gt;Hi,&lt;/P&gt;&lt;P style="direction: ltr;"&gt;&lt;/P&gt;&lt;P style="direction: ltr;"&gt;i am designing a new Base&amp;nbsp;board&amp;nbsp;for the the som. i plan to connect a UVC camera directly to the USB1,&amp;nbsp; which has a Type C connector, but without the connector.&amp;nbsp;&lt;/P&gt;&lt;P style="direction: ltr;"&gt;i tried connecting only DP, DN, GND and 5V for the camera from an external power supply but the it didn`t reocgnized the device.&lt;/P&gt;&lt;P style="direction: ltr;"&gt;i guess it is because the USB is listed in the device tree as Type C, using the&amp;nbsp;&lt;SPAN style="color: #24292e; background-color: #ffffff;"&gt;ptn5110 componet.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="direction: ltr;"&gt;&lt;SPAN style="color: #24292e; background-color: #ffffff;"&gt;how can i change it to a regular usb connection? what do i need to change in the device tree or is there a way to change it from the terminal?&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="direction: ltr;"&gt;&lt;/P&gt;&lt;P style="direction: ltr;"&gt;&lt;SPAN style="color: #24292e; background-color: #ffffff;"&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="direction: ltr;"&gt;&lt;SPAN style="color: #24292e; background-color: #ffffff;"&gt;Dudi.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Apr 2020 22:30:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-EVK-Type-C-connector/m-p/1065334#M156567</guid>
      <dc:creator>dudisasson</dc:creator>
      <dc:date>2020-04-22T22:30:59Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MM EVK Type C connector</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-EVK-Type-C-connector/m-p/1065335#M156568</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;maybe you can refer to the document as below:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-346008"&gt;https://community.nxp.com/docs/DOC-346008&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Apr 2020 04:40:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-EVK-Type-C-connector/m-p/1065335#M156568</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2020-04-23T04:40:13Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MM EVK Type C connector</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-EVK-Type-C-connector/m-p/1065336#M156569</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="direction: ltr;"&gt;Hi,&lt;/P&gt;&lt;P style="direction: ltr;"&gt;&lt;/P&gt;&lt;P style="direction: ltr;"&gt;i&amp;nbsp;compiled the&amp;nbsp; U-BOOT as described but i am not sure about the changes in the kernel.&lt;/P&gt;&lt;P style="direction: ltr;"&gt;i tried removing this parts:&lt;/P&gt;&lt;P style="direction: ltr;"&gt;&lt;/P&gt;&lt;P style="direction: ltr;"&gt;pinctrl_typec1: typec1grp {&lt;BR /&gt; fsl,pins = &amp;lt;&lt;BR /&gt; MX8MM_IOMUXC_SD1_STROBE_GPIO2_IO11 0x159&lt;BR /&gt; &amp;gt;;&lt;BR /&gt; };&lt;/P&gt;&lt;P style="direction: ltr;"&gt;&lt;/P&gt;&lt;P style="direction: ltr;"&gt;&lt;BR /&gt; typec1_ptn5110: tcpci@50 {&lt;BR /&gt; compatible = "usb,tcpci";&lt;BR /&gt; pinctrl-names = "default";&lt;BR /&gt; pinctrl-0 = &amp;lt;&amp;amp;pinctrl_typec1&amp;gt;;&lt;BR /&gt; reg = &amp;lt;0x50&amp;gt;;&lt;BR /&gt; interrupt-parent = &amp;lt;&amp;amp;gpio2&amp;gt;;&lt;BR /&gt; interrupts = &amp;lt;11 8&amp;gt;;&lt;BR /&gt; src-pdos = &amp;lt;0x380190c8&amp;gt;;&lt;BR /&gt; snk-pdos = &amp;lt;0x380190c8&amp;gt;;&lt;BR /&gt; /* Only can sink 5V for safe */&lt;BR /&gt; max-snk-mv = &amp;lt;5000&amp;gt;;&lt;BR /&gt; max-snk-ma = &amp;lt;3000&amp;gt;;&lt;BR /&gt; op-snk-mw = &amp;lt;10000&amp;gt;;&lt;BR /&gt; max-snk-mw = &amp;lt;15000&amp;gt;;&lt;BR /&gt; port-type = "drp";&lt;BR /&gt; default-role = "sink";&lt;BR /&gt; status = "okay";&lt;BR /&gt; };&lt;/P&gt;&lt;P style="direction: ltr;"&gt;&lt;/P&gt;&lt;P style="direction: ltr;"&gt;and changed the&amp;nbsp;&lt;SPAN&gt;&amp;amp;usbotg config:&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="direction: ltr;"&gt;&amp;amp;usbotg1 {&lt;BR /&gt; dr_mode = "otg";&lt;BR /&gt;/*extcon = &amp;lt;0&amp;gt;, &amp;lt;&amp;amp;typec1_ptn5110&amp;gt;;&lt;BR /&gt; picophy,pre-emp-curr-control = &amp;lt;3&amp;gt;;&lt;BR /&gt; picophy,dc-vol-level-adjust = &amp;lt;7&amp;gt;;*/&lt;BR /&gt; status = "okay";&lt;BR /&gt;};&lt;/P&gt;&lt;P style="direction: ltr;"&gt;&lt;/P&gt;&lt;P style="direction: ltr;"&gt;what do i need to add in the IOMUX? do i need to config the DP/DP lines?&lt;/P&gt;&lt;P style="direction: ltr;"&gt;if so, how do i add them? i didnt find their pinctrl definition.&lt;/P&gt;&lt;P style="direction: ltr;"&gt;do i need to add anything else?&lt;/P&gt;&lt;P style="direction: ltr;"&gt;&lt;/P&gt;&lt;P style="direction: ltr;"&gt;Thanks,&lt;/P&gt;&lt;P style="direction: ltr;"&gt;Dudi.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Apr 2020 09:10:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-EVK-Type-C-connector/m-p/1065336#M156569</guid>
      <dc:creator>dudisasson</dc:creator>
      <dc:date>2020-04-30T09:10:56Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MM EVK Type C connector</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-EVK-Type-C-connector/m-p/1065337#M156570</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="direction: ltr;"&gt;Hi,&lt;/P&gt;&lt;P style="direction: ltr;"&gt;&lt;/P&gt;&lt;P style="direction: ltr;"&gt;any ideas?&lt;/P&gt;&lt;P style="direction: ltr;"&gt;&lt;/P&gt;&lt;P style="direction: ltr;"&gt;Thanks,&lt;/P&gt;&lt;P style="direction: ltr;"&gt;Dudi.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 May 2020 13:42:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-EVK-Type-C-connector/m-p/1065337#M156570</guid>
      <dc:creator>dudisasson</dc:creator>
      <dc:date>2020-05-05T13:42:40Z</dc:date>
    </item>
  </channel>
</rss>