<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Change pin configuration during runtime</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Change-pin-configuration-during-runtime/m-p/1065332#M156565</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Unfortunately runtime pin configuration is not supported by the BSP.&lt;BR /&gt;However you can try to write to IOMUX registers directly from application.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 22 Jun 2020 04:32:26 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2020-06-22T04:32:26Z</dc:date>
    <item>
      <title>Change pin configuration during runtime</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Change-pin-configuration-during-runtime/m-p/1065331#M156564</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i need to reconfigure my I2C clock and data line to GPIO during runtime.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How is it possible on imx8-m4?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Roman&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jun 2020 08:02:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Change-pin-configuration-during-runtime/m-p/1065331#M156564</guid>
      <dc:creator>roman_g1</dc:creator>
      <dc:date>2020-06-19T08:02:56Z</dc:date>
    </item>
    <item>
      <title>Re: Change pin configuration during runtime</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Change-pin-configuration-during-runtime/m-p/1065332#M156565</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Unfortunately runtime pin configuration is not supported by the BSP.&lt;BR /&gt;However you can try to write to IOMUX registers directly from application.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jun 2020 04:32:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Change-pin-configuration-during-runtime/m-p/1065332#M156565</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2020-06-22T04:32:26Z</dc:date>
    </item>
    <item>
      <title>Re: Change pin configuration during runtime</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Change-pin-configuration-during-runtime/m-p/1065333#M156566</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, thank you for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a given sequence to write to register for changing the pin configuration?&lt;/P&gt;&lt;P&gt;For example if i want to write to MIPI_DSI1_GPIO0_00 register to set the mode to "000b".&lt;/P&gt;&lt;P&gt;Is the mux_mode field to set enough?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/113391iC2B06E065A8B8833/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/113392i98D06180663330A6/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jun 2020 07:01:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Change-pin-configuration-during-runtime/m-p/1065333#M156566</guid>
      <dc:creator>roman_g1</dc:creator>
      <dc:date>2020-06-22T07:01:02Z</dc:date>
    </item>
  </channel>
</rss>