<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: More than 4 CS lines for SPI</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/More-than-4-CS-lines-for-SPI/m-p/1064887#M156503</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marcus&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes this understanding is correct.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 24 May 2020 23:21:04 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2020-05-24T23:21:04Z</dc:date>
    <item>
      <title>More than 4 CS lines for SPI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/More-than-4-CS-lines-for-SPI/m-p/1064886#M156502</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The documentation&amp;nbsp;for iMX6UL and iMX8 says SPI has 4 CS lines.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I intend to&amp;nbsp;use a total of 12 SPI devices connected to SPI1, 2 and 3 (4 in each).&lt;BR /&gt;As far as I understood, I can configure CS pins as GPIO and use the kernel driver configurations to define all 12 CS lines from GPIOs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is my understanding correct or is there some hardware limitation I'm missing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 May 2020 03:57:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/More-than-4-CS-lines-for-SPI/m-p/1064886#M156502</guid>
      <dc:creator>marcus_cps</dc:creator>
      <dc:date>2020-05-23T03:57:47Z</dc:date>
    </item>
    <item>
      <title>Re: More than 4 CS lines for SPI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/More-than-4-CS-lines-for-SPI/m-p/1064887#M156503</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marcus&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes this understanding is correct.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 24 May 2020 23:21:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/More-than-4-CS-lines-for-SPI/m-p/1064887#M156503</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-05-24T23:21:04Z</dc:date>
    </item>
  </channel>
</rss>