<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FLEX-iMX8M Mini can't use VPU encoder in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/FLEX-iMX8M-Mini-can-t-use-VPU-encoder/m-p/1064638#M156457</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I changed to using Yocto image OS (built by Technexion). Now VPU is working well now.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 May 2020 06:52:06 GMT</pubDate>
    <dc:creator>toanjunifer</dc:creator>
    <dc:date>2020-05-28T06:52:06Z</dc:date>
    <item>
      <title>FLEX-iMX8M Mini can't use VPU encoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FLEX-iMX8M-Mini-can-t-use-VPU-encoder/m-p/1064637#M156456</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using FLEX iMX8M Mini (by Technexion). I built image OS with&amp;nbsp;&lt;A href="https://github.com/TechNexion/tn-imx-yocto-manifest/tree/sumo_4.14.y_GA-stable"&gt;Yocto&lt;/A&gt;. I also install gstreamer-1.0.&amp;nbsp;&lt;/P&gt;&lt;P&gt;VPU encoder:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;vpu: vpuenc_h264: IMX VPU-based AVC/H264 video encoder&lt;BR /&gt;vpu: vpuenc_mpeg4: IMX VPU-based MPEG4 video encoder&lt;BR /&gt;vpu: vpuenc_h263: IMX VPU-based H263 video encoder&lt;BR /&gt;vpu: vpuenc_jpeg: IMX VPU-based JPEG video encoder&lt;BR /&gt;vpu: vpudec: IMX VPU-based video decoder&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;But when I run gstreamer command to record video, I get this:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Setting pipeline to PAUSED ...&lt;BR /&gt;[ERR] Error: Unable to obtain system rev information&lt;BR /&gt;[ERR] IOSystemInit() failure.&lt;BR /&gt;ERROR: Pipeline doesn't want to pause.&lt;BR /&gt;ERROR: from element /GstPipeline:pipeline0/vpuenc_h264:vpuenc_h264-0: Could not initialize supporting library.&lt;BR /&gt;Additional debug info:&lt;BR /&gt;../../../../git/gst-libs/gst/video/gstvideoencoder.c(1627): gst_video_encoder_change_state (): /GstPipeline:pipeline0/vpuenc_h264:vpuenc_h264-0:&lt;BR /&gt;Failed to open encoder&lt;BR /&gt;Setting pipeline to NULL ...&lt;BR /&gt;Freeing pipeline ...&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;This is the first time I use iMX8M Mini. I have no idea with this issue.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I also receive this message each&amp;nbsp;10 seconds.&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;[ 1122.994574] alloc_contig_range: [60240, 60254) PFNs busy&lt;BR /&gt;[ 1133.230580] alloc_contig_range: [60240, 60254) PFNs busy&lt;BR /&gt;[ 1143.485313] alloc_contig_range: [60240, 60254) PFNs busy&lt;BR /&gt;[ 1153.733584] alloc_contig_range: [60240, 60254) PFNs busy&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;What should I do now ?&lt;/P&gt;&lt;P&gt;Thank you so much,&lt;/P&gt;&lt;P&gt;Toan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 May 2020 12:11:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FLEX-iMX8M-Mini-can-t-use-VPU-encoder/m-p/1064637#M156456</guid>
      <dc:creator>toanjunifer</dc:creator>
      <dc:date>2020-05-22T12:11:58Z</dc:date>
    </item>
    <item>
      <title>Re: FLEX-iMX8M Mini can't use VPU encoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FLEX-iMX8M-Mini-can-t-use-VPU-encoder/m-p/1064638#M156457</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I changed to using Yocto image OS (built by Technexion). Now VPU is working well now.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 May 2020 06:52:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FLEX-iMX8M-Mini-can-t-use-VPU-encoder/m-p/1064638#M156457</guid>
      <dc:creator>toanjunifer</dc:creator>
      <dc:date>2020-05-28T06:52:06Z</dc:date>
    </item>
  </channel>
</rss>