<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックUSB port is not detecting on i.MX6 Quad board.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-port-is-not-detecting-on-i-MX6-Quad-board/m-p/1064569#M156441</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;We are prototyping a custom board with the i.MX6 Quad processor part no is MCIMX6Q5EYM10AD and USB controller part is USB2422-I/MJ . We have 2 USB ports available, both ports are not detecting USB drive/Keyboard once boot the device.&lt;BR /&gt;Electrically i have probe and checked the voltage attached table below for reference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE border="0" cellpadding="0" cellspacing="0" height="80" style="border-collapse: collapse; width: 185.28pt;" width="247"&gt;&lt;TBODY&gt;&lt;TR style="height: 15.00pt;"&gt;&lt;TD class="" height="20" style="height: 15.00pt; width: 70.70pt;" width="94"&gt;(USB_PORT1)_USBPWR1&lt;/TD&gt;&lt;TD class="" style="width: 114.75pt;" width="153"&gt;&amp;nbsp; 3.17V&lt;/TD&gt;&lt;/TR&gt;&lt;TR style="height: 15.00pt;"&gt;&lt;TD class="" height="20" style="height: 15.00pt;"&gt;(USB_PORT2)_USBPWR2&lt;/TD&gt;&lt;TD class=""&gt;4.97V&lt;/TD&gt;&lt;/TR&gt;&lt;TR style="height: 15.00pt;"&gt;&lt;TD class="" height="20" style="height: 15.00pt;"&gt;ENA&lt;/TD&gt;&lt;TD class=""&gt;1.256V&lt;/TD&gt;&lt;/TR&gt;&lt;TR style="height: 15.00pt;"&gt;&lt;TD class="" height="20" style="height: 15.00pt;"&gt;ENB&lt;/TD&gt;&lt;TD class=""&gt;1.256V&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;Above table USB port is VCC is 3.17V which is not expected ENA(OCS1) 1.256V which is not expected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help me to resolve this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Advance Thanks,&lt;/P&gt;&lt;P&gt;Ramesha S P&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Jun 2020 11:13:44 GMT</pubDate>
    <dc:creator>rameshasp</dc:creator>
    <dc:date>2020-06-18T11:13:44Z</dc:date>
    <item>
      <title>USB port is not detecting on i.MX6 Quad board.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-port-is-not-detecting-on-i-MX6-Quad-board/m-p/1064569#M156441</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;We are prototyping a custom board with the i.MX6 Quad processor part no is MCIMX6Q5EYM10AD and USB controller part is USB2422-I/MJ . We have 2 USB ports available, both ports are not detecting USB drive/Keyboard once boot the device.&lt;BR /&gt;Electrically i have probe and checked the voltage attached table below for reference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE border="0" cellpadding="0" cellspacing="0" height="80" style="border-collapse: collapse; width: 185.28pt;" width="247"&gt;&lt;TBODY&gt;&lt;TR style="height: 15.00pt;"&gt;&lt;TD class="" height="20" style="height: 15.00pt; width: 70.70pt;" width="94"&gt;(USB_PORT1)_USBPWR1&lt;/TD&gt;&lt;TD class="" style="width: 114.75pt;" width="153"&gt;&amp;nbsp; 3.17V&lt;/TD&gt;&lt;/TR&gt;&lt;TR style="height: 15.00pt;"&gt;&lt;TD class="" height="20" style="height: 15.00pt;"&gt;(USB_PORT2)_USBPWR2&lt;/TD&gt;&lt;TD class=""&gt;4.97V&lt;/TD&gt;&lt;/TR&gt;&lt;TR style="height: 15.00pt;"&gt;&lt;TD class="" height="20" style="height: 15.00pt;"&gt;ENA&lt;/TD&gt;&lt;TD class=""&gt;1.256V&lt;/TD&gt;&lt;/TR&gt;&lt;TR style="height: 15.00pt;"&gt;&lt;TD class="" height="20" style="height: 15.00pt;"&gt;ENB&lt;/TD&gt;&lt;TD class=""&gt;1.256V&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;Above table USB port is VCC is 3.17V which is not expected ENA(OCS1) 1.256V which is not expected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help me to resolve this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Advance Thanks,&lt;/P&gt;&lt;P&gt;Ramesha S P&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jun 2020 11:13:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-port-is-not-detecting-on-i-MX6-Quad-board/m-p/1064569#M156441</guid>
      <dc:creator>rameshasp</dc:creator>
      <dc:date>2020-06-18T11:13:44Z</dc:date>
    </item>
    <item>
      <title>Re: USB port is not detecting on i.MX6 Quad board.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-port-is-not-detecting-on-i-MX6-Quad-board/m-p/1064570#M156442</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ramesha&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try to narrow down issue, checking if this is caused by USB2422 or i.MX6,&lt;/P&gt;&lt;P&gt;please check:&lt;/P&gt;&lt;P&gt;&lt;A data-doctype="Application Notes" data-type="Application Notes" href="http://www.microchip.com//wwwAppNotes/AppNotes.aspx?appnote=en567016" target="_blank"&gt;AN26.21 - USB Device Design Checklist&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A data-doctype="Application Notes" data-type="Application Notes" href="http://www.microchip.com/wwwappnotes/appnotes.aspx?appnote=en562711" target="_blank"&gt;AN 26.2 - Implementation Guidelines for Microchip's USB 2.0 and USB 3.0 Hub Devices&lt;/A&gt;&lt;/P&gt;&lt;P&gt;i.MX6 usb side:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-105609"&gt;https://community.nxp.com/docs/DOC-105609&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jun 2020 00:42:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-port-is-not-detecting-on-i-MX6-Quad-board/m-p/1064570#M156442</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-06-19T00:42:01Z</dc:date>
    </item>
    <item>
      <title>Re: USB port is not detecting on i.MX6 Quad board.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-port-is-not-detecting-on-i-MX6-Quad-board/m-p/1064571#M156443</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your reply Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My problem is while doing board bring up test if I connect any USB pendrive or keyboard it should detect, but in our it is not.&lt;/P&gt;&lt;P&gt;We are not able stop the u-boot and type any command .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help me to resolve this.&lt;/P&gt;&lt;P&gt;Advance Thank you,&lt;/P&gt;&lt;P&gt;Ramesha S P&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jun 2020 03:33:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-port-is-not-detecting-on-i-MX6-Quad-board/m-p/1064571#M156443</guid>
      <dc:creator>rameshasp</dc:creator>
      <dc:date>2020-06-19T03:33:37Z</dc:date>
    </item>
  </channel>
</rss>