<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックPython package installation fails due to aarch64-poky-linux-gcc: No such file or directory</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Python-package-installation-fails-due-to-aarch64-poky-linux-gcc/m-p/1064550#M156434</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I&amp;nbsp;am using the BSP Linux Image &lt;A href="https://www.nxp.com/webapp/sps/download/preDownload.jsp"&gt;L5.4.24-2.1.0_images_MX8MMEVK&lt;/A&gt;&amp;nbsp;for &amp;nbsp;my i.MX8M mini Evalkit.&lt;/P&gt;&lt;P&gt;I want to use several i2cdevices on my i.MX&amp;nbsp;and therefore I&amp;nbsp;need to install some packages, one of it is smbus.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When installing with: &lt;STRONG&gt;pip3 install smbus&lt;/STRONG&gt;&amp;nbsp;, I get the following output, where it says (see appended file):&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;unable to execute 'aarch64-poky-linux-gcc': No such file or directory&lt;BR /&gt; error: command 'aarch64-poky-linux-gcc' failed with exit status 1&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did some research but don't know how to get the&lt;STRONG&gt;&amp;nbsp;aarch64-poky-linux-gcc.&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Another issue I have is, that I can't build the imx-image-full by myselfe because I always get error when installing some packages during the build process (&lt;A _jive_internal="true" href="https://community.nxp.com/thread/538107"&gt;see this article&lt;/A&gt;). So I am not able to build the toolchain with &lt;STRONG&gt;populate_sdk&lt;/STRONG&gt; command.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maybe someone has the same issue or knows a solution for my problem?&lt;/P&gt;&lt;P&gt;Alternatively can I use i2cdevices without smbus? Installing smbus2 (pip3 install smbus2) works, but the library I am using for my sensor is not&amp;nbsp;designed for it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&amp;nbsp;&lt;/P&gt;&lt;P&gt;Patrick Stenger&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Aug 2020 08:29:06 GMT</pubDate>
    <dc:creator>pstenger</dc:creator>
    <dc:date>2020-08-05T08:29:06Z</dc:date>
    <item>
      <title>Python package installation fails due to aarch64-poky-linux-gcc: No such file or directory</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Python-package-installation-fails-due-to-aarch64-poky-linux-gcc/m-p/1064550#M156434</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I&amp;nbsp;am using the BSP Linux Image &lt;A href="https://www.nxp.com/webapp/sps/download/preDownload.jsp"&gt;L5.4.24-2.1.0_images_MX8MMEVK&lt;/A&gt;&amp;nbsp;for &amp;nbsp;my i.MX8M mini Evalkit.&lt;/P&gt;&lt;P&gt;I want to use several i2cdevices on my i.MX&amp;nbsp;and therefore I&amp;nbsp;need to install some packages, one of it is smbus.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When installing with: &lt;STRONG&gt;pip3 install smbus&lt;/STRONG&gt;&amp;nbsp;, I get the following output, where it says (see appended file):&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;unable to execute 'aarch64-poky-linux-gcc': No such file or directory&lt;BR /&gt; error: command 'aarch64-poky-linux-gcc' failed with exit status 1&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did some research but don't know how to get the&lt;STRONG&gt;&amp;nbsp;aarch64-poky-linux-gcc.&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Another issue I have is, that I can't build the imx-image-full by myselfe because I always get error when installing some packages during the build process (&lt;A _jive_internal="true" href="https://community.nxp.com/thread/538107"&gt;see this article&lt;/A&gt;). So I am not able to build the toolchain with &lt;STRONG&gt;populate_sdk&lt;/STRONG&gt; command.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maybe someone has the same issue or knows a solution for my problem?&lt;/P&gt;&lt;P&gt;Alternatively can I use i2cdevices without smbus? Installing smbus2 (pip3 install smbus2) works, but the library I am using for my sensor is not&amp;nbsp;designed for it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&amp;nbsp;&lt;/P&gt;&lt;P&gt;Patrick Stenger&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Aug 2020 08:29:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Python-package-installation-fails-due-to-aarch64-poky-linux-gcc/m-p/1064550#M156434</guid>
      <dc:creator>pstenger</dc:creator>
      <dc:date>2020-08-05T08:29:06Z</dc:date>
    </item>
    <item>
      <title>Re: Python package installation fails due to aarch64-poky-linux-gcc: No such file or directory</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Python-package-installation-fails-due-to-aarch64-poky-linux-gcc/m-p/1064551#M156435</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please try to add this line into local.conf file:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;IMAGE_INSTALL_append = " python-smbus"&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Aug 2020 02:37:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Python-package-installation-fails-due-to-aarch64-poky-linux-gcc/m-p/1064551#M156435</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2020-08-06T02:37:38Z</dc:date>
    </item>
    <item>
      <title>Re: Python package installation fails due to aarch64-poky-linux-gcc: No such file or directory</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Python-package-installation-fails-due-to-aarch64-poky-linux-gcc/m-p/1064552#M156436</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hm, this will only work if I build the Image myselfe with Yocto Right?&lt;/P&gt;&lt;P&gt;Unfortunately this does not work :smileysad: (see article linked in my first comment)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But thanks for your hint.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I want to install &lt;STRONG&gt;smbus&lt;/STRONG&gt; or &lt;STRONG&gt;smbus2&lt;/STRONG&gt; with &lt;STRONG&gt;pip3&lt;/STRONG&gt; is there also a command which I could use in the &lt;STRONG&gt;local.conf&lt;/STRONG&gt; instead &lt;STRONG&gt;python-smbus&lt;/STRONG&gt; or is it the same at the end of the day?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Aug 2020 07:08:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Python-package-installation-fails-due-to-aarch64-poky-linux-gcc/m-p/1064552#M156436</guid>
      <dc:creator>pstenger</dc:creator>
      <dc:date>2020-08-06T07:08:03Z</dc:date>
    </item>
    <item>
      <title>Re: Python package installation fails due to aarch64-poky-linux-gcc: No such file or directory</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Python-package-installation-fails-due-to-aarch64-poky-linux-gcc/m-p/1064553#M156437</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey Victor,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I finally was able to build the imx-image-full and like you suggested I added the line in the local.conf file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Another issue I am facing is the following:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Another library I want to use in my image is the "&lt;SPAN style="color: #c7254e; background-color: #f9f2f4;"&gt;adafruit-circuitpython-ina219&lt;/SPAN&gt;" which normally is installed with&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;SPAN style="color: #c7254e; background-color: #f9f2f4;"&gt;sudo pip3 install adafruit-circuitpython-ina219&lt;/SPAN&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Unfortunately it&amp;nbsp; does not find&amp;nbsp;"&lt;SPAN&gt;aarch64-poky-linux-gcc" and throws the error when trying to install via pip3&lt;/SPAN&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;unable to execute 'aarch64-poky-linux-gcc': No such file or directory&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;So is there a solution to build the library during the image build process?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Alternatively how do I get the&amp;nbsp;&lt;SPAN style="background-color: #f6f6f6;"&gt;aarch64-poky-linux-gcc? Maybe with :&lt;/SPAN&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;SPAN style="background-color: #f6f6f6;"&gt;bitbake &amp;lt;image_name&amp;gt; -c populate_sdk&lt;/SPAN&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also ask besides trying myselfe because the build need very much time and I dont want to run in the wrong direction.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help, regards&lt;/P&gt;&lt;P&gt;Patrick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Aug 2020 08:53:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Python-package-installation-fails-due-to-aarch64-poky-linux-gcc/m-p/1064553#M156437</guid>
      <dc:creator>pstenger</dc:creator>
      <dc:date>2020-08-26T08:53:52Z</dc:date>
    </item>
    <item>
      <title>Re: Python package installation fails due to aarch64-poky-linux-gcc: No such file or directory</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Python-package-installation-fails-due-to-aarch64-poky-linux-gcc/m-p/1064554#M156438</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Patrick,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you able to resolve the&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;"&lt;/SPAN&gt;&lt;SPAN style="color: #51626f; background-color: #f6f6f6;"&gt;unable to execute 'aarch64-poky-linux-gcc': No such file or directory"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I am also facing the similar error, Could you please share details if you have resolved&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Sreedhar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Aug 2020 07:14:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Python-package-installation-fails-due-to-aarch64-poky-linux-gcc/m-p/1064554#M156438</guid>
      <dc:creator>sreedhar_appala</dc:creator>
      <dc:date>2020-08-28T07:14:25Z</dc:date>
    </item>
    <item>
      <title>Re: Python package installation fails due to aarch64-poky-linux-gcc: No such file or directory</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Python-package-installation-fails-due-to-aarch64-poky-linux-gcc/m-p/1064555#M156439</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, I could not solve the issue by now :smileysad:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Aug 2020 07:39:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Python-package-installation-fails-due-to-aarch64-poky-linux-gcc/m-p/1064555#M156439</guid>
      <dc:creator>pstenger</dc:creator>
      <dc:date>2020-08-28T07:39:13Z</dc:date>
    </item>
    <item>
      <title>Re: Python package installation fails due to aarch64-poky-linux-gcc: No such file or directory</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Python-package-installation-fails-due-to-aarch64-poky-linux-gcc/m-p/1064556#M156440</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Patrick,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the response.&lt;/P&gt;&lt;P&gt;I got the below response from nxp,&amp;nbsp; &amp;nbsp;please check it might help you.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/540924"&gt;https://community.nxp.com/thread/540924&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Sreedhar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Aug 2020 15:48:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Python-package-installation-fails-due-to-aarch64-poky-linux-gcc/m-p/1064556#M156440</guid>
      <dc:creator>sreedhar_appala</dc:creator>
      <dc:date>2020-08-28T15:48:05Z</dc:date>
    </item>
  </channel>
</rss>