<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx6solosabresd do_image_wic failed in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6solosabresd-do-image-wic-failed/m-p/1063836#M156333</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, it worked. The file "u-boot-emmc-2019.04-r0.imx" was deployed. But another problem is mfgtools downloading.&lt;/P&gt;&lt;P&gt;Firstly, I used "bitbake fsl-image-mfgtool-initramfs&amp;nbsp;" to produce firmware sucessfully.&lt;/P&gt;&lt;P&gt;Then, L4.9.88_2.0.0_mfg-tool-with-rootfs was used&amp;nbsp; to download the firmware and kernels.&amp;nbsp; But it stopped at "Jumping to OS image". There was nothing output at the debug uart1.&lt;/P&gt;&lt;P&gt;The XML configuration file is attached. I revised the original XML file for solo device downloading. The vid and pid of solo and MX6D were the same. Only the downloading files related were substituted. But it seemed faild. Please help. Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Jun 2020 12:56:04 GMT</pubDate>
    <dc:creator>jfsong1</dc:creator>
    <dc:date>2020-06-04T12:56:04Z</dc:date>
    <item>
      <title>imx6solosabresd do_image_wic failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6solosabresd-do-image-wic-failed/m-p/1063829#M156326</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;您好，我在ubuntu18.04环境中，LF_L5.4.3_1.0.0生成针对imx6solo的 image,uboot等，但是最后阶段报错误，无法生成u-boot.imx，最后也无法生成需要的image等文件，不知道是什么原因，谢谢。&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DISTRO=fsl-imx-fb MACHINE=imx6solosabresd source imx-setup-release.sh -b buildminimal&lt;BR /&gt;echo "UBOOT_CONFIG = \"emmc\"" &amp;gt;&amp;gt; conf/local.conf&lt;BR /&gt;bitbake core-image-minimal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;jfsong@ubuntu:~/imx-yocto-bsp/buildminimal$ bitbake core-image-minimal&lt;BR /&gt;NOTE: Your conf/bblayers.conf has been automatically updated.&lt;BR /&gt;Loading cache: 100% |############################################| Time: 0:00:02&lt;BR /&gt;Loaded 4067 entries from dependency cache.&lt;BR /&gt;NOTE: Resolving any missing task queue dependencies&lt;/P&gt;&lt;P&gt;Build Configuration:&lt;BR /&gt;BB_VERSION = "1.44.0"&lt;BR /&gt;BUILD_SYS = "x86_64-linux"&lt;BR /&gt;NATIVELSBSTRING = "ubuntu-18.04"&lt;BR /&gt;TARGET_SYS = "arm-poky-linux-gnueabi"&lt;BR /&gt;MACHINE = "imx6solosabresd"&lt;BR /&gt;DISTRO = "fsl-imx-fb"&lt;BR /&gt;DISTRO_VERSION = "5.4-zeus"&lt;BR /&gt;TUNE_FEATURES = "arm vfp cortexa9 neon thumb callconvention-hard"&lt;BR /&gt;TARGET_FPU = "hard"&lt;BR /&gt;meta &lt;BR /&gt;meta-poky = "HEAD:0275e68b0576cdefc19718e4b1977044f9f43f48"&lt;BR /&gt;meta-oe &lt;BR /&gt;meta-multimedia &lt;BR /&gt;meta-python = "HEAD:aad5b3d070cd8c58828b0975cf861d8ebc90f460"&lt;BR /&gt;meta-freescale = "HEAD:0be39721cea6e04c589a419f4bb07fabd0da6704"&lt;BR /&gt;meta-freescale-3rdparty = "HEAD:aea3771baa77e74762358ceb673d407e36637e5f"&lt;BR /&gt;meta-freescale-distro = "HEAD:ca27d12e4964d1336e662bcc60184bbff526c857"&lt;BR /&gt;meta-bsp &lt;BR /&gt;meta-sdk &lt;BR /&gt;meta-ml = "HEAD:435f5e984856a943986491fddd061734a0b9eba5"&lt;BR /&gt;meta-browser = "HEAD:5f365ef0f842ba4651efe88787cf9c63bc8b6cb3"&lt;BR /&gt;meta-rust = "HEAD:5cda04c7c2158fc982502ca1e7893f71e4ca1729"&lt;BR /&gt;meta-gnome &lt;BR /&gt;meta-networking &lt;BR /&gt;meta-filesystems = "HEAD:aad5b3d070cd8c58828b0975cf861d8ebc90f460"&lt;BR /&gt;meta-qt5 = "HEAD:432ad2aa6c3a13253fefc909faba368851d21fb1"&lt;/P&gt;&lt;P&gt;WARNING: /home/jfsong/imx-yocto-bsp/sources/meta-imx/meta-bsp/recipes-bsp/u-boot/u-boot-imx_2019.04.bb:do_compile is tainted from a forced run&lt;BR /&gt;WARNING: /home/jfsong/imx-yocto-bsp/sources/meta-imx/meta-bsp/recipes-bsp/u-boot/u-boot-imx_2019.04.bb:do_deploy is tainted from a forced run&lt;BR /&gt;Initialising tasks: 100% |#######################################| Time: 0:00:02&lt;BR /&gt;Sstate summary: Wanted 45 Found 0 Missed 45 Current 736 (0% match, 94% complete)&lt;BR /&gt;NOTE: Executing Tasks&lt;BR /&gt;NOTE: Setscene tasks completed&lt;BR /&gt;ERROR: core-image-minimal-1.0-r0 do_image_wic: Execution of '/home/jfsong/imx-yocto-bsp/buildminimal/tmp/work/imx6solosabresd-poky-linux-gnueabi/core-image-minimal/1.0-r0/temp/run.do_image_wic.93572' failed with exit code 1:&lt;BR /&gt;INFO: Creating image(s)...&lt;/P&gt;&lt;P&gt;Traceback (most recent call last):&lt;BR /&gt; File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 127, in _open_image_file&lt;BR /&gt; self._f_image = open(self._image_path, 'rb')&lt;BR /&gt;FileNotFoundError: [Errno 2] No such file or directory: '/home/jfsong/imx-yocto-bsp/buildminimal/tmp/deploy/images/imx6solosabresd/u-boot.imx'&lt;/P&gt;&lt;P&gt;During handling of the above exception, another exception occurred:&lt;/P&gt;&lt;P&gt;Traceback (most recent call last):&lt;BR /&gt; File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/wic", line 525, in &amp;lt;module&amp;gt;&lt;BR /&gt; sys.exit(main(sys.argv[1:]))&lt;BR /&gt; File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/wic", line 520, in main&lt;BR /&gt; return hlp.invoke_subcommand(args, parser, hlp.wic_help_usage, subcommands)&lt;BR /&gt; File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/help.py", line 83, in invoke_subcommand&lt;BR /&gt; subcmd[0](args, usage)&lt;BR /&gt; File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/wic", line 220, in wic_create_subcommand&lt;BR /&gt; native_sysroot, options)&lt;BR /&gt; File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/engine.py", line 189, in wic_create&lt;BR /&gt; plugin.do_create()&lt;BR /&gt; File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/plugins/imager/direct.py", line 86, in do_create&lt;BR /&gt; self.create()&lt;BR /&gt; File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/plugins/imager/direct.py", line 179, in create&lt;BR /&gt; self._image.prepare(self)&lt;BR /&gt; File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/plugins/imager/direct.py", line 354, in prepare&lt;BR /&gt; imager.kernel_dir, imager.native_sysroot)&lt;BR /&gt; File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/partition.py", line 174, in prepare&lt;BR /&gt; kernel_dir, rootfs_dir, native_sysroot)&lt;BR /&gt; File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/plugins/source/rawcopy.py", line 68, in do_prepare_partition&lt;BR /&gt; sparse_copy(src, dst)&lt;BR /&gt; File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 550, in sparse_copy&lt;BR /&gt; fmap = api(src_fname)&lt;BR /&gt; File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 532, in filemap&lt;BR /&gt; return FilemapFiemap(image, log)&lt;BR /&gt; File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 350, in __init__&lt;BR /&gt; _FilemapBase.__init__(self, image, log)&lt;BR /&gt; File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 86, in __init__&lt;BR /&gt; self._open_image_file()&lt;BR /&gt; File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 130, in _open_image_file&lt;BR /&gt; % (self._image_path, err))&lt;BR /&gt;wic.filemap.Error: cannot open image file '/home/jfsong/imx-yocto-bsp/buildminimal/tmp/deploy/images/imx6solosabresd/u-boot.imx': [Errno 2] No such file or directory: '/home/jfsong/imx-yocto-bsp/buildminimal/tmp/deploy/images/imx6solosabresd/u-boot.imx'&lt;BR /&gt;WARNING: exit code 1 from a shell command.&lt;/P&gt;&lt;P&gt;ERROR: Logfile of failure stored in: /home/jfsong/imx-yocto-bsp/buildminimal/tmp/work/imx6solosabresd-poky-linux-gnueabi/core-image-minimal/1.0-r0/temp/log.do_image_wic.93572&lt;BR /&gt;Log data follows:&lt;BR /&gt;| DEBUG: Executing python function set_image_size&lt;BR /&gt;| DEBUG: 49602.800000 = 38156 * 1.300000&lt;BR /&gt;| DEBUG: 53698.800000 = max(49602.800000, 8192)[49602.800000] + 4096&lt;BR /&gt;| DEBUG: 53699.000000 = int(53698.800000)&lt;BR /&gt;| DEBUG: 53699 = aligned(53699)&lt;BR /&gt;| DEBUG: returning 53699&lt;BR /&gt;| DEBUG: Python function set_image_size finished&lt;BR /&gt;| DEBUG: Executing python function extend_recipe_sysroot&lt;BR /&gt;| NOTE: Direct dependencies are ['/home/jfsong/imx-yocto-bsp/sources/meta-imx/meta-bsp/recipes-kernel/linux/linux-imx_5.4.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/python/python-native_2.7.16.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-bsp/u-boot/u-boot-tools_2019.07.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/dnf/dnf_4.2.2.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-core/glibc/glibc_2.30.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/bison/bison_3.4.1.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-core/glibc/ldconfig-native_2.12.1.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/automake/automake_1.16.1.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/qemu/qemuwrapper-cross_1.0.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/libtool/libtool-native_2.4.6.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-support/bmap-tools/bmap-tools_3.5.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/mklibs/mklibs-native_0.1.44.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/opkg-utils/opkg-utils_0.4.1.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-support/lzop/lzop_1.04.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-core/update-rc.d/update-rc.d_0.8.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/autoconf/autoconf_2.69.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-extended/pigz/pigz_2.4.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/meta-imx/meta-bsp/recipes-bsp/u-boot/u-boot-imx_2019.04.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/flex/flex_2.6.0.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/meta-freescale/recipes-security/optee-imx/optee-os_3.2.0.imx.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/libtool/libtool-cross_2.4.6.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/binutils/binutils-cross_2.32.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/makedevs/makedevs_1.0.1.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/gcc/gcc-cross_9.2.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/quilt/quilt-native_0.66.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-connectivity/openssl/openssl_1.1.1d.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-kernel/kmod/depmodwrapper-cross_1.0.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/prelink/prelink_git.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-core/glibc/cross-localedef-native_2.30.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-extended/bc/bc_1.07.1.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-extended/parted/parted_3.2.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/gnu-config/gnu-config_git.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/meta-imx/meta-bsp/recipes-devtools/python/python-pycrypto_2.6.1.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/opkg/opkg_0.4.1.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/mtools/mtools_4.0.23.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/fdisk/gptfdisk_1.0.4.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/swig/swig_3.0.12.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-kernel/dtc/dtc_1.5.1.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-extended/pbzip2/pbzip2_1.1.13.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/createrepo-c/createrepo-c_0.15.0.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/pseudo/pseudo_git.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/rpm/rpm_4.14.2.1.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/dosfstools/dosfstools_4.1.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-kernel/kern-tools/kern-tools-native_git.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-kernel/kmod/kmod-native_git.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/e2fsprogs/e2fsprogs_1.45.3.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/gcc/gcc-runtime_9.2.bb:do_populate_sysroot']&lt;BR /&gt;| NOTE: Installed into sysroot: []&lt;BR /&gt;| NOTE: Skipping as already exists in sysroot: ['linux-imx', 'python-native', 'u-boot-tools-native', 'dnf-native', 'glibc', 'bison-native', 'ldconfig-native', 'automake-native', 'qemuwrapper-cross', 'libtool-native', 'bmap-tools-native', 'mklibs-native', 'opkg-utils-native', 'lzop-native', 'update-rc.d-native', 'autoconf-native', 'pigz-native', 'u-boot-imx', 'flex-native', 'optee-os', 'libtool-cross', 'binutils-cross-arm', 'makedevs-native', 'gcc-cross-arm', 'quilt-native', 'openssl-native', 'depmodwrapper-cross', 'prelink-native', 'cross-localedef-native', 'bc-native', 'parted-native', 'gnu-config-native', 'python-pycrypto-native', 'opkg-native', 'mtools-native', 'gptfdisk-native', 'swig-native', 'dtc-native', 'pbzip2-native', 'createrepo-c-native', 'pseudo-native', 'rpm-native', 'dosfstools-native', 'kern-tools-native', 'kmod-native', 'e2fsprogs-native', 'gcc-runtime', 'bzip2-native', 'expat-native', 'zlib-native', 'sqlite3-native', 'pkgconfig-native', 'gdbm-native', 'xz-native', 'readline-native', 'db-native', 'systemd-systemctl-native', 'gettext-minimal-native', 'python3-iniparse-native', 'ninja-native', 'librepo-native', 'libdnf-native', 'libcomps-native', 'cmake-native', 'python3-native', 'elfutils-native', 'binutils-native', 'linux-libc-headers', 'texinfo-dummy-native', 'm4-native', 'qemu-native', 'util-linux-native', 'ncurses-native', 'shadow-native', 'python3-setuptools-native', 'python3-six-native', 'lzo-native', 'debianutils-native', 'libsolv-native', 'libarchive-native', 'gmp-native', 'libpcre-native', 'popt-native', 'glib-2.0-native', 'curl-native', 'file-native', 'libmodulemd-native', 'libxml2-native', 'perl-native', 'dbus-native', 'nss-native', 'gtk-doc-native', 'mpfr-native', 'libmpc-native', 'attr-native', 'libgcc', 're2c-native', 'gpgme-native', 'gobject-introspection-native', 'libcheck-native', 'json-c-native', 'libtirpc-native', 'libffi-native', 'libnsl2-native', 'libcap-ng-native', 'unzip-native', 'gettext-native', 'meson-native', 'libyaml-native', 'nspr-native', 'libassuan-native', 'libgpg-error-native']&lt;BR /&gt;| DEBUG: Python function extend_recipe_sysroot finished&lt;BR /&gt;| DEBUG: Executing shell function do_image_wic&lt;BR /&gt;| INFO: Creating image(s)...&lt;BR /&gt;| &lt;BR /&gt;| Traceback (most recent call last):&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 127, in _open_image_file&lt;BR /&gt;| self._f_image = open(self._image_path, 'rb')&lt;BR /&gt;| FileNotFoundError: [Errno 2] No such file or directory: '/home/jfsong/imx-yocto-bsp/buildminimal/tmp/deploy/images/imx6solosabresd/u-boot.imx'&lt;BR /&gt;| &lt;BR /&gt;| During handling of the above exception, another exception occurred:&lt;BR /&gt;| &lt;BR /&gt;| Traceback (most recent call last):&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/wic", line 525, in &amp;lt;module&amp;gt;&lt;BR /&gt;| sys.exit(main(sys.argv[1:]))&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/wic", line 520, in main&lt;BR /&gt;| return hlp.invoke_subcommand(args, parser, hlp.wic_help_usage, subcommands)&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/help.py", line 83, in invoke_subcommand&lt;BR /&gt;| subcmd[0](args, usage)&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/wic", line 220, in wic_create_subcommand&lt;BR /&gt;| native_sysroot, options)&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/engine.py", line 189, in wic_create&lt;BR /&gt;| plugin.do_create()&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/plugins/imager/direct.py", line 86, in do_create&lt;BR /&gt;| self.create()&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/plugins/imager/direct.py", line 179, in create&lt;BR /&gt;| self._image.prepare(self)&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/plugins/imager/direct.py", line 354, in prepare&lt;BR /&gt;| imager.kernel_dir, imager.native_sysroot)&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/partition.py", line 174, in prepare&lt;BR /&gt;| kernel_dir, rootfs_dir, native_sysroot)&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/plugins/source/rawcopy.py", line 68, in do_prepare_partition&lt;BR /&gt;| sparse_copy(src, dst)&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 550, in sparse_copy&lt;BR /&gt;| fmap = api(src_fname)&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 532, in filemap&lt;BR /&gt;| return FilemapFiemap(image, log)&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 350, in __init__&lt;BR /&gt;| _FilemapBase.__init__(self, image, log)&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 86, in __init__&lt;BR /&gt;| self._open_image_file()&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 130, in _open_image_file&lt;BR /&gt;| % (self._image_path, err))&lt;BR /&gt;| wic.filemap.Error: cannot open image file '/home/jfsong/imx-yocto-bsp/buildminimal/tmp/deploy/images/imx6solosabresd/u-boot.imx': [Errno 2] No such file or directory: '/home/jfsong/imx-yocto-bsp/buildminimal/tmp/deploy/images/imx6solosabresd/u-boot.imx'&lt;BR /&gt;| WARNING: exit code 1 from a shell command.&lt;BR /&gt;| ERROR: Execution of '/home/jfsong/imx-yocto-bsp/buildminimal/tmp/work/imx6solosabresd-poky-linux-gnueabi/core-image-minimal/1.0-r0/temp/run.do_image_wic.93572' failed with exit code 1:&lt;BR /&gt;| INFO: Creating image(s)...&lt;BR /&gt;| &lt;BR /&gt;| Traceback (most recent call last):&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 127, in _open_image_file&lt;BR /&gt;| self._f_image = open(self._image_path, 'rb')&lt;BR /&gt;| FileNotFoundError: [Errno 2] No such file or directory: '/home/jfsong/imx-yocto-bsp/buildminimal/tmp/deploy/images/imx6solosabresd/u-boot.imx'&lt;BR /&gt;| &lt;BR /&gt;| During handling of the above exception, another exception occurred:&lt;BR /&gt;| &lt;BR /&gt;| Traceback (most recent call last):&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/wic", line 525, in &amp;lt;module&amp;gt;&lt;BR /&gt;| sys.exit(main(sys.argv[1:]))&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/wic", line 520, in main&lt;BR /&gt;| return hlp.invoke_subcommand(args, parser, hlp.wic_help_usage, subcommands)&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/help.py", line 83, in invoke_subcommand&lt;BR /&gt;| subcmd[0](args, usage)&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/wic", line 220, in wic_create_subcommand&lt;BR /&gt;| native_sysroot, options)&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/engine.py", line 189, in wic_create&lt;BR /&gt;| plugin.do_create()&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/plugins/imager/direct.py", line 86, in do_create&lt;BR /&gt;| self.create()&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/plugins/imager/direct.py", line 179, in create&lt;BR /&gt;| self._image.prepare(self)&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/plugins/imager/direct.py", line 354, in prepare&lt;BR /&gt;| imager.kernel_dir, imager.native_sysroot)&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/partition.py", line 174, in prepare&lt;BR /&gt;| kernel_dir, rootfs_dir, native_sysroot)&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/plugins/source/rawcopy.py", line 68, in do_prepare_partition&lt;BR /&gt;| sparse_copy(src, dst)&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 550, in sparse_copy&lt;BR /&gt;| fmap = api(src_fname)&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 532, in filemap&lt;BR /&gt;| return FilemapFiemap(image, log)&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 350, in __init__&lt;BR /&gt;| _FilemapBase.__init__(self, image, log)&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 86, in __init__&lt;BR /&gt;| self._open_image_file()&lt;BR /&gt;| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 130, in _open_image_file&lt;BR /&gt;| % (self._image_path, err))&lt;BR /&gt;| wic.filemap.Error: cannot open image file '/home/jfsong/imx-yocto-bsp/buildminimal/tmp/deploy/images/imx6solosabresd/u-boot.imx': [Errno 2] No such file or directory: '/home/jfsong/imx-yocto-bsp/buildminimal/tmp/deploy/images/imx6solosabresd/u-boot.imx'&lt;BR /&gt;| WARNING: exit code 1 from a shell command.&lt;BR /&gt;| &lt;BR /&gt;ERROR: Task (/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-core/images/core-image-minimal.bb:do_image_wic) failed with exit code '1'&lt;BR /&gt;NOTE: Tasks Summary: Attempted 2265 tasks of which 2252 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;Summary: 1 task failed:&lt;BR /&gt; /home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-core/images/core-image-minimal.bb:do_image_wic&lt;BR /&gt;Summary: There were 2 WARNING messages shown.&lt;BR /&gt;Summary: There was 1 ERROR message shown, returning a non-zero exit code.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 May 2020 04:19:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6solosabresd-do-image-wic-failed/m-p/1063829#M156326</guid>
      <dc:creator>jfsong1</dc:creator>
      <dc:date>2020-05-23T04:19:00Z</dc:date>
    </item>
    <item>
      <title>Re: imx6solosabresd do_image_wic failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6solosabresd-do-image-wic-failed/m-p/1063830#M156327</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;for "echo "UBOOT_CONFIG = \"emmc\"" &amp;gt;&amp;gt; conf/local.conf",did you add this? you want to boot up from emmc? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 May 2020 10:06:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6solosabresd-do-image-wic-failed/m-p/1063830#M156327</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2020-05-27T10:06:32Z</dc:date>
    </item>
    <item>
      <title>Re: imx6solosabresd do_image_wic failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6solosabresd-do-image-wic-failed/m-p/1063831#M156328</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, I add&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;echo "UBOOT_CONFIG = \"emmc\".&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;I want to boot up from emmc.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 May 2020 11:24:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6solosabresd-do-image-wic-failed/m-p/1063831#M156328</guid>
      <dc:creator>jfsong1</dc:creator>
      <dc:date>2020-05-27T11:24:29Z</dc:date>
    </item>
    <item>
      <title>Re: imx6solosabresd do_image_wic failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6solosabresd-do-image-wic-failed/m-p/1063832#M156329</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use "bitbake -c deploy u-boot-imx" to generate u-boot.imx. There is no error, but nothing is deployed in the directory"../tmp/deploy/images/imx6solosabresd"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;jfsong@ubuntu:~/imx-yocto-bsp/buildbase$ bitbake -c deploy u-boot-imx&lt;BR /&gt;Loading cache: 100% |############################################| Time: 0:00:01&lt;BR /&gt;Loaded 4067 entries from dependency cache.&lt;BR /&gt;NOTE: Resolving any missing task queue dependencies&lt;/P&gt;&lt;P&gt;Build Configuration:&lt;BR /&gt;BB_VERSION = "1.44.0"&lt;BR /&gt;BUILD_SYS = "x86_64-linux"&lt;BR /&gt;NATIVELSBSTRING = "ubuntu-18.04"&lt;BR /&gt;TARGET_SYS = "arm-poky-linux-gnueabi"&lt;BR /&gt;MACHINE = "imx6solosabresd"&lt;BR /&gt;DISTRO = "fsl-imx-fb"&lt;BR /&gt;DISTRO_VERSION = "5.4-zeus"&lt;BR /&gt;TUNE_FEATURES = "arm vfp cortexa9 neon thumb callconvention-hard"&lt;BR /&gt;TARGET_FPU = "hard"&lt;BR /&gt;meta &lt;BR /&gt;meta-poky = "HEAD:0275e68b0576cdefc19718e4b1977044f9f43f48"&lt;BR /&gt;meta-oe &lt;BR /&gt;meta-multimedia &lt;BR /&gt;meta-python = "HEAD:aad5b3d070cd8c58828b0975cf861d8ebc90f460"&lt;BR /&gt;meta-freescale = "HEAD:0be39721cea6e04c589a419f4bb07fabd0da6704"&lt;BR /&gt;meta-freescale-3rdparty = "HEAD:aea3771baa77e74762358ceb673d407e36637e5f"&lt;BR /&gt;meta-freescale-distro = "HEAD:ca27d12e4964d1336e662bcc60184bbff526c857"&lt;BR /&gt;meta-bsp &lt;BR /&gt;meta-sdk &lt;BR /&gt;meta-ml = "HEAD:435f5e984856a943986491fddd061734a0b9eba5"&lt;BR /&gt;meta-browser = "HEAD:5f365ef0f842ba4651efe88787cf9c63bc8b6cb3"&lt;BR /&gt;meta-rust = "HEAD:5cda04c7c2158fc982502ca1e7893f71e4ca1729"&lt;BR /&gt;meta-gnome &lt;BR /&gt;meta-networking &lt;BR /&gt;meta-filesystems = "HEAD:aad5b3d070cd8c58828b0975cf861d8ebc90f460"&lt;BR /&gt;meta-qt5 = "HEAD:432ad2aa6c3a13253fefc909faba368851d21fb1"&lt;/P&gt;&lt;P&gt;Initialising tasks: 100% |#######################################| Time: 0:00:00&lt;BR /&gt;Sstate summary: Wanted 0 Found 0 Missed 0 Current 52 (0% match, 100% complete)&lt;BR /&gt;NOTE: Executing Tasks&lt;BR /&gt;NOTE: Setscene tasks completed&lt;BR /&gt;NOTE: Tasks Summary: Attempted 402 tasks of which 402 didn't need to be rerun and all succeeded.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jun 2020 00:37:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6solosabresd-do-image-wic-failed/m-p/1063832#M156329</guid>
      <dc:creator>jfsong1</dc:creator>
      <dc:date>2020-06-02T00:37:55Z</dc:date>
    </item>
    <item>
      <title>Re: imx6solosabresd do_image_wic failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6solosabresd-do-image-wic-failed/m-p/1063833#M156330</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I haven't built 5.4.3 for imx6s, so I couldn't access the source code, since you built successfully, could you send the "sources/meta-fsl-bsp-release/imx/meta-bsp/conf/machine/boardname.conf" file to me? as I known , you need add more code in the conf file besides of "UBOOT_CONFIG = \"emmc\""&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jun 2020 08:35:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6solosabresd-do-image-wic-failed/m-p/1063833#M156330</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2020-06-02T08:35:41Z</dc:date>
    </item>
    <item>
      <title>Re: imx6solosabresd do_image_wic failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6solosabresd-do-image-wic-failed/m-p/1063834#M156331</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The conf file is "sources/meta-imx/meta-bsp/conf/machine/imx6solosabresd.conf "&amp;nbsp; . The related inc file is also attached. Thanks.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jun 2020 14:10:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6solosabresd-do-image-wic-failed/m-p/1063834#M156331</guid>
      <dc:creator>jfsong1</dc:creator>
      <dc:date>2020-06-02T14:10:00Z</dc:date>
    </item>
    <item>
      <title>Re: imx6solosabresd do_image_wic failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6solosabresd-do-image-wic-failed/m-p/1063835#M156332</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;try to add "UBOOT_CONFIG[emmc] = "mx6solosabresd_config,sdcard" in the "imx6solosabresd.conf", then build again&lt;BR /&gt;"&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jun 2020 08:18:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6solosabresd-do-image-wic-failed/m-p/1063835#M156332</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2020-06-03T08:18:38Z</dc:date>
    </item>
    <item>
      <title>Re: imx6solosabresd do_image_wic failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6solosabresd-do-image-wic-failed/m-p/1063836#M156333</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, it worked. The file "u-boot-emmc-2019.04-r0.imx" was deployed. But another problem is mfgtools downloading.&lt;/P&gt;&lt;P&gt;Firstly, I used "bitbake fsl-image-mfgtool-initramfs&amp;nbsp;" to produce firmware sucessfully.&lt;/P&gt;&lt;P&gt;Then, L4.9.88_2.0.0_mfg-tool-with-rootfs was used&amp;nbsp; to download the firmware and kernels.&amp;nbsp; But it stopped at "Jumping to OS image". There was nothing output at the debug uart1.&lt;/P&gt;&lt;P&gt;The XML configuration file is attached. I revised the original XML file for solo device downloading. The vid and pid of solo and MX6D were the same. Only the downloading files related were substituted. But it seemed faild. Please help. Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jun 2020 12:56:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6solosabresd-do-image-wic-failed/m-p/1063836#M156333</guid>
      <dc:creator>jfsong1</dc:creator>
      <dc:date>2020-06-04T12:56:04Z</dc:date>
    </item>
    <item>
      <title>Re: imx6solosabresd do_image_wic failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6solosabresd-do-image-wic-failed/m-p/1063837#M156334</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;since you built 5.4.3 image, why did you use 4.9.88 mfgtool? if you use 5.4.3 image, try to use uuu tool, for more detailed information, pls refer to user guide of 5.4.3 version&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jun 2020 08:21:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6solosabresd-do-image-wic-failed/m-p/1063837#M156334</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2020-06-10T08:21:46Z</dc:date>
    </item>
  </channel>
</rss>