<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Audio Interface in IMX7ULP with DMA in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Audio-Interface-in-IMX7ULP-with-DMA/m-p/1062979#M156236</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1) yes, refer to the schematic, imx7ulp uses wm8960, refer to the driver of wm8960, which can support up to SNDRV_PCM_FORMAT_S24_LE&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;2） one can set in dts file&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx7ulp.dtsi?h=imx_4.14.98_2.0.0_ga" rel="nofollow noopener noreferrer" title="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx7ulp.dtsi?h=imx_4.14.98_2.0.0_ga" target="_blank"&gt;imx7ulp.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;for more detailed information, pls refer to the enclose file, focus on the Chapter 7 Audio&lt;/P&gt;&lt;PRE&gt;&lt;PRE&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/PRE&gt;&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 17 Jul 2020 06:22:41 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2020-07-17T06:22:41Z</dc:date>
    <item>
      <title>Audio Interface in IMX7ULP with DMA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Audio-Interface-in-IMX7ULP-with-DMA/m-p/1062978#M156235</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Setup:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;IMX7ULP + dig mic&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Queries&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;1) Is there a way to capture audio data using DMA over I2S interface? if yes, how much max audio data(at 16k sample rate) can be captured?&lt;/P&gt;&lt;P&gt;2) Is there a way to access I2S interface from Cortex A7 processor?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking forward to a helpful response. It would be great if someone can provide sample applications for audio capturing on IMX7ULP either on M4/A7.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Vivek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 May 2020 08:43:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Audio-Interface-in-IMX7ULP-with-DMA/m-p/1062978#M156235</guid>
      <dc:creator>vivekrajpara</dc:creator>
      <dc:date>2020-05-22T08:43:50Z</dc:date>
    </item>
    <item>
      <title>Re: Audio Interface in IMX7ULP with DMA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Audio-Interface-in-IMX7ULP-with-DMA/m-p/1062979#M156236</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1) yes, refer to the schematic, imx7ulp uses wm8960, refer to the driver of wm8960, which can support up to SNDRV_PCM_FORMAT_S24_LE&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;2） one can set in dts file&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx7ulp.dtsi?h=imx_4.14.98_2.0.0_ga" rel="nofollow noopener noreferrer" title="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx7ulp.dtsi?h=imx_4.14.98_2.0.0_ga" target="_blank"&gt;imx7ulp.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;for more detailed information, pls refer to the enclose file, focus on the Chapter 7 Audio&lt;/P&gt;&lt;PRE&gt;&lt;PRE&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/PRE&gt;&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jul 2020 06:22:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Audio-Interface-in-IMX7ULP-with-DMA/m-p/1062979#M156236</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2020-07-17T06:22:41Z</dc:date>
    </item>
  </channel>
</rss>