<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックGen II .wf</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Gen-II-wf/m-p/1062862#M156218</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have the i.MX 6SLL dev board with the EBOOKDC4 EPD board.&lt;/P&gt;&lt;P&gt;Can you provide updated .wf to leverage the&amp;nbsp;Reagl/- D Support (Gen II)?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Apr 2020 22:51:10 GMT</pubDate>
    <dc:creator>ekerebel</dc:creator>
    <dc:date>2020-04-21T22:51:10Z</dc:date>
    <item>
      <title>Gen II .wf</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gen-II-wf/m-p/1062862#M156218</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have the i.MX 6SLL dev board with the EBOOKDC4 EPD board.&lt;/P&gt;&lt;P&gt;Can you provide updated .wf to leverage the&amp;nbsp;Reagl/- D Support (Gen II)?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Apr 2020 22:51:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gen-II-wf/m-p/1062862#M156218</guid>
      <dc:creator>ekerebel</dc:creator>
      <dc:date>2020-04-21T22:51:10Z</dc:date>
    </item>
    <item>
      <title>Re: Gen II .wf</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gen-II-wf/m-p/1062863#M156219</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Erwan Kerebel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you interested in a specific BSP Release? If the Regal/Regal-D algorithms are needed, the Regal/Regal-D algorithm patches must be applied to the basic BSP. The last BSP I checked that had these as controlled access packages on the Release Notes is L4.9.88_2.0.0, these controlled packages are available through a marketing representative or Distributor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Beside these patches the waveform would also change for the Regal/Regal-D algorithms from the usual 4-bit to a 5-bit pixel waveform. This should be provided by EInk as part of the support to their panels. Once you have this waveform you may open a Case asking for it to be parsed for the i.MX6SLL, but you would still need the patched BSP so that the driver can understand this waveform.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Apr 2020 20:16:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gen-II-wf/m-p/1062863#M156219</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2020-04-22T20:16:35Z</dc:date>
    </item>
  </channel>
</rss>