<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX8M mini + 2GB DDR4 boot problems in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-mini-2GB-DDR4-boot-problems/m-p/1062345#M156149</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Giacomo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if only some boards do not boot properly, this may be poor soldering issue,&lt;/P&gt;&lt;P&gt;one can try to test boards with x-ray screening.&lt;/P&gt;&lt;P&gt;Alternatively one can try to tweak drive strength and ODT parameters using&lt;/P&gt;&lt;P&gt;RPA tool on &lt;A href="https://community.nxp.com/docs/DOC-340179"&gt;i.MX 8M Family DDR Tool Release&lt;/A&gt;&amp;nbsp;&lt;BR /&gt;Check power supply noise or spikes – refering to HW Developers Guide&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX8MMHDG" target="_blank"&gt;&lt;STRONG&gt;i.MX 8M Mini Hardware Developer’s Guide&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Jul 2020 23:22:41 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2020-07-03T23:22:41Z</dc:date>
    <item>
      <title>iMX8M mini + 2GB DDR4 boot problems</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-mini-2GB-DDR4-boot-problems/m-p/1062344#M156148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;I have some booting problems on my custom board based on iMX8M mini processor.&lt;/P&gt;&lt;P&gt;We use PMIC PCA9450.&lt;/P&gt;&lt;P&gt;Processor code&amp;nbsp;MIMX8MM5DVTLZAA&lt;/P&gt;&lt;P&gt;DDR4 DRAM code (2GB total): 2 x&amp;nbsp;MT40A512M16LY-075:E&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DRAM Schematics connections is the same than EVK&amp;nbsp;SCH-35104_B1&amp;nbsp; (8MMINID4-CPU).&lt;/P&gt;&lt;P&gt;We set main voltage as follows:&lt;/P&gt;&lt;P&gt;- VDD_DRAM&amp;amp;PU = 0,9V&lt;/P&gt;&lt;P&gt;- VDD_DRAM_1V2 = 1,2V&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We produced 14 prototipes of this board. 10 boards always boot properly and they have no problems.&lt;/P&gt;&lt;P&gt;The other 4 boards do not boot properly every time. Console output is following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot SPL 2018.03-g5f7f913-dirty (Jul 03 2020 - 13:57:13 +0200)&lt;BR /&gt;DRAM PHY training for 2400MTS&lt;BR /&gt;check ddr4_pmu_train_imem code&lt;BR /&gt;check ddr4_pmu_train_imem code pass&lt;BR /&gt;check ddr4_pmu_train_dmem code&lt;BR /&gt;check ddr4_pmu_train_dmem code pass&lt;BR /&gt;Training PASS&lt;BR /&gt;DRAM PHY training for 400MTS&lt;BR /&gt;check ddr4_pmu_train_imem code&lt;BR /&gt;check ddr4_pmu_train_imem code pass&lt;BR /&gt;check ddr4_pmu_train_dmem code&lt;BR /&gt;check ddr4_pmu_train_dmem code pass&lt;BR /&gt;Training PASS&lt;BR /&gt;DRAM PHY training for 100MTS&lt;BR /&gt;check ddr4_pmu_train_imem code&lt;BR /&gt;check ddr4_pmu_train_imem code pass&lt;BR /&gt;check ddr4_pmu_train_dmem code&lt;BR /&gt;check ddr4_pmu_train_dmem code pass&lt;BR /&gt;Training FAILED&lt;BR /&gt;DRAM PHY training for 2400MTS&lt;BR /&gt;check ddr4_pmu_train_imem code&lt;BR /&gt;check ddr4_pmu_train_imem code pass&lt;BR /&gt;check ddr4_pmu_train_dmem code&lt;BR /&gt;check ddr4_pmu_train_dmem code pass&lt;BR /&gt;Training FAILED&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are 2 FAILED on DRAM test so the boot process stops.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I run RAM Stress Test "mscale_ddr_tool_v310_setup.exe" (both calibration and Stress Test) all works fine so it seems that DDR4 connections have no problems but when I use the UBOOT the booting stops after RAM tests in SPL (only on this 4 boards).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you help me?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Giacomo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jul 2020 13:11:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-mini-2GB-DDR4-boot-problems/m-p/1062344#M156148</guid>
      <dc:creator>giacomobiancala</dc:creator>
      <dc:date>2020-07-03T13:11:36Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M mini + 2GB DDR4 boot problems</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-mini-2GB-DDR4-boot-problems/m-p/1062345#M156149</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Giacomo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if only some boards do not boot properly, this may be poor soldering issue,&lt;/P&gt;&lt;P&gt;one can try to test boards with x-ray screening.&lt;/P&gt;&lt;P&gt;Alternatively one can try to tweak drive strength and ODT parameters using&lt;/P&gt;&lt;P&gt;RPA tool on &lt;A href="https://community.nxp.com/docs/DOC-340179"&gt;i.MX 8M Family DDR Tool Release&lt;/A&gt;&amp;nbsp;&lt;BR /&gt;Check power supply noise or spikes – refering to HW Developers Guide&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX8MMHDG" target="_blank"&gt;&lt;STRONG&gt;i.MX 8M Mini Hardware Developer’s Guide&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jul 2020 23:22:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-mini-2GB-DDR4-boot-problems/m-p/1062345#M156149</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-07-03T23:22:41Z</dc:date>
    </item>
  </channel>
</rss>