<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Performance query for eiq-sample-apps on imx8m nano cpu vs gpu</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Performance-query-for-eiq-sample-apps-on-imx8m-nano-cpu-vs-gpu/m-p/1062293#M156143</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am atempting to confirm my performance numbers when running the eiq demos on the imx8m nano.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am running a stock image (fsl-image-validation-imx) using the&amp;nbsp;4.14.98-2.3.0&amp;nbsp;yocto sumo manifest in the imx8mnevk board. I am using the opencv obj_recognition_cpp example code&amp;nbsp;modified to set the Preferable target either set to CPU or OPENCL&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;edit to force hardware openCL shown below&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&amp;nbsp; //Net net = readNetFromTensorflow(model, config);&lt;BR /&gt;&amp;nbsp; net = readNetFromCaffe(config, model);&lt;BR /&gt;&amp;nbsp; net.setPreferableTarget(cv::dnn::DNN_TARGET_OPENCL);&lt;BR /&gt;}&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When using cpu processing I get an Inference fps of about 3 fps&lt;/P&gt;&lt;P&gt;When using the gpu for open cl I get an Inference fps of arround 1/12 (0.08) fps&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are these the expected performance levels for running open cl on the gpu or have I misconfigured something?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Tyler&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Jun 2020 20:56:05 GMT</pubDate>
    <dc:creator>tyler_ward</dc:creator>
    <dc:date>2020-06-17T20:56:05Z</dc:date>
    <item>
      <title>Performance query for eiq-sample-apps on imx8m nano cpu vs gpu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Performance-query-for-eiq-sample-apps-on-imx8m-nano-cpu-vs-gpu/m-p/1062293#M156143</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am atempting to confirm my performance numbers when running the eiq demos on the imx8m nano.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am running a stock image (fsl-image-validation-imx) using the&amp;nbsp;4.14.98-2.3.0&amp;nbsp;yocto sumo manifest in the imx8mnevk board. I am using the opencv obj_recognition_cpp example code&amp;nbsp;modified to set the Preferable target either set to CPU or OPENCL&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;edit to force hardware openCL shown below&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&amp;nbsp; //Net net = readNetFromTensorflow(model, config);&lt;BR /&gt;&amp;nbsp; net = readNetFromCaffe(config, model);&lt;BR /&gt;&amp;nbsp; net.setPreferableTarget(cv::dnn::DNN_TARGET_OPENCL);&lt;BR /&gt;}&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When using cpu processing I get an Inference fps of about 3 fps&lt;/P&gt;&lt;P&gt;When using the gpu for open cl I get an Inference fps of arround 1/12 (0.08) fps&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are these the expected performance levels for running open cl on the gpu or have I misconfigured something?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Tyler&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jun 2020 20:56:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Performance-query-for-eiq-sample-apps-on-imx8m-nano-cpu-vs-gpu/m-p/1062293#M156143</guid>
      <dc:creator>tyler_ward</dc:creator>
      <dc:date>2020-06-17T20:56:05Z</dc:date>
    </item>
    <item>
      <title>Re: Performance query for eiq-sample-apps on imx8m nano cpu vs gpu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Performance-query-for-eiq-sample-apps-on-imx8m-nano-cpu-vs-gpu/m-p/1062294#M156144</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Tyler,&lt;/P&gt;&lt;P&gt;1. you can follow &lt;SPAN style="text-decoration: underline;"&gt;chapter 15 Application Programing Recommandations&lt;/SPAN&gt; in the&amp;nbsp; iMX_Graphics_User's_Guide to optimize the apps.&lt;/P&gt;&lt;P&gt;2. Customer can use vProfiler and vAnalyzer ( &lt;A class="" data-content-finding="Community" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdesign%2Fdevelopment-boards%2Fi.mx-evaluation-and-development-boards%2Fsabre-for-automotive-infotainment-based-on-the-i.mx-6-series%3ARDIMX6SABREAUTO" rel="nofollow" target="_blank"&gt;VivanteVTK&lt;/A&gt;) to get a&amp;nbsp;more detailed GPU performance, including GPU utilization, pixel rate, GPU idle cycles, and so on. For more info, please refer to &lt;SPAN style="text-decoration: underline;"&gt;vProfiler and vAnalyzer&lt;/SPAN&gt;&amp;nbsp;in the Graphics User Guide documentation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;When GPU load is very high, other GPU apps will be slower. So, users must balance GPU resource among different GPU apps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jun 2020 16:02:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Performance-query-for-eiq-sample-apps-on-imx8m-nano-cpu-vs-gpu/m-p/1062294#M156144</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2020-06-18T16:02:58Z</dc:date>
    </item>
  </channel>
</rss>