<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 iMX25 - internal RAM used by ROM boot loader</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX25-internal-RAM-used-by-ROM-boot-loader/m-p/224560#M15614</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am writing some simple &amp;amp; short test programs that I would like to load into the internal RAM of the iMX257 by using the ROM boot loader via the Serial Download Protocol (SDP) on UART1.&amp;nbsp; I would like to know what (if any) memory regions within the internal RAM are used by the boot loader.&amp;nbsp; The 128kbyte internal ram is mapped from 0x7800 0000 to 0x7801 FFFF with the last 64 bytes used for the interrupt vector table.&amp;nbsp; Unfortunately I can not find any information in the reference manual concerning the boot loader's memory usage. I would like to place my programs in a region separate from what may be used by the ROM boot loader.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One other question...&lt;/P&gt;&lt;P&gt;From the reference manual, the boot loader uses the watchdog with a 90 second reset period.&amp;nbsp; Does the watchdog get turned off when an application file is loaded via SDP and executed?&amp;nbsp; Or is the application responsible for turning off (or resetting) the watchdog timer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ralph&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Jul 2013 23:52:51 GMT</pubDate>
    <dc:creator>ralphlang</dc:creator>
    <dc:date>2013-07-25T23:52:51Z</dc:date>
    <item>
      <title>iMX25 - internal RAM used by ROM boot loader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX25-internal-RAM-used-by-ROM-boot-loader/m-p/224560#M15614</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am writing some simple &amp;amp; short test programs that I would like to load into the internal RAM of the iMX257 by using the ROM boot loader via the Serial Download Protocol (SDP) on UART1.&amp;nbsp; I would like to know what (if any) memory regions within the internal RAM are used by the boot loader.&amp;nbsp; The 128kbyte internal ram is mapped from 0x7800 0000 to 0x7801 FFFF with the last 64 bytes used for the interrupt vector table.&amp;nbsp; Unfortunately I can not find any information in the reference manual concerning the boot loader's memory usage. I would like to place my programs in a region separate from what may be used by the ROM boot loader.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One other question...&lt;/P&gt;&lt;P&gt;From the reference manual, the boot loader uses the watchdog with a 90 second reset period.&amp;nbsp; Does the watchdog get turned off when an application file is loaded via SDP and executed?&amp;nbsp; Or is the application responsible for turning off (or resetting) the watchdog timer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ralph&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jul 2013 23:52:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX25-internal-RAM-used-by-ROM-boot-loader/m-p/224560#M15614</guid>
      <dc:creator>ralphlang</dc:creator>
      <dc:date>2013-07-25T23:52:51Z</dc:date>
    </item>
  </channel>
</rss>