<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: I2C Address Register</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I2C-Address-Register/m-p/1061019#M156013</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tetsuya&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;I think that I2C_IADR should be set only when making i.MX8Mmini an I2C slave device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you are right.&lt;/P&gt;&lt;P&gt;One can look at i2c master example in uboot:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/uboot-imx/tree/drivers/i2c/mxc_i2c.c?h=imx_v2019.04_4.19.35_1.1.0" title="https://source.codeaurora.org/external/imx/uboot-imx/tree/drivers/i2c/mxc_i2c.c?h=imx_v2019.04_4.19.35_1.1.0"&gt;mxc_i2c.c\i2c\drivers - uboot-imx - i.MX U-Boot&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Apr 2020 10:30:07 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2020-04-06T10:30:07Z</dc:date>
    <item>
      <title>I2C Address Register</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I2C-Address-Register/m-p/1061018#M156012</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;I have a question about {16.1.4.1 Initialization sequence} in i.MX 8M Mini Applications Processor Reference Manual, Rev. 2, 08/2019.&lt;BR /&gt;I am wondering about the following:&lt;BR /&gt;"2.Update the address in the (I2C_IADR) to define its slave address (address can range from 0 to 0x7f)."&lt;BR /&gt;What should I set in the I2C_IADR register when I consider to make the i.MX8Mmini an I2C master?&lt;BR /&gt;Is the transfer destination slave ID correct?&lt;BR /&gt;I think that I2C_IADR should be set only when making i.MX8Mmini an I2C slave device.&lt;BR /&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tetsuya.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 05 Apr 2020 15:13:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I2C-Address-Register/m-p/1061018#M156012</guid>
      <dc:creator>t-sugiyama</dc:creator>
      <dc:date>2020-04-05T15:13:09Z</dc:date>
    </item>
    <item>
      <title>Re: I2C Address Register</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I2C-Address-Register/m-p/1061019#M156013</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tetsuya&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;I think that I2C_IADR should be set only when making i.MX8Mmini an I2C slave device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you are right.&lt;/P&gt;&lt;P&gt;One can look at i2c master example in uboot:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/uboot-imx/tree/drivers/i2c/mxc_i2c.c?h=imx_v2019.04_4.19.35_1.1.0" title="https://source.codeaurora.org/external/imx/uboot-imx/tree/drivers/i2c/mxc_i2c.c?h=imx_v2019.04_4.19.35_1.1.0"&gt;mxc_i2c.c\i2c\drivers - uboot-imx - i.MX U-Boot&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Apr 2020 10:30:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I2C-Address-Register/m-p/1061019#M156013</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-04-06T10:30:07Z</dc:date>
    </item>
  </channel>
</rss>