<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX7 linux kernel freezing? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX7-linux-kernel-freezing/m-p/1060205#M155876</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am having an issue running Linux kernel on a custom hardware board, and I'm reaching out to get help. It seems that Linux is starting correctly, but then ends up freezing/stalling at some point, as I am not able to do anything beyond this point, including writing to terminal. This same build, however, works on the IMX7 Sabre board using only a different DDR config.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have debugged it so far that I know that the stalling happens in &lt;STRONG&gt;cpu_startup_entry()&lt;/STRONG&gt; function in &lt;STRONG&gt;linux-imx/init/main.c&lt;/STRONG&gt;. Furthermore, I have attached the minicom output, where the stalling happens after the very last command.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this definitely a DDR configuration related issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Apr 2020 12:15:22 GMT</pubDate>
    <dc:creator>jjamesson</dc:creator>
    <dc:date>2020-04-21T12:15:22Z</dc:date>
    <item>
      <title>IMX7 linux kernel freezing?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7-linux-kernel-freezing/m-p/1060205#M155876</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am having an issue running Linux kernel on a custom hardware board, and I'm reaching out to get help. It seems that Linux is starting correctly, but then ends up freezing/stalling at some point, as I am not able to do anything beyond this point, including writing to terminal. This same build, however, works on the IMX7 Sabre board using only a different DDR config.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have debugged it so far that I know that the stalling happens in &lt;STRONG&gt;cpu_startup_entry()&lt;/STRONG&gt; function in &lt;STRONG&gt;linux-imx/init/main.c&lt;/STRONG&gt;. Furthermore, I have attached the minicom output, where the stalling happens after the very last command.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this definitely a DDR configuration related issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Apr 2020 12:15:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7-linux-kernel-freezing/m-p/1060205#M155876</guid>
      <dc:creator>jjamesson</dc:creator>
      <dc:date>2020-04-21T12:15:22Z</dc:date>
    </item>
    <item>
      <title>Re: IMX7 linux kernel freezing?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7-linux-kernel-freezing/m-p/1060206#M155877</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Status update:&lt;/P&gt;&lt;P&gt;I checked the DDR configuration with the stress tester tool, and it passed the test. So this problem is unlikely a DDR configuration problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Apr 2020 13:24:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7-linux-kernel-freezing/m-p/1060206#M155877</guid>
      <dc:creator>jjamesson</dc:creator>
      <dc:date>2020-04-22T13:24:44Z</dc:date>
    </item>
    <item>
      <title>Re: IMX7 linux kernel freezing?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7-linux-kernel-freezing/m-p/1060207#M155878</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Issue resolved!&lt;BR /&gt;I fixed it by removing any irrelevant peripherals in the device tree for Linux.&lt;/P&gt;&lt;P&gt;Thank you, and this issue can be closed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Apr 2020 18:54:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7-linux-kernel-freezing/m-p/1060207#M155878</guid>
      <dc:creator>jjamesson</dc:creator>
      <dc:date>2020-04-22T18:54:47Z</dc:date>
    </item>
    <item>
      <title>Re: IMX7 linux kernel freezing?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7-linux-kernel-freezing/m-p/1060208#M155879</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello James Jamesson,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for updating this thread and letting us know what the problem was! Hopefully it may help other community users.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Apr 2020 21:20:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7-linux-kernel-freezing/m-p/1060208#M155879</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2020-04-22T21:20:23Z</dc:date>
    </item>
  </channel>
</rss>