<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Have wayland use /dev/fb1</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Have-wayland-use-dev-fb1/m-p/1060169#M155869</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello richc128,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The kernel command line configuration for display may vary according the kernel release. You will find the correct parameters at release notes contained at the BSP package you're using. For example, for BSP release the video command line is: video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666 video=mxcfb1:dev=hdmi, 1920x1080M@60,if=RGB24&lt;/P&gt;&lt;P&gt;If you switch the fb0 with fb1, Linux will switch the primary display. For example, if lcd was the /dev/fb0, it will now be the /dev/fb1. all this is done in uboot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Aug 2020 13:32:07 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2020-08-26T13:32:07Z</dc:date>
    <item>
      <title>Have wayland use /dev/fb1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Have-wayland-use-dev-fb1/m-p/1060168#M155868</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have two displays in my boundary devices i.mx8m mini system. The first is HDMI (via the DSI and a converter) and an ssd1306 oled via i2c.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The oled is getting mapped to /dev/fb0 and the dsi/hdmi to /dev/fb1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a way to swap these?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or, is there a way to make wayland use /dev/fb1?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Aug 2020 00:17:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Have-wayland-use-dev-fb1/m-p/1060168#M155868</guid>
      <dc:creator>richc128</dc:creator>
      <dc:date>2020-08-25T00:17:13Z</dc:date>
    </item>
    <item>
      <title>Re: Have wayland use /dev/fb1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Have-wayland-use-dev-fb1/m-p/1060169#M155869</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello richc128,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The kernel command line configuration for display may vary according the kernel release. You will find the correct parameters at release notes contained at the BSP package you're using. For example, for BSP release the video command line is: video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666 video=mxcfb1:dev=hdmi, 1920x1080M@60,if=RGB24&lt;/P&gt;&lt;P&gt;If you switch the fb0 with fb1, Linux will switch the primary display. For example, if lcd was the /dev/fb0, it will now be the /dev/fb1. all this is done in uboot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Aug 2020 13:32:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Have-wayland-use-dev-fb1/m-p/1060169#M155869</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2020-08-26T13:32:07Z</dc:date>
    </item>
  </channel>
</rss>