<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx-yocto-L4.14.98_2.0.0_ga下载错误？ in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx-yocto-L4-14-98-2-0-0-ga%E4%B8%8B%E8%BD%BD%E9%94%99%E8%AF%AF/m-p/1059941#M155846</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;以前做过后面新版本也会不一样的，建议是全部删除了，重新做repo sync, 你这个是明显没有下载完整，我之前也碰到过，重新下载就好了，可能网络问题的问题导致没有下载完全，如果你拷贝过来可以用也行，但不知道是否会影响你接下去的编译&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Aug 2020 05:06:12 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2020-08-26T05:06:12Z</dc:date>
    <item>
      <title>imx-yocto-L4.14.98_2.0.0_ga下载错误？</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-yocto-L4-14-98-2-0-0-ga%E4%B8%8B%E8%BD%BD%E9%94%99%E8%AF%AF/m-p/1059938#M155843</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;以前一直用fsl-yocto-L4.1.15_2.0.0-ga，现在想看看imx-yocto-L4.14.98_2.0.0_ga怎么样，所以想编译imx-yocto-L4.14.98_2.0.0_ga，然而当我repo sync后发现在imx-yocto-bsp目录下只有sources文件夹，而fsl-setup-release.sh,README-IMXBSP,README,setup-environment这些都没有。是哪里的问题了？？还是本来就是这样？&lt;/P&gt;&lt;P&gt;我的系统是ubuntu 16.04 LTS&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Aug 2020 02:34:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-yocto-L4-14-98-2-0-0-ga%E4%B8%8B%E8%BD%BD%E9%94%99%E8%AF%AF/m-p/1059938#M155843</guid>
      <dc:creator>longbin</dc:creator>
      <dc:date>2020-08-24T02:34:09Z</dc:date>
    </item>
    <item>
      <title>Re: imx-yocto-L4.14.98_2.0.0_ga下载错误？</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-yocto-L4-14-98-2-0-0-ga%E4%B8%8B%E8%BD%BD%E9%94%99%E8%AF%AF/m-p/1059939#M155844</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;it seems your building is incomplete, try to delete the whole folder, then build this bsp from the first step as yocto user guide mentions&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Aug 2020 08:58:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-yocto-L4-14-98-2-0-0-ga%E4%B8%8B%E8%BD%BD%E9%94%99%E8%AF%AF/m-p/1059939#M155844</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2020-08-25T08:58:43Z</dc:date>
    </item>
    <item>
      <title>Re: imx-yocto-L4.14.98_2.0.0_ga下载错误？</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-yocto-L4-14-98-2-0-0-ga%E4%B8%8B%E8%BD%BD%E9%94%99%E8%AF%AF/m-p/1059940#M155845</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;非常感谢你的回复，我已经删除过2次，也是按文档的步骤来做的，只是setting up the repo utility没有做，毕竟我以前已经下载过，不知道问题出在哪里？我现在只能从source内拷贝fsl-setup-release.sh,setup-environment到imx-yocto-bsp目录下，现在编译也完成。&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Aug 2020 00:59:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-yocto-L4-14-98-2-0-0-ga%E4%B8%8B%E8%BD%BD%E9%94%99%E8%AF%AF/m-p/1059940#M155845</guid>
      <dc:creator>longbin</dc:creator>
      <dc:date>2020-08-26T00:59:55Z</dc:date>
    </item>
    <item>
      <title>Re: imx-yocto-L4.14.98_2.0.0_ga下载错误？</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-yocto-L4-14-98-2-0-0-ga%E4%B8%8B%E8%BD%BD%E9%94%99%E8%AF%AF/m-p/1059941#M155846</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;以前做过后面新版本也会不一样的，建议是全部删除了，重新做repo sync, 你这个是明显没有下载完整，我之前也碰到过，重新下载就好了，可能网络问题的问题导致没有下载完全，如果你拷贝过来可以用也行，但不知道是否会影响你接下去的编译&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Aug 2020 05:06:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-yocto-L4-14-98-2-0-0-ga%E4%B8%8B%E8%BD%BD%E9%94%99%E8%AF%AF/m-p/1059941#M155846</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2020-08-26T05:06:12Z</dc:date>
    </item>
    <item>
      <title>Re: imx-yocto-L4.14.98_2.0.0_ga下载错误？</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-yocto-L4-14-98-2-0-0-ga%E4%B8%8B%E8%BD%BD%E9%94%99%E8%AF%AF/m-p/1059942#M155847</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;非常感谢，我现在已经编译好了，删除再下载太麻烦了。所以先看看，有问题再说。我主要是想用实时linux方案Xenomai，编译也完成，等待手头项目完成后再试试这个系统，看看实时性怎么样。&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Aug 2020 07:47:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-yocto-L4-14-98-2-0-0-ga%E4%B8%8B%E8%BD%BD%E9%94%99%E8%AF%AF/m-p/1059942#M155847</guid>
      <dc:creator>longbin</dc:creator>
      <dc:date>2020-08-26T07:47:37Z</dc:date>
    </item>
    <item>
      <title>Re: imx-yocto-L4.14.98_2.0.0_ga下载错误？</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-yocto-L4-14-98-2-0-0-ga%E4%B8%8B%E8%BD%BD%E9%94%99%E8%AF%AF/m-p/1059943#M155848</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;OK, 那就行&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Aug 2020 07:50:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-yocto-L4-14-98-2-0-0-ga%E4%B8%8B%E8%BD%BD%E9%94%99%E8%AF%AF/m-p/1059943#M155848</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2020-08-26T07:50:56Z</dc:date>
    </item>
    <item>
      <title>Re: imx-yocto-L4.14.98_2.0.0_ga下载错误？</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-yocto-L4-14-98-2-0-0-ga%E4%B8%8B%E8%BD%BD%E9%94%99%E8%AF%AF/m-p/1059944#M155849</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;有可能是repo版本的问题，可以看看repo版本，以及manifest存在差异&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Aug 2020 09:25:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-yocto-L4-14-98-2-0-0-ga%E4%B8%8B%E8%BD%BD%E9%94%99%E8%AF%AF/m-p/1059944#M155849</guid>
      <dc:creator>songhongliang</dc:creator>
      <dc:date>2020-08-26T09:25:24Z</dc:date>
    </item>
    <item>
      <title>Re: imx-yocto-L4.14.98_2.0.0_ga下载错误？</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-yocto-L4-14-98-2-0-0-ga%E4%B8%8B%E8%BD%BD%E9%94%99%E8%AF%AF/m-p/1059945#M155850</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;非常不好意思，我对repo不熟，我不知道怎么查看repo版本。因为google不能上，这个repo是很多年前从国内网站下载的。&lt;/P&gt;&lt;P&gt;manifest差异问题，我对比过&lt;A href="https://source.codeaurora.org/external/imx/imx-manifest/tree/?h=imx-linux-sumo下的imx-4.14.98-2.0.0_ga.xml与我本机.repo下manifest.xml，它们没有不同。"&gt;https://source.codeaurora.org/external/imx/imx-manifest/tree/?h=imx-linux-sumo下的imx-4.14.98-2.0.0_ga.xml与我本机.repo下manifest.xml，它们没有不同。&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Aug 2020 01:52:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-yocto-L4-14-98-2-0-0-ga%E4%B8%8B%E8%BD%BD%E9%94%99%E8%AF%AF/m-p/1059945#M155850</guid>
      <dc:creator>longbin</dc:creator>
      <dc:date>2020-08-28T01:52:22Z</dc:date>
    </item>
  </channel>
</rss>