<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx8mm NAND boot issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-NAND-boot-issue/m-p/1059449#M155769</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried in U-Boot console nand torture command for testing NAND and simple RAM mtest and they have both passed. Also tried dumping mtd0 partition that contains boot structures and data and compared between working and non working board, they are the same.&lt;/P&gt;&lt;P&gt;Do note that boards that don't boot from NAND, do work correctly when only SPL is booted from SD (mtd0 wiped clean, boards switch to SD manufacture boot) and then when the SPL loads from SD it fetches rest of the image from NAND.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I've also tried to be sure that our built imx-boot image is not corrupted is using imx-boot (imx-boot-imx8mmddr4evk-nand.bin-flash_ddr4_evk) from NXPs L5.4.24-2.1.0_images_MX8MMEVK archive.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;On boards that DO boot with our images from NAND, SPL is loaded and it stops on DDR training which is expected since our board is different then EVK&lt;/LI&gt;&lt;LI&gt;On boards that DON'T boot with our images from NAND there is also no output on serial console when using EVK image&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suspect that problem when booting from NAND is prior to actually entering SPL and that board never reaches it or initializes RAM (there is no output on console at all) and that maybe SPL image data gets corrupted while being read from NAND and copied to TCML? Is there some way to test that?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Damjan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Jul 2020 08:36:02 GMT</pubDate>
    <dc:creator>damjan_frantal</dc:creator>
    <dc:date>2020-07-21T08:36:02Z</dc:date>
    <item>
      <title>imx8mm NAND boot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-NAND-boot-issue/m-p/1059447#M155767</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we have custom boards based on i.MX 8M Mini Quad CPU (MIMX8MM6CVTKZAA) that are being booted from RAW NAND. NAND chip used is: Micron MT29F8G08ABBCAH4.&lt;/P&gt;&lt;P&gt;Boards are being flashed by &lt;SPAN style="font-size: 15px;"&gt;mfgtools&lt;/SPAN&gt; USB booting the board and then using imx-kobs as FBK command. Flash image is generated with Yocto and signed with CST tool. Bootloader is U-Boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The issue is that some of the boards do boot from NAND after successful flash and restart, while others don't. Image and flashing procedure for boards is the same, as are board electrical components and layout. Only difference on boards that we could find so far is CPU lot number written on CPU chip:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;boards that &lt;STRONG&gt;DO&lt;/STRONG&gt; boot from NAND: &lt;SPAN style="font-size: 11.0pt;"&gt;&lt;STRONG&gt;SBCN1934H&lt;/STRONG&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;boards that &lt;STRONG&gt;DON'T&lt;/STRONG&gt; boot from NAND: &lt;SPAN style="font-size: 11.0pt;"&gt;&lt;STRONG&gt;SBBT1925F&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Fuses that are programed on boards are SRK Hash, GP10, GP11, and BOOT CFG0 fuses.&lt;/SPAN&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;BOOT CFG0 is programed with 0x10003400 (NAND boot select, BT_FUSE_SEL, NAND 64 Pages in Block)&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Device is not locked for the moment.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;ROM Log Events (&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN12853.pdf" rel="nofollow noopener noreferrer" title="https://www.nxp.com/docs/en/application-note/AN12853.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12853.pdf&lt;/A&gt;) for:&lt;/SPAN&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Devices that &lt;STRONG&gt;DO&lt;/STRONG&gt; boot from NAND:&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;PRE class="language-none line-numbers"&gt;&lt;CODE&gt;0090E558 = E0000000 10000000 22000000 41000000
0090E568 = 50000000 60000000 80000000 0000009C
0090E578 = 81000000 000000D7 90000000 00000200
0090E588 = 91000000 00000105 90000000 00000202
0090E598 = 91000000 000005A9 A0000000 000000F0
0090E5A8 = 000061A4 C0000000 007E1000 00006253‍‍‍‍‍‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Devices that &lt;STRONG&gt;DON'T&lt;/STRONG&gt; boot from NAND:&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;PRE class="language-none line-numbers"&gt;&lt;CODE&gt;0090E558 = E0000000 10000000 22000000 41000000
0090E568 = 50000000 60000000 80000000 00000072
0090E578 = 81000000 00000099 90000000 00000200
0090E588 = 91000000 000000C7 90000000 00000202
0090E598 = 91000000 0000056A A0000000 FFC01833
0090E5A8 = 000032D6 C0000000 007E1000 00003385‍‍‍‍‍‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;SPAN style="font-size: 15px;"&gt;Seems that Image authentication failed with status 0xFFC01833 (from HAB4 API document), output&lt;SPAN style="left: 217.233px; top: 787.322px; font-family: sans-serif; transform: scaleX(0.956118);"&gt; is the same regardless of SRK Hash fuses programed or not&lt;/SPAN&gt;:&lt;/SPAN&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI style="text-align: justify;"&gt;&lt;SPAN style="font-size: 15px;"&gt;33 - HAB_FAILURE&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI style="text-align: justify;"&gt;&lt;SPAN style="font-size: 15px;"&gt;18 - HAB_INV_SIGNATURE&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI style="text-align: justify;"&gt;&lt;SPAN style="font-size: 15px;"&gt;C0 - HAB_CTX_COMMAND&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI style="text-align: justify;"&gt;&lt;SPAN style="font-size: 15px;"&gt;FF - &lt;SPAN style="left: 217.233px; top: 787.322px; font-family: sans-serif; transform: scaleX(0.956118);"&gt;HAB_ENG_SW&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;SPAN style="transform: scaleX(0.956118); top: 787.322px; left: 217.233px; font-size: 15px; font-family: sans-serif;"&gt;After failed authentication board still proceeds to boot from NAND since it is not locked but fails and reboots.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="transform: scaleX(0.956118); top: 787.322px; left: 217.233px; font-size: 15px; font-family: sans-serif;"&gt;Same image does work correctly when used for booting from USB (serial downloader) or SD card (tested using SD Manufacture boot).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="transform: scaleX(0.956118); top: 787.322px; left: 217.233px; font-size: 15px; font-family: sans-serif;"&gt;imx-kobs output (mtd0 size is 6 MiB):&lt;/SPAN&gt;&lt;/P&gt;&lt;PRE class="language-none line-numbers"&gt;&lt;CODE&gt;Start Cmd:FBK: ucmd source /mytmpfs/mtd.sh; cd /tmp; kobs-ng init -x -v --chip_0_device_path=/dev/mtd0 /mytmpfs/boot
MTD CONFIG:
  chip_0_device_path = "/dev/mtd0"
  chip_1_device_path = "(null)"
  search_exponent = 2
  data_setup_time = 80
  data_hold_time = 60
  address_setup_time = 25
  data_sample_time = 6
  row_address_size = 3
  column_address_size = 2
  read_command_code1 = 0
  read_command_code2 = 48
  boot_stream_major_version = 1
  boot_stream_minor_version = 0
  boot_stream_sub_version = 0
  ncb_version = 3
  boot_stream_1_address = 0
  boot_stream_2_address = 0
  secondary_boot_stream_off_in_MB = 64
         -- We add the 1k-padding to the uboot.
.tmp_kobs_ng: verifying using key '00000000000000000000000000000000'
.tmp_kobs_ng: is a valid bootstream for key '00000000000000000000000000000000'
mtd: use new bch layout raw access mode
mtd: opening: "/dev/mtd0"
NFC geometry :
        ECC Strength       : 8
        Page Size in Bytes : 4210
        Metadata size      : 10
        ECC Chunk Size in byte : 512
        ECC Chunk count        : 8
        Block Mark Byte Offset : 3995
        Block Mark Bit Offset  : 0
====================================================
mtd: opened '/dev/mtd0' - '(null)'
mtd: max_boot_stream_size_in_bytes = 2097152
mtd: boot_stream_size_in_bytes = 253952
mtd: boot_stream_size_in_pages = 62
mtd: extra_boot_stream_size_in_bytes =253952
mtd: extra_boot_stream_size_in_pages = 62
mtd: #1 0x00200000 - 0x00400000 (0x0023e000)
mtd: #2 0x00400000 - 0x00600000 (0x0043e000)
FCB
  m_u32Checksum = 0x00000000
  m_u32FingerPrint = 0x20424346
  m_u32Version = 0x01000000
  m_NANDTiming.m_u8DataSetup = 80
  m_NANDTiming.m_u8DataHold = 60
  m_NANDTiming.m_u8AddressSetup = 25
  m_NANDTiming.m_u8DSAMPLE_TIME = 6
  m_u32PageDataSize = 4096
  m_u32TotalPageSize = 4320
  m_u32SectorsPerBlock = 64
  m_u32NumberOfNANDs = 0
  m_u32TotalInternalDie = 0
  m_u32CellType = 0
  m_u32EccBlockNEccType = 4
  m_u32EccBlock0Size = 512
  m_u32EccBlockNSize = 512
  m_u32EccBlock0EccType = 4
  m_u32MetadataBytes = 10
  m_u32NumEccBlocksPerPage = 7
  m_u32EccBlockNEccLevelSDK = 0
  m_u32EccBlock0SizeSDK = 0
  m_u32EccBlockNSizeSDK = 0
  m_u32EccBlock0EccLevelSDK = 0
  m_u32NumEccBlocksPerPageSDK = 0
  m_u32MetadataBytesSDK = 0
  m_u32EraseThreshold = 0
  m_u32Firmware1_startingPage = 512
  m_u32Firmware2_startingPage = 1024
  m_u32PagesInFirmware1 = 62
  m_u32PagesInFirmware2 = 62
  m_u32DBBTSearchAreaStartAddress = 256
  m_u32BadBlockMarkerByte = 3995
  m_u32BadBlockMarkerStartBit = 0
  m_u32BBMarkerPhysicalOffset = 4096
  m_u32BCHType = 0
  m_NANDTMTiming.m_u32TMTiming2_ReadLatency = 0
  m_NANDTMTiming.m_u32TMTiming2_PreambleDelay = 0
  m_NANDTMTiming.m_u32TMTiming2_CEDelay = 0
  m_NANDTMTiming.m_u32TMTiming2_PostambleDelay = 0
  m_NANDTMTiming.m_u32TMTiming2_CmdAddPause = 0
  m_NANDTMTiming.m_u32TMTiming2_DataPause = 0
  m_NANDTMTiming.m_u32TMSpeed = 0
  m_NANDTMTiming.m_u32TMTiming1_BusyTimeout = 0
  m_u32DISBBM = 0
  m_u32BBMarkerPhysicalOffsetInSpareData = 0
  m_u32OnfiSyncEnable = 0
  m_NANDONFITiming.m_u32ONFISpeed = 0
  m_NANDONFITiming.m_u32ONFITiming_ReadLatency = 0
  m_NANDONFITiming.m_u32ONFITiming_CEDelay = 0
  m_NANDONFITiming.m_u32ONFITiming_PreambleDelay = 0
  m_NANDONFITiming.m_u32ONFITiming_PostambleDelay = 0
  m_NANDONFITiming.m_u32ONFITiming_CmdAddPause = 0
  m_NANDONFITiming.m_u32ONFITiming_DataPause = 0
  m_NANDONFITiming.m_u32ONFITiming_BusyTimeout = 0
  m_u32DISBBSearch = 0
  m_u32RandomizerEnable = 0
  m_u32ReadRetryEnable = 0
  m_u32ReadRetrySeqLength = 0
DBBT
  m_u32Checksum = 0x00000000
  m_u32FingerPrint = 0x54424244
  m_u32Version = 0x01000000
  m_u32DBBTNumOfPages = 0
Firmware: image #0 @ 0x200000 size 0x3e000 - available 0x200000
Firmware: image #1 @ 0x400000 size 0x3e000 - available 0x200000
Extra Firmware: image #0 @ 0x240000 size 0x3e000 - available 0x1c0000
Firmware: image #1 @ 0x440000 size 0x3e000 - available 0x1c0000
-------------- Start to write the [ FCB ] -----
mtd: erasing @0:0x0-0x40000
mtd: Writing FCB0 [ @0:0x0 ] (10e0) *
mtd: erasing @0:0x40000-0x80000
mtd: Writing FCB1 [ @0:0x40000 ] (10e0) *
mtd: erasing @0:0x80000-0xc0000
mtd: Writing FCB2 [ @0:0x80000 ] (10e0) *
mtd: erasing @0:0xc0000-0x100000
mtd: Writing FCB3 [ @0:0xc0000 ] (10e0) *
mtd_commit_bcb(FCB): status 0

-------------- Start to write the [ DBBT ] -----
mtd: erasing @0:0x100000-0x140000
mtd: Writing DBBT0 [ @0:0x100000 ] (1000) *
mtd: erasing @0:0x140000-0x180000
mtd: Writing DBBT1 [ @0:0x140000 ] (1000) *
mtd: erasing @0:0x180000-0x1c0000
mtd: Writing DBBT2 [ @0:0x180000 ] (1000) *
mtd: erasing @0:0x1c0000-0x200000
mtd: Writing DBBT3 [ @0:0x1c0000 ] (1000) *
mtd_commit_bcb(DBBT): status 0

---------- Start to write the [ .tmp_kobs_ng ]----
mtd: Writting .tmp_kobs_ng: #0 @0: 0x00200000 - 0x0023e000
mtd: erasing @0:0x200000-0x240000
mtd: We write one page for save guard. *
mtd: Writting .tmp_kobs_ng: #1 @0: 0x00400000 - 0x0043e000
mtd: erasing @0:0x400000-0x440000
mtd: We write one page for save guard. *
write the second part of boot stream
---------- Start to write the [ .tmp_kobs_ng ]----
mtd: Writting .tmp_kobs_ng: #0 @0: 0x00240000 - 0x0027e000
mtd: Writting .tmp_kobs_ng: #0 @0: 0x00240000 - 0x0027e000
mtd: erasing @0:0x240000-0x280000
mtd: We write one page for save guard. *
mtd: Writting .tmp_kobs_ng: #1 @0: 0x00440000 - 0x0047e000
mtd: Writting .tmp_kobs_ng: #1 @0: 0x00440000 - 0x0047e000
mtd: erasing @0:0x440000-0x480000
mtd: We write one page for save guard. *‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="transform: scaleX(0.956118); top: 787.322px; left: 217.233px; font-size: 15px; font-family: sans-serif;"&gt;Is there some difference in IMX8 lots regarding the NAND boot or we are missing some fuse config?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="transform: scaleX(0.956118); top: 787.322px; left: 217.233px; font-size: 15px; font-family: sans-serif;"&gt;BR,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="transform: scaleX(0.956118); top: 787.322px; left: 217.233px; font-size: 15px; font-family: sans-serif;"&gt;Damjan&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jul 2020 12:44:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-NAND-boot-issue/m-p/1059447#M155767</guid>
      <dc:creator>damjan_frantal</dc:creator>
      <dc:date>2020-07-17T12:44:00Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mm NAND boot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-NAND-boot-issue/m-p/1059448#M155768</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/damjan.frantal@zenitel.com"&gt;damjan.frantal@zenitel.com&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; have You tried the memory test on the boards?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jul 2020 06:40:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-NAND-boot-issue/m-p/1059448#M155768</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2020-07-21T06:40:54Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mm NAND boot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-NAND-boot-issue/m-p/1059449#M155769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried in U-Boot console nand torture command for testing NAND and simple RAM mtest and they have both passed. Also tried dumping mtd0 partition that contains boot structures and data and compared between working and non working board, they are the same.&lt;/P&gt;&lt;P&gt;Do note that boards that don't boot from NAND, do work correctly when only SPL is booted from SD (mtd0 wiped clean, boards switch to SD manufacture boot) and then when the SPL loads from SD it fetches rest of the image from NAND.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I've also tried to be sure that our built imx-boot image is not corrupted is using imx-boot (imx-boot-imx8mmddr4evk-nand.bin-flash_ddr4_evk) from NXPs L5.4.24-2.1.0_images_MX8MMEVK archive.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;On boards that DO boot with our images from NAND, SPL is loaded and it stops on DDR training which is expected since our board is different then EVK&lt;/LI&gt;&lt;LI&gt;On boards that DON'T boot with our images from NAND there is also no output on serial console when using EVK image&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suspect that problem when booting from NAND is prior to actually entering SPL and that board never reaches it or initializes RAM (there is no output on console at all) and that maybe SPL image data gets corrupted while being read from NAND and copied to TCML? Is there some way to test that?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Damjan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jul 2020 08:36:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-NAND-boot-issue/m-p/1059449#M155769</guid>
      <dc:creator>damjan_frantal</dc:creator>
      <dc:date>2020-07-21T08:36:02Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mm NAND boot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-NAND-boot-issue/m-p/1059450#M155770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/damjan.frantal@zenitel.com"&gt;damjan.frantal@zenitel.com&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; perhaps PCB issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Aug 2020 07:58:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-NAND-boot-issue/m-p/1059450#M155770</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2020-08-11T07:58:43Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mm NAND boot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-NAND-boot-issue/m-p/1263521#M172730</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/119376"&gt;@damjan_frantal&lt;/a&gt;&amp;nbsp;!&lt;/P&gt;&lt;P&gt;Did you find a way to solve the issue you had?&lt;/P&gt;&lt;P&gt;I'm facing a similar problem, and the lot number of the imx8mm assembled on my board starts with SBB. Unfortunately, I don't have boards with other lot numbers to test.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I also tried the&amp;nbsp;&lt;SPAN&gt;imx-boot-imx8mmddr4evk-nand.bin-flash_ddr4_evk from the binary images pack and got the same results.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Fernando.&lt;/P&gt;</description>
      <pubDate>Fri, 16 Apr 2021 11:30:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-NAND-boot-issue/m-p/1263521#M172730</guid>
      <dc:creator>fernando_lopes</dc:creator>
      <dc:date>2021-04-16T11:30:32Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mm NAND boot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-NAND-boot-issue/m-p/1264147#M172801</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;we switched to newer batches of CPU on more recent devices which boot correctly from NAND in our case.&lt;/P&gt;&lt;P&gt;For older CPU batch that had issues booting from NAND on our boards, we booted SPL from SD card which then loads U-Boot and rest of the image from NAND.&lt;/P&gt;&lt;P&gt;Change in SPL to always try booting from NAND:&lt;/P&gt;&lt;PRE&gt;&lt;SPAN class="line"&gt;&lt;SPAN class="gh"&gt;diff --git a/common/spl/spl.c b/common/spl/spl.c&lt;/SPAN&gt;&lt;/SPAN&gt;
&lt;SPAN class="line"&gt;&lt;SPAN class="gh"&gt;index 88d4b8a9bf..26af38f59b 100644&lt;/SPAN&gt;&lt;/SPAN&gt;
&lt;SPAN class="line"&gt;&lt;SPAN class="gd"&gt;--- a/common/spl/spl.c&lt;/SPAN&gt;&lt;/SPAN&gt;
&lt;SPAN class="line"&gt;&lt;SPAN class="gi"&gt;+++ b/common/spl/spl.c&lt;/SPAN&gt;&lt;/SPAN&gt;
&lt;SPAN class="line"&gt;&lt;SPAN class="p"&gt;@@ -488,6 +488,7 @@&lt;/SPAN&gt; int spl_init(void)&lt;/SPAN&gt;
&lt;SPAN class="line"&gt; __weak void board_boot_order(u32 *spl_boot_list)&lt;/SPAN&gt;
&lt;SPAN class="line"&gt; {&lt;/SPAN&gt;
&lt;SPAN class="line"&gt; 	spl_boot_list[0] = spl_boot_device();&lt;/SPAN&gt;
&lt;SPAN class="line"&gt;&lt;SPAN class="gi"&gt;+	spl_boot_list[1] = BOOT_DEVICE_NAND;&lt;/SPAN&gt;&lt;/SPAN&gt;
&lt;SPAN class="line"&gt; }&lt;/SPAN&gt;
 
&lt;SPAN class="line"&gt; static struct spl_image_loader *spl_ll_find_loader(uint boot_device)&lt;/SPAN&gt;
&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 19 Apr 2021 07:54:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-NAND-boot-issue/m-p/1264147#M172801</guid>
      <dc:creator>damjan_frantal</dc:creator>
      <dc:date>2021-04-19T07:54:22Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mm NAND boot issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-NAND-boot-issue/m-p/1264294#M172819</link>
      <description>&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Mon, 19 Apr 2021 10:55:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-NAND-boot-issue/m-p/1264294#M172819</guid>
      <dc:creator>fernando_lopes</dc:creator>
      <dc:date>2021-04-19T10:55:49Z</dc:date>
    </item>
  </channel>
</rss>