<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx8   uuu in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8-uuu/m-p/1059438#M155766</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can not use the&amp;nbsp; B0 binaries to C0 board. &lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN12770.pdf" title="https://www.nxp.com/docs/en/application-note/AN12770.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN12770.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The configuration files and there is a separate MACHINE for each of the two silicon versions supported:&lt;/P&gt;&lt;P&gt;imx8qxpmek for the B0 silicon&lt;/P&gt;&lt;P&gt;imx8qxpc0mek for the C0 silicon&lt;/P&gt;&lt;P&gt;Bake the recipes you need. For how to build for C0 you can see this &lt;A href="https://community.nxp.com/thread/531451"&gt;How to build C0 binary for imx8qxp-mek on imx-4.14.98-2.3.0 branch?&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Jul 2020 07:31:58 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2020-07-09T07:31:58Z</dc:date>
    <item>
      <title>imx8   uuu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8-uuu/m-p/1059437#M155765</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/114500iB979174E2AE57533/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;各位，如上图，是基于yocto_4.14.98_2.3.0编译得到的文件，&lt;/P&gt;&lt;P&gt;我这里有两块imx8的板，两块板的DDR，电源管理，EMMC都相同，&lt;/P&gt;&lt;P&gt;板1：旧的PCB板贴的是B版本的imx8芯片&lt;/P&gt;&lt;P&gt;板2：新做的PCB板贴的是C版本的imx8芯片&lt;/P&gt;&lt;P&gt;用uuu可以烧录“板1”，但不能烧录“板2”，错误如下，请问大概问题出在哪里？谢谢。&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/114503i799B6A2718A11CAB/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jul 2020 02:23:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8-uuu/m-p/1059437#M155765</guid>
      <dc:creator>383826029</dc:creator>
      <dc:date>2020-07-03T02:23:16Z</dc:date>
    </item>
    <item>
      <title>Re: imx8   uuu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8-uuu/m-p/1059438#M155766</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can not use the&amp;nbsp; B0 binaries to C0 board. &lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN12770.pdf" title="https://www.nxp.com/docs/en/application-note/AN12770.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN12770.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The configuration files and there is a separate MACHINE for each of the two silicon versions supported:&lt;/P&gt;&lt;P&gt;imx8qxpmek for the B0 silicon&lt;/P&gt;&lt;P&gt;imx8qxpc0mek for the C0 silicon&lt;/P&gt;&lt;P&gt;Bake the recipes you need. For how to build for C0 you can see this &lt;A href="https://community.nxp.com/thread/531451"&gt;How to build C0 binary for imx8qxp-mek on imx-4.14.98-2.3.0 branch?&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jul 2020 07:31:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8-uuu/m-p/1059438#M155766</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2020-07-09T07:31:58Z</dc:date>
    </item>
  </channel>
</rss>