<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: RPMSG-specific DTS</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RPMSG-specific-DTS/m-p/1059079#M155726</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Thierry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;rpmsg specific dts settings can be found in&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8qm-mek.dts?h=imx_5.4.3_2.0.0" title="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8qm-mek.dts?h=imx_5.4.3_2.0.0"&gt;imx8qm-mek.dts\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8qm.dtsi?h=imx_5.4.3_2.0.0" title="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8qm.dtsi?h=imx_5.4.3_2.0.0"&gt;imx8qm.dtsi\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;do not require a specific linux device tree for sdk.&lt;/P&gt;&lt;P&gt;Need for these rpmsg settings can be analysed in driver sources described in&lt;/P&gt;&lt;P&gt;RPMSG Chapter in Linux Manual included in &lt;A class="" href="https://www.nxp.com/webapp/Download?colCode=L5.4.3_1.0.0_LINUX_DOCS" target="_blank"&gt;Linux 5.4.3_1.0.0 Documentation&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Jun 2020 23:29:54 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2020-06-17T23:29:54Z</dc:date>
    <item>
      <title>RPMSG-specific DTS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RPMSG-specific-DTS/m-p/1059078#M155725</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;Running the RPMSG demos from the SDK requires a specific Linux device tree. If I get it correctly, the differences are as follow:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;the INTMUX of both M4 cores are disabled&lt;/LI&gt;&lt;LI&gt;the RPMSG shared memory doubles in size from 64KB to 128KB for each core&lt;/LI&gt;&lt;LI&gt;two remote virtual devices per M4 core&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;The demos run fine with those settings. However, I'd like to better understand why those changes are required. Would somebody please elaborate?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;--&lt;/P&gt;&lt;P&gt;TD&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jun 2020 13:12:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RPMSG-specific-DTS/m-p/1059078#M155725</guid>
      <dc:creator>EmbeddedExpertise</dc:creator>
      <dc:date>2020-06-17T13:12:49Z</dc:date>
    </item>
    <item>
      <title>Re: RPMSG-specific DTS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RPMSG-specific-DTS/m-p/1059079#M155726</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Thierry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;rpmsg specific dts settings can be found in&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8qm-mek.dts?h=imx_5.4.3_2.0.0" title="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8qm-mek.dts?h=imx_5.4.3_2.0.0"&gt;imx8qm-mek.dts\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8qm.dtsi?h=imx_5.4.3_2.0.0" title="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8qm.dtsi?h=imx_5.4.3_2.0.0"&gt;imx8qm.dtsi\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;do not require a specific linux device tree for sdk.&lt;/P&gt;&lt;P&gt;Need for these rpmsg settings can be analysed in driver sources described in&lt;/P&gt;&lt;P&gt;RPMSG Chapter in Linux Manual included in &lt;A class="" href="https://www.nxp.com/webapp/Download?colCode=L5.4.3_1.0.0_LINUX_DOCS" target="_blank"&gt;Linux 5.4.3_1.0.0 Documentation&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jun 2020 23:29:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RPMSG-specific-DTS/m-p/1059079#M155726</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-06-17T23:29:54Z</dc:date>
    </item>
  </channel>
</rss>