<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Debug port and cortex-A apps</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Debug-port-and-cortex-A-apps/m-p/1057771#M155551</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;ravi.kohli&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it is possible to create image with enabled Cortex-A and Cortex-M4 in&lt;/P&gt;&lt;P&gt;various combinations as described on&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-343178"&gt;i.MX8 Boot process and creating a bootable image&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For uart one can check:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/uboot-imx/tree/include/configs/imx8qm_mek.h?h=imx_v2020.04_5.4.24_2.1.0" title="https://source.codeaurora.org/external/imx/uboot-imx/tree/include/configs/imx8qm_mek.h?h=imx_v2020.04_5.4.24_2.1.0"&gt;imx8qm_mek.h\configs\include - uboot-imx - i.MX U-Boot&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/imx8qm_mek/imx8qm_mek.c?h=imx_v2020.04_5.4.24_2.1.0" title="https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/imx8qm_mek/imx8qm_mek.c?h=imx_v2020.04_5.4.24_2.1.0"&gt;imx8qm_mek.c\imx8qm_mek\freescale\board - uboot-imx - i.MX U-Boot&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/uboot-imx/tree/arch/arm/mach-imx/imx8/cpu.c?h=imx_v2020.04_5.4.24_2.1.0" title="https://source.codeaurora.org/external/imx/uboot-imx/tree/arch/arm/mach-imx/imx8/cpu.c?h=imx_v2020.04_5.4.24_2.1.0"&gt;cpu.c\imx8\mach-imx\arm\arch - uboot-imx - i.MX U-Boot&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;example of starting m4 from linux&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imxsupport/m4ctrl/about/" title="https://source.codeaurora.org/external/imxsupport/m4ctrl/about/"&gt;m4ctrl - M4 Control Tool for i.MX platforms&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 04 Aug 2020 04:27:16 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2020-08-04T04:27:16Z</dc:date>
    <item>
      <title>Debug port and cortex-A apps</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Debug-port-and-cortex-A-apps/m-p/1057770#M155550</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have SCU (CM4) debug port output from the UART and 2xCM4 UART serial access as well for the i.MX8QM EVK. Is there any serial output accessible from the AP cores (4xA53 and 2xA72) ? In other words, I don't see UART access for the AP cores. Is there some way for checking the start of any of the AP cores (A53 or A72) from the debug port or the SCU FW ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Aug 2020 00:06:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Debug-port-and-cortex-A-apps/m-p/1057770#M155550</guid>
      <dc:creator>ravi_kohli</dc:creator>
      <dc:date>2020-08-04T00:06:15Z</dc:date>
    </item>
    <item>
      <title>Re: Debug port and cortex-A apps</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Debug-port-and-cortex-A-apps/m-p/1057771#M155551</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;ravi.kohli&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it is possible to create image with enabled Cortex-A and Cortex-M4 in&lt;/P&gt;&lt;P&gt;various combinations as described on&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-343178"&gt;i.MX8 Boot process and creating a bootable image&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For uart one can check:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/uboot-imx/tree/include/configs/imx8qm_mek.h?h=imx_v2020.04_5.4.24_2.1.0" title="https://source.codeaurora.org/external/imx/uboot-imx/tree/include/configs/imx8qm_mek.h?h=imx_v2020.04_5.4.24_2.1.0"&gt;imx8qm_mek.h\configs\include - uboot-imx - i.MX U-Boot&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/imx8qm_mek/imx8qm_mek.c?h=imx_v2020.04_5.4.24_2.1.0" title="https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/imx8qm_mek/imx8qm_mek.c?h=imx_v2020.04_5.4.24_2.1.0"&gt;imx8qm_mek.c\imx8qm_mek\freescale\board - uboot-imx - i.MX U-Boot&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/uboot-imx/tree/arch/arm/mach-imx/imx8/cpu.c?h=imx_v2020.04_5.4.24_2.1.0" title="https://source.codeaurora.org/external/imx/uboot-imx/tree/arch/arm/mach-imx/imx8/cpu.c?h=imx_v2020.04_5.4.24_2.1.0"&gt;cpu.c\imx8\mach-imx\arm\arch - uboot-imx - i.MX U-Boot&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;example of starting m4 from linux&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imxsupport/m4ctrl/about/" title="https://source.codeaurora.org/external/imxsupport/m4ctrl/about/"&gt;m4ctrl - M4 Control Tool for i.MX platforms&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Aug 2020 04:27:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Debug-port-and-cortex-A-apps/m-p/1057771#M155551</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-08-04T04:27:16Z</dc:date>
    </item>
    <item>
      <title>Re: Debug port and cortex-A apps</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Debug-port-and-cortex-A-apps/m-p/1057772#M155552</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Igor.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Aug 2020 04:34:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Debug-port-and-cortex-A-apps/m-p/1057772#M155552</guid>
      <dc:creator>ravi_kohli</dc:creator>
      <dc:date>2020-08-04T04:34:18Z</dc:date>
    </item>
  </channel>
</rss>