<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX8 Nano SD / eMMC boot - pins usage? Datasheet Error</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Nano-SD-eMMC-boot-pins-usage-Datasheet-Error/m-p/1057462#M155520</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to understand which pins, and for what purpose, the iMX8 Nano uses for SD/eMMC boot. Specifically the USDHC-3 port. Our product will boot from an eMMC on USDHC-3. It appears the datasheet and the reference manual don't agree on pin usage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The datasheet lists these pins:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="nano-ds.JPG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/110500i8D72106EF4CCBA5B/image-size/large?v=v2&amp;amp;px=999" role="button" title="nano-ds.JPG" alt="nano-ds.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I've highlighted the pins that don't seem to agree with the reference manual (below).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Reference Manual lists a different set of pins:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="nano-rm.JPG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/110397i1F8BCEF644CDFAC4/image-size/large?v=v2&amp;amp;px=999" role="button" title="nano-rm.JPG" alt="nano-rm.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;As can be seen, some of these pins are the same as listed in the datasheet, some are different. I've highlighted the pins that are different.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As an example: If I look at the datasheet, I would believe the NAND_READY_B pin is used for the eMMC/SD reset. But if I look at the reference manual it says the GPIO1_IO09 pin. Either is potentially possible:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="nano-rm2.JPG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/110398iB43696D5B36361D7/image-size/large?v=v2&amp;amp;px=999" role="button" title="nano-rm2.JPG" alt="nano-rm2.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the correct list of pins and functionality for USDHC3 boot?&lt;/P&gt;&lt;P&gt;Thanks very much.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Aug 2020 18:37:24 GMT</pubDate>
    <dc:creator>frank_vanhooft</dc:creator>
    <dc:date>2020-08-24T18:37:24Z</dc:date>
    <item>
      <title>i.MX8 Nano SD / eMMC boot - pins usage? Datasheet Error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Nano-SD-eMMC-boot-pins-usage-Datasheet-Error/m-p/1057462#M155520</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to understand which pins, and for what purpose, the iMX8 Nano uses for SD/eMMC boot. Specifically the USDHC-3 port. Our product will boot from an eMMC on USDHC-3. It appears the datasheet and the reference manual don't agree on pin usage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The datasheet lists these pins:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="nano-ds.JPG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/110500i8D72106EF4CCBA5B/image-size/large?v=v2&amp;amp;px=999" role="button" title="nano-ds.JPG" alt="nano-ds.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I've highlighted the pins that don't seem to agree with the reference manual (below).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Reference Manual lists a different set of pins:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="nano-rm.JPG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/110397i1F8BCEF644CDFAC4/image-size/large?v=v2&amp;amp;px=999" role="button" title="nano-rm.JPG" alt="nano-rm.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;As can be seen, some of these pins are the same as listed in the datasheet, some are different. I've highlighted the pins that are different.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As an example: If I look at the datasheet, I would believe the NAND_READY_B pin is used for the eMMC/SD reset. But if I look at the reference manual it says the GPIO1_IO09 pin. Either is potentially possible:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="nano-rm2.JPG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/110398iB43696D5B36361D7/image-size/large?v=v2&amp;amp;px=999" role="button" title="nano-rm2.JPG" alt="nano-rm2.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the correct list of pins and functionality for USDHC3 boot?&lt;/P&gt;&lt;P&gt;Thanks very much.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Aug 2020 18:37:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Nano-SD-eMMC-boot-pins-usage-Datasheet-Error/m-p/1057462#M155520</guid>
      <dc:creator>frank_vanhooft</dc:creator>
      <dc:date>2020-08-24T18:37:24Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8 Nano SD / eMMC boot - pins usage? Datasheet Error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Nano-SD-eMMC-boot-pins-usage-Datasheet-Error/m-p/1057463#M155521</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm updating this post after we received a reply from NXP support. They said the datasheet is wrong, and the reference manual is correct.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note this also means the USDHC3 pins are spread over two different power domains (which is a bit unfortunate, but at least we know).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Aug 2020 15:55:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Nano-SD-eMMC-boot-pins-usage-Datasheet-Error/m-p/1057463#M155521</guid>
      <dc:creator>frank_vanhooft</dc:creator>
      <dc:date>2020-08-27T15:55:01Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8 Nano SD / eMMC boot - pins usage? Datasheet Error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Nano-SD-eMMC-boot-pins-usage-Datasheet-Error/m-p/1057464#M155522</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please refer to the Reference Manual in this point.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Aug 2020 03:26:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Nano-SD-eMMC-boot-pins-usage-Datasheet-Error/m-p/1057464#M155522</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2020-08-28T03:26:38Z</dc:date>
    </item>
  </channel>
</rss>