<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Set touchscreen available area</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Set-touchscreen-available-area/m-p/1056605#M155403</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks brother.&lt;/P&gt;&lt;P&gt;So do you have other ways to set the touch screen avalible area, such as setting&amp;nbsp;coordinate and size?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Jul 2020 01:33:07 GMT</pubDate>
    <dc:creator>Mihan</dc:creator>
    <dc:date>2020-07-21T01:33:07Z</dc:date>
    <item>
      <title>Set touchscreen available area</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Set-touchscreen-available-area/m-p/1056603#M155401</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all&lt;/P&gt;&lt;P&gt;I set two monitors for imx6 before&amp;nbsp;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/537453"&gt;Multiple monitors&lt;/A&gt;, now their display functions work well.&lt;/P&gt;&lt;P&gt;But the touchscreen can move the cursor between two monitors, so I follow&amp;nbsp;&lt;A href="https://wiki.archlinux.org/index.php/Touchscreen#Using_a_touchscreen_in_a_multi-head_setup"&gt;Using a touchscreen in a multi-head setup&lt;/A&gt;&amp;nbsp;and try to set it.&lt;/P&gt;&lt;P&gt;But I find the screen shown by 'xrandr' is only one as follow:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;root@imx6qsabresd:~# xrandr &lt;BR /&gt;Screen 0: minimum 240 x 240, current 1024 x 768, maximum 8192 x 8192&lt;BR /&gt;DISP3 BG connected 1024x768+0+0 (normal left inverted right x axis y axis) 0mm x 0mm&lt;BR /&gt; 1024x768_60.00 59.92*+&lt;BR /&gt; U:1024x768p-59 59.91 +&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;What's this 'DISP3 BG'? Why there is only one screen?&amp;nbsp;&lt;/P&gt;&lt;P&gt;The GPU is&amp;nbsp;vivante maybe (I see the default xorg.conf is vivante). the latest configuration has uploaded on the last topic above.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I try to find the registration of this 'DISP3 BG'. It's on 'drivers/video/fbdev/mxc/mxc_ipuv3_fb.c' (also i find it on 'drivers/media/platform/mxc/capture/mxc_v4l2_capture.c' and 'drivers/video/fbdev/mx3fb.c').&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Later I print some graphics information:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;root@imx6qsabresd:~# cat /sys/class/graphics/fb*/fsl_disp_dev_property &lt;BR /&gt;ldb&lt;BR /&gt;overlay&lt;BR /&gt;hdmi&lt;BR /&gt;root@imx6qsabresd:~# cat /sys/class/graphics/fb*/fsl_disp_property &lt;BR /&gt;2-layer-fb-bg&lt;BR /&gt;2-layer-fb-fg&lt;BR /&gt;1-layer-fb&lt;BR /&gt;root@imx6qsabresd:~#&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I think maybe the fb2 should be the&amp;nbsp;&lt;SPAN&gt;MEM_BG_SYNC no the&amp;nbsp;&lt;/SPAN&gt;MEM_DC_SYNC so that xrandr can detect two screens.&lt;/P&gt;&lt;P&gt;What should I do?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Mihan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jul 2020 07:14:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Set-touchscreen-available-area/m-p/1056603#M155401</guid>
      <dc:creator>Mihan</dc:creator>
      <dc:date>2020-07-17T07:14:27Z</dc:date>
    </item>
    <item>
      <title>Re: Set touchscreen available area</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Set-touchscreen-available-area/m-p/1056604#M155402</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Current xrand is supported however there are some features that are not working well, as example this and the acceleration by GPU, this is marked as a bug.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jul 2020 14:48:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Set-touchscreen-available-area/m-p/1056604#M155402</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2020-07-20T14:48:10Z</dc:date>
    </item>
    <item>
      <title>Re: Set touchscreen available area</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Set-touchscreen-available-area/m-p/1056605#M155403</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks brother.&lt;/P&gt;&lt;P&gt;So do you have other ways to set the touch screen avalible area, such as setting&amp;nbsp;coordinate and size?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jul 2020 01:33:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Set-touchscreen-available-area/m-p/1056605#M155403</guid>
      <dc:creator>Mihan</dc:creator>
      <dc:date>2020-07-21T01:33:07Z</dc:date>
    </item>
  </channel>
</rss>