<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: The entry of data link layer(OS:linux) ,when using command &amp;quot;ping www.baidu.com&amp;quot;</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/The-entry-of-data-link-layer-OS-linux-when-using-command-quot/m-p/1056596#M155400</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Johnny,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The ping function is included as part of the networking utilities included on the Yocto BSPs from Open Embedded.&lt;/P&gt;&lt;P&gt;You can find more information for this package if you look at the fping recipe inside Yocto. Inside the recipe you can find the repository for this package’s source code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 07 May 2020 20:27:16 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2020-05-07T20:27:16Z</dc:date>
    <item>
      <title>The entry of data link layer(OS:linux) ,when using command "ping www.baidu.com"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-entry-of-data-link-layer-OS-linux-when-using-command-quot/m-p/1056595#M155399</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Platform:Imx8qxp&lt;/P&gt;&lt;P&gt;Environment:Yocto&lt;/P&gt;&lt;P&gt;OS:linux&lt;/P&gt;&lt;P&gt;Question:&lt;/P&gt;&lt;P&gt;I want to know the entry of data link layer(OS:linux) ,when using command "ping &lt;A href="http://www.baidu.com&amp;quot;,because"&gt;www.baidu.com",because&lt;/A&gt;&amp;nbsp;I want to add some log to check ping data package(ping command lose package sometimes).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can somebody help me?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BRs&lt;/P&gt;&lt;P&gt;Johnny&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 May 2020 10:34:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-entry-of-data-link-layer-OS-linux-when-using-command-quot/m-p/1056595#M155399</guid>
      <dc:creator>liuyonggang</dc:creator>
      <dc:date>2020-05-07T10:34:23Z</dc:date>
    </item>
    <item>
      <title>Re: The entry of data link layer(OS:linux) ,when using command "ping www.baidu.com"</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-entry-of-data-link-layer-OS-linux-when-using-command-quot/m-p/1056596#M155400</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Johnny,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The ping function is included as part of the networking utilities included on the Yocto BSPs from Open Embedded.&lt;/P&gt;&lt;P&gt;You can find more information for this package if you look at the fping recipe inside Yocto. Inside the recipe you can find the repository for this package’s source code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 May 2020 20:27:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-entry-of-data-link-layer-OS-linux-when-using-command-quot/m-p/1056596#M155400</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2020-05-07T20:27:16Z</dc:date>
    </item>
  </channel>
</rss>