<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX6 GPU Libraries in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-GPU-Libraries/m-p/1056300#M155346</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kein&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;linux gpu drivers are described in Linux Manual included in &lt;A href="https://www.nxp.com/webapp/Download?colCode=L5.4.3_1.0.0_LINUX_DOCS" target="_blank"&gt;Linux 5.4.3_1.0.0 Documentation&lt;/A&gt;&lt;/P&gt;&lt;P&gt;memory requirements: &lt;A href="https://community.nxp.com/thread/445874"&gt;https://community.nxp.com/thread/445874&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For baremetal gpu one can look at sdk example (folder..apps/gpu_demo/)&lt;/P&gt;&lt;P&gt;file 1.1.0_iMX6_Platform_SDK.zip on &lt;A href="https://community.nxp.com/thread/432859"&gt;SMP Enable in IMX6&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;or open source efforts &lt;A class="link-titled" href="https://github.com/etnaviv" title="https://github.com/etnaviv"&gt;Etnaviv · GitHub&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Jun 2020 04:25:37 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2020-06-17T04:25:37Z</dc:date>
    <item>
      <title>iMX6 GPU Libraries</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-GPU-Libraries/m-p/1056299#M155345</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am creating a bare metal application (not using Linux). I want to use the GPU libraries as the GPUs are why I picked the iMX6 Quad, but Linux doesn't meet my needs. Are the libraries written as to be independent of the OS (can be used independent of Linux)? I noticed that in the Graphics User's Guide that there is a Linux kernel section to the libraries where as a minimum they request memory. What else needs to be done in the kernel?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jun 2020 02:10:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-GPU-Libraries/m-p/1056299#M155345</guid>
      <dc:creator>ogj</dc:creator>
      <dc:date>2020-06-17T02:10:40Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 GPU Libraries</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-GPU-Libraries/m-p/1056300#M155346</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kein&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;linux gpu drivers are described in Linux Manual included in &lt;A href="https://www.nxp.com/webapp/Download?colCode=L5.4.3_1.0.0_LINUX_DOCS" target="_blank"&gt;Linux 5.4.3_1.0.0 Documentation&lt;/A&gt;&lt;/P&gt;&lt;P&gt;memory requirements: &lt;A href="https://community.nxp.com/thread/445874"&gt;https://community.nxp.com/thread/445874&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For baremetal gpu one can look at sdk example (folder..apps/gpu_demo/)&lt;/P&gt;&lt;P&gt;file 1.1.0_iMX6_Platform_SDK.zip on &lt;A href="https://community.nxp.com/thread/432859"&gt;SMP Enable in IMX6&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;or open source efforts &lt;A class="link-titled" href="https://github.com/etnaviv" title="https://github.com/etnaviv"&gt;Etnaviv · GitHub&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jun 2020 04:25:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-GPU-Libraries/m-p/1056300#M155346</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-06-17T04:25:37Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 GPU Libraries</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-GPU-Libraries/m-p/1056301#M155347</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the response. I’ll check this out.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jun 2020 06:05:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-GPU-Libraries/m-p/1056301#M155347</guid>
      <dc:creator>ogj</dc:creator>
      <dc:date>2020-06-17T06:05:55Z</dc:date>
    </item>
  </channel>
</rss>