<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: H264 over RTP - missing h264 sequences in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/H264-over-RTP-missing-h264-sequences/m-p/1056081#M155332</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Joan,&lt;/P&gt;&lt;P&gt;we use a Trizeps7&amp;nbsp;SOM module from Keith &amp;amp; Koep. The Ethernet PHY is already on this module. We only fit a RJ45 plug with coils to our base board.&lt;/P&gt;&lt;P&gt;Therefore we use a modified Keith &amp;amp; Koep BSP.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 28 Aug 2020 06:01:57 GMT</pubDate>
    <dc:creator>MicMoba</dc:creator>
    <dc:date>2020-08-28T06:01:57Z</dc:date>
    <item>
      <title>H264 over RTP - missing h264 sequences</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/H264-over-RTP-missing-h264-sequences/m-p/1056079#M155330</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I can show a h264 stream over RTP on my display by using GStreamer. Bandwith usage is approximately at 25Mb.&lt;/P&gt;&lt;P&gt;When I connect a second streaming source to my display the video is juddering. But only one stream. The Bandwith usage is approximately at 50Mb.&lt;/P&gt;&lt;P&gt;To exclude the VPU I extracted from every streaming source a h264-file and copied to my display. Then I playback both files simultaniosly by using GStreamer. It works well.&lt;/P&gt;&lt;P&gt;So the receiving of RTP frames and the rtph264depay was left. To check this I recorded rtpdumps with rtpdump-tool form rtptools.&lt;/P&gt;&lt;P&gt;I recorded a stream fom source 1 and source 2 while both streams are running. Then I recorded a from each stream a single dump.&lt;/P&gt;&lt;P&gt;I copied the dumps to my PC. Then I playback the dumps with rtpplay also from rtptools to localhost and trace these dumps with Wireshark.&lt;/P&gt;&lt;P&gt;I decoded the UDP frames as RTP-&amp;gt;H264 and looked at the H264 Seq-Number. (Is shown in the info field of each frame). I noticed that the seq-numbers of all good working streams were always increased by 1. At the stream where I noticed juddering the seq-numbers sometimes increased by 10 or 20 or something between&amp;nbsp; (See attached Image No.19 to No.20, Seq jumps from 55256 to 55269)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So my question. Is it allowed that the seq-numbers increased by more than 1?&lt;/P&gt;&lt;P&gt;Is there a lost of frames in my network stack?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks Michael&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EDIT: 03.08.2020 - 15:26&lt;/P&gt;&lt;P&gt;I did further investigations. I think it has something to do with udp frame drops. When I look at /proc/net/udp I can see a lot of drops when both streams are running. It can be an explaination for the missing seq-numbers but I don't understand why only seq-numbers of one stream are missing and not of both.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EDIT: 04.08.2020 - 9:16&lt;/P&gt;&lt;P&gt;I did tcpdump for both UDP ports on my display and analyse them with Wireshark. I saw that packets of the one stream that also has missing h264 seq-numbers were droped.&lt;/P&gt;&lt;P&gt;In my opinion this is the proof that it is an issue with the network stack. But I can't understand why only frames of one stream were droped.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Aug 2020 08:50:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/H264-over-RTP-missing-h264-sequences/m-p/1056079#M155330</guid>
      <dc:creator>MicMoba</dc:creator>
      <dc:date>2020-08-03T08:50:12Z</dc:date>
    </item>
    <item>
      <title>Re: H264 over RTP - missing h264 sequences</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/H264-over-RTP-missing-h264-sequences/m-p/1056080#M155331</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;what board and bsp version are you talking about?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Aug 2020 04:42:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/H264-over-RTP-missing-h264-sequences/m-p/1056080#M155331</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2020-08-28T04:42:38Z</dc:date>
    </item>
    <item>
      <title>Re: H264 over RTP - missing h264 sequences</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/H264-over-RTP-missing-h264-sequences/m-p/1056081#M155332</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Joan,&lt;/P&gt;&lt;P&gt;we use a Trizeps7&amp;nbsp;SOM module from Keith &amp;amp; Koep. The Ethernet PHY is already on this module. We only fit a RJ45 plug with coils to our base board.&lt;/P&gt;&lt;P&gt;Therefore we use a modified Keith &amp;amp; Koep BSP.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Aug 2020 06:01:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/H264-over-RTP-missing-h264-sequences/m-p/1056081#M155332</guid>
      <dc:creator>MicMoba</dc:creator>
      <dc:date>2020-08-28T06:01:57Z</dc:date>
    </item>
    <item>
      <title>Re: H264 over RTP - missing h264 sequences</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/H264-over-RTP-missing-h264-sequences/m-p/1156808#M162283</link>
      <description>&lt;P&gt;I'm not familiar with this board, what nxp board did you board design based on? could you reproduce this issue on nxp board?&lt;/P&gt;</description>
      <pubDate>Tue, 22 Sep 2020 08:39:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/H264-over-RTP-missing-h264-sequences/m-p/1156808#M162283</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2020-09-22T08:39:17Z</dc:date>
    </item>
  </channel>
</rss>