<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX6UL OCRAM in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-OCRAM/m-p/1055096#M155192</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Paul,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt; According to app note AN12077 (Using the i.MX RT FlexRAM) OCRAM is used during boot:&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;The minimum configuration of OCRAM is 128 KB I guess is for MX6UL.&amp;nbsp; This is required due to ROM code requires at least &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;64 KB of RAM for its execution (device dependent).&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="" style="min-height: 8pt; padding: 0px;"&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;A data-content-finding="Community" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fapplication-note%2FAN12077.pdf" rel="nofollow" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12077.pdf&lt;/A&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="" style="min-height: 8pt; padding: 0px;"&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; Customers can use OCRAM (after boot) as needed, in particular - for buffers.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; App note AN12437 (i.MX RT Series Performance Optimization) states, that "OCRAM shows higher &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;performance than TCM when accessed by DMA, while lower performance when accessed by MCU core.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt; The reason is that OCRAM and DMA are in this same bus fabric, with less latency during the access." &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="" style="min-height: 8pt; padding: 0px;"&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;A data-content-finding="Community" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fapplication-note%2FAN12437.pdf" rel="nofollow" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12437.pdf&lt;/A&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="" style="min-height: 8pt; padding: 0px;"&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P class="" style="min-height: 8pt; padding: 0px;"&gt;Of course, you can use a small OS-less applications running in OCRAM only not using DRAM. However, the functionality of such applications seems to be very limited due to small amount of memory available. On the other hand, it is possible to run the code directly from, for example, external parallel NOR flash using the External Memory Interface module and use OCRAM for stack/data only. The limitations here are: 1) relatively slow EIM operation and 2) relatively small address space of up to 128MBytes.&lt;/P&gt;&lt;P class="" style="min-height: 8pt; padding: 0px;"&gt;&lt;/P&gt;&lt;P class="" style="min-height: 8pt; padding: 0px;"&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Apr 2020 14:21:29 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2020-04-22T14:21:29Z</dc:date>
    <item>
      <title>IMX6UL OCRAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-OCRAM/m-p/1055095#M155191</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have been looking at the ""documentation"" for OCRAM in the IMX6ULL ref manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems to have mysterious 'advanced features' designed to avoid timing issues..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These advanced features are controlled by&amp;nbsp;IOMUXC.GPR3 and configure wait states and pipe lining. It seems that at 'higher frequency'&amp;nbsp;these features are required to avoid potential timing problems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What are these potential timing problems?? Does the read / write fail or lock up or does that chip just explode?&lt;/P&gt;&lt;P&gt;What exactly is 'higher frequency'? When should wait&amp;nbsp;states and pipe lining be enabled?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have checked the ref manuals for many IMX6 devices and they contain the same cut-and-paste info.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Apr 2020 03:16:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-OCRAM/m-p/1055095#M155191</guid>
      <dc:creator>paulbox23</dc:creator>
      <dc:date>2020-04-21T03:16:16Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6UL OCRAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-OCRAM/m-p/1055096#M155192</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Paul,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt; According to app note AN12077 (Using the i.MX RT FlexRAM) OCRAM is used during boot:&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;The minimum configuration of OCRAM is 128 KB I guess is for MX6UL.&amp;nbsp; This is required due to ROM code requires at least &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;64 KB of RAM for its execution (device dependent).&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="" style="min-height: 8pt; padding: 0px;"&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;A data-content-finding="Community" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fapplication-note%2FAN12077.pdf" rel="nofollow" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12077.pdf&lt;/A&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="" style="min-height: 8pt; padding: 0px;"&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; Customers can use OCRAM (after boot) as needed, in particular - for buffers.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; App note AN12437 (i.MX RT Series Performance Optimization) states, that "OCRAM shows higher &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;performance than TCM when accessed by DMA, while lower performance when accessed by MCU core.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt; The reason is that OCRAM and DMA are in this same bus fabric, with less latency during the access." &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="" style="min-height: 8pt; padding: 0px;"&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;A data-content-finding="Community" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fapplication-note%2FAN12437.pdf" rel="nofollow" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12437.pdf&lt;/A&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="" style="min-height: 8pt; padding: 0px;"&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P class="" style="min-height: 8pt; padding: 0px;"&gt;Of course, you can use a small OS-less applications running in OCRAM only not using DRAM. However, the functionality of such applications seems to be very limited due to small amount of memory available. On the other hand, it is possible to run the code directly from, for example, external parallel NOR flash using the External Memory Interface module and use OCRAM for stack/data only. The limitations here are: 1) relatively slow EIM operation and 2) relatively small address space of up to 128MBytes.&lt;/P&gt;&lt;P class="" style="min-height: 8pt; padding: 0px;"&gt;&lt;/P&gt;&lt;P class="" style="min-height: 8pt; padding: 0px;"&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Apr 2020 14:21:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-OCRAM/m-p/1055096#M155192</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2020-04-22T14:21:29Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6UL OCRAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-OCRAM/m-p/1055097#M155193</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Thanks for the feedback.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But my question is about the performance bits in&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;IOMUXC.GPR3 in IMX6UL (not RT)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;These performance bits are used&amp;nbsp;to insert wait states and pipelining when the OCRAM (AXI bus I assume) is accessed at a 'higher frequency'. The reference manual does not specify what 'higher frequency' is&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Please take a look at&amp;nbsp;&lt;STRONG&gt;i.MX 6UltraLite Applications Processor Reference Manual&lt;/STRONG&gt; &amp;nbsp;Section 36.3&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;At what bus speed are these wait states required?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Cheers&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Paul&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Apr 2020 11:17:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6UL-OCRAM/m-p/1055097#M155193</guid>
      <dc:creator>paulbox23</dc:creator>
      <dc:date>2020-04-23T11:17:44Z</dc:date>
    </item>
  </channel>
</rss>