<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: sabresd flash</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/sabresd-flash/m-p/224127#M15511</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Niklas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I included it in my image build. This is the procedure that I followed,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the L3.0.35_4.1.0 BSP.&lt;/P&gt;&lt;P&gt;U-boot : 2008:09&lt;/P&gt;&lt;P&gt;mx6q_sabreauto_weimnor&lt;/P&gt;&lt;P&gt;Minimum profile.&lt;/P&gt;&lt;P&gt;I included just the one e2fsprogs package in addition to the default minimum profile packages and built the image. &lt;/P&gt;&lt;P&gt;Loaded the images in the NOR flash,&lt;/P&gt;&lt;P&gt;Once I booted my system from the parallel nor, it showed up in my rootfs.&lt;/P&gt;&lt;P&gt;yes, there might be some conflicting packages.&lt;/P&gt;&lt;P&gt;May be a fresh LTIB build with just the e2fsprogs package and then adding the other packages serially would help you find out the conflicting package. &lt;/P&gt;&lt;P&gt;hope it helps.&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P&gt;nishad&lt;/P&gt;&lt;P&gt;From: Niklas Molin &lt;/P&gt;&lt;P&gt;Sent: Sunday, March 23, 2014 3:00 AM&lt;/P&gt;&lt;P&gt;To: nishad nishad &lt;/P&gt;&lt;P&gt;Subject: Re:  - sabresd flash&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;           &lt;/P&gt;&lt;P&gt;            sabresd flash &lt;/P&gt;&lt;P&gt;            reply from Niklas Molin in i.MX Community - View the full discussion&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Mar 2014 05:59:20 GMT</pubDate>
    <dc:creator>nishad_kamdar</dc:creator>
    <dc:date>2014-03-24T05:59:20Z</dc:date>
    <item>
      <title>sabresd flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/sabresd-flash/m-p/224120#M15504</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm doings some tests with the sabresd board and the flash (emmc).&lt;/P&gt;&lt;P&gt;I noticed that there is boot0 and boot1 created for that chip.&lt;/P&gt;&lt;P&gt;What is the reason for this 2 boot "devices" and where in the code can I change that.&lt;/P&gt;&lt;P&gt;I notice that (I have to confirm this tomorrow) I portioning the Linux part to a few GB, but when I reboot next time it is only around 300Mb.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Niklas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Nov 2013 07:29:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/sabresd-flash/m-p/224120#M15504</guid>
      <dc:creator>niklasmolin</dc:creator>
      <dc:date>2013-11-25T07:29:46Z</dc:date>
    </item>
    <item>
      <title>Re: sabresd flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/sabresd-flash/m-p/224121#M15505</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. &lt;/P&gt;&lt;P&gt;Please let me know what do You mean under "boot0" and "boot1" ?&lt;/P&gt;&lt;P&gt;Are there&amp;nbsp; BOOT_MODE[1:0] pins of the i.MX6 ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; If so, these pins just define boot modes, described in section 8.2.1 (Boot mode pin settings) of i.MX6 Reference &lt;BR /&gt;Manual (IMX6DQRM, Rev. 1, 04/2013). Boot devices are configured using so called BOOT_CFG fuses / pins.&lt;BR /&gt;Please refer to chapter 8 of the RM for more details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.&lt;/P&gt;&lt;P&gt;As for Linux partition of 300 MB, please check ucl2.xml file in "&amp;lt;MFG_dir&amp;gt;\Profiles\MX6Q Linux Update\OS Firmware\"&lt;/P&gt;&lt;P&gt;if the MFG is applied to deploy the images. In ucl2.xml file we can see details about deploying process. Perhaps &lt;/P&gt;&lt;P&gt;it makes sense to check script "&lt;SPAN style="font-size: 12.0pt; font-family: 'Verdana','sans-serif';"&gt;mksdcard.sh.tar&lt;/SPAN&gt;", which provides instructions for sfdisk.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Nov 2013 03:12:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/sabresd-flash/m-p/224121#M15505</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2013-11-28T03:12:08Z</dc:date>
    </item>
    <item>
      <title>Re: sabresd flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/sabresd-flash/m-p/224122#M15506</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I look in the /dev (plus during boot up) there is mmcbl1boot0 and mmcbl1boot1 (which is for the flash).&lt;/P&gt;&lt;P&gt;Not sure why this one is created and where in the code (I haven't had time to investigate this).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also tried to format the Linux partition in my flash (mmcblk1p2) with mkfs, but get following errors:&lt;/P&gt;&lt;P&gt;root@imx6qsabresd:~# mkfs.ext3 /dev/mmcblk1p2&lt;/P&gt;&lt;P&gt;-sh: mkfs.ext3: command not found&lt;/P&gt;&lt;P&gt;root@imx6qsabresd:~# mkfs -t ext3 /dev/mmcblk1p2&lt;/P&gt;&lt;P&gt;mkfs.ext3: No such file or directory&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Niklas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Dec 2013 18:52:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/sabresd-flash/m-p/224122#M15506</guid>
      <dc:creator>niklasmolin</dc:creator>
      <dc:date>2013-12-02T18:52:51Z</dc:date>
    </item>
    <item>
      <title>Re: sabresd flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/sabresd-flash/m-p/224123#M15507</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Niklas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;were you able to solve the mkfs.ext3 : command not found issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am stuck at the same point right now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P&gt;nishad&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Mar 2014 06:33:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/sabresd-flash/m-p/224123#M15507</guid>
      <dc:creator>nishad_kamdar</dc:creator>
      <dc:date>2014-03-21T06:33:18Z</dc:date>
    </item>
    <item>
      <title>Re: sabresd flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/sabresd-flash/m-p/224124#M15508</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;nishad.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;I recall I manually compiled.installed that package (E2fsprogs) &lt;/SPAN&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 10pt; line-height: 1.5em;"&gt;on the board. I haven't played around with it since then.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="line-height: 1.5em; color: #3d3d3d; font-size: 10pt; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;But I need to do that soon again, for our custom board. Then I'll look in to fixing the recipes, so I don't &lt;/SPAN&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;manually&lt;/SPAN&gt;&lt;SPAN style="line-height: 1.5em; color: #3d3d3d; font-size: 10pt; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt; have to install it.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 10pt; line-height: 1.5em;"&gt;Right now I have problem that I don't have gcc in my image (not sure if you have had that problem).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 10pt; line-height: 1.5em;"&gt;Before I could include tools-sdk in my build, but no it doesn't compile if I include that.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 10pt; line-height: 1.5em;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 10pt; line-height: 1.5em;"&gt;Niklas&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Mar 2014 13:47:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/sabresd-flash/m-p/224124#M15508</guid>
      <dc:creator>niklasmolin</dc:creator>
      <dc:date>2014-03-21T13:47:00Z</dc:date>
    </item>
    <item>
      <title>Re: sabresd flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/sabresd-flash/m-p/224125#M15509</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Niklas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the prompt reply,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I included the e2fsprogs and I was able to acquire all the files for forming .ext3 and .ext4 partiotons. I partitioned the eMMC and stored my rootfs in it. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have attached the console log of my rootfs booting from eMMC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again,&lt;/P&gt;&lt;P&gt;nishad&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From: Niklas Molin &lt;/P&gt;&lt;P&gt;Sent: Friday, March 21, 2014 7:18 PM&lt;/P&gt;&lt;P&gt;To: nishad nishad &lt;/P&gt;&lt;P&gt;Subject: Re:  - sabresd flash&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;           &lt;/P&gt;&lt;P&gt;            sabresd flash &lt;/P&gt;&lt;P&gt;            reply from Niklas Molin in i.MX Community - View the full discussion&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 22 Mar 2014 07:42:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/sabresd-flash/m-p/224125#M15509</guid>
      <dc:creator>nishad_kamdar</dc:creator>
      <dc:date>2014-03-22T07:42:09Z</dc:date>
    </item>
    <item>
      <title>Re: sabresd flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/sabresd-flash/m-p/224126#M15510</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi nishad.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did you manually compile the e2fsprogs or include it in your image build?&lt;/P&gt;&lt;P&gt;When I include it in my image build, it won't show up in my rootfs (might&lt;/P&gt;&lt;P&gt;be some other recipes I include that causing the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Niklas&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On Sat, Mar 22, 2014 at 12:43 AM, nishad nishad &amp;lt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 22 Mar 2014 21:30:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/sabresd-flash/m-p/224126#M15510</guid>
      <dc:creator>niklasmolin</dc:creator>
      <dc:date>2014-03-22T21:30:10Z</dc:date>
    </item>
    <item>
      <title>Re: sabresd flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/sabresd-flash/m-p/224127#M15511</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Niklas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I included it in my image build. This is the procedure that I followed,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the L3.0.35_4.1.0 BSP.&lt;/P&gt;&lt;P&gt;U-boot : 2008:09&lt;/P&gt;&lt;P&gt;mx6q_sabreauto_weimnor&lt;/P&gt;&lt;P&gt;Minimum profile.&lt;/P&gt;&lt;P&gt;I included just the one e2fsprogs package in addition to the default minimum profile packages and built the image. &lt;/P&gt;&lt;P&gt;Loaded the images in the NOR flash,&lt;/P&gt;&lt;P&gt;Once I booted my system from the parallel nor, it showed up in my rootfs.&lt;/P&gt;&lt;P&gt;yes, there might be some conflicting packages.&lt;/P&gt;&lt;P&gt;May be a fresh LTIB build with just the e2fsprogs package and then adding the other packages serially would help you find out the conflicting package. &lt;/P&gt;&lt;P&gt;hope it helps.&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P&gt;nishad&lt;/P&gt;&lt;P&gt;From: Niklas Molin &lt;/P&gt;&lt;P&gt;Sent: Sunday, March 23, 2014 3:00 AM&lt;/P&gt;&lt;P&gt;To: nishad nishad &lt;/P&gt;&lt;P&gt;Subject: Re:  - sabresd flash&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;           &lt;/P&gt;&lt;P&gt;            sabresd flash &lt;/P&gt;&lt;P&gt;            reply from Niklas Molin in i.MX Community - View the full discussion&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Mar 2014 05:59:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/sabresd-flash/m-p/224127#M15511</guid>
      <dc:creator>nishad_kamdar</dc:creator>
      <dc:date>2014-03-24T05:59:20Z</dc:date>
    </item>
    <item>
      <title>Re: sabresd flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/sabresd-flash/m-p/224128#M15512</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;STRONG style="font-size: 12px; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&lt;A href="https://community.nxp.com/people/nishad.kamdar@bitmapper.com"&gt;nishad.kamdar@bitmapper.com&lt;/A&gt;&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using Yocto, so there might be some difference.&lt;/P&gt;&lt;P&gt;But I haven't had time to look into this lately.&lt;/P&gt;&lt;P&gt;I'll dig into this when I'm starting with the eMMC again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Niklas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Mar 2014 06:04:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/sabresd-flash/m-p/224128#M15512</guid>
      <dc:creator>niklasmolin</dc:creator>
      <dc:date>2014-03-24T06:04:09Z</dc:date>
    </item>
  </channel>
</rss>