<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.mx6q opencv opencl error</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6q-opencv-opencl-error/m-p/1053939#M155056</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using OpenCV 4.3 on i.mx6 quad plus.&lt;/P&gt;&lt;P&gt;And I used OpenCL in OpenCV.&lt;/P&gt;&lt;P&gt;but got error&lt;/P&gt;&lt;P&gt;======== error ========&lt;/P&gt;&lt;P&gt;OpenCL error CL_INVALID_WORK_GROUP_SIZE (-54) during call: clEnqueueNDRangeKerneA&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;======== platform =========&lt;/P&gt;&lt;P&gt;imx6qpsabresd:~/DSMS# opencv_version --opencl &lt;BR /&gt;4.3.0 &lt;BR /&gt;OpenCL Platforms: &lt;BR /&gt; Vivante OpenCL Platform &lt;BR /&gt; iGPU: Vivante OpenCL Device GC3000.5450.0000 (OpenCL 1.1 ) &lt;BR /&gt;Current OpenCL device: &lt;BR /&gt; Type = iGPU &lt;BR /&gt; Name = Vivante OpenCL Device GC3000.5450.0000 &lt;BR /&gt; Version = OpenCL 1.1 &lt;BR /&gt; Driver version = OpenCL 1.1 V6.2.2.93313 &lt;BR /&gt; Address bits = 32 &lt;BR /&gt; Compute units = 4 &lt;BR /&gt; Max work group size = 1024 &lt;BR /&gt; Local memory size = 1 KB &lt;BR /&gt; Max memory allocation size = 128 MB &lt;BR /&gt; Double support = No &lt;BR /&gt; Host unified memory = Yes &lt;BR /&gt; Device extensions: &lt;BR /&gt; cl_khr_byte_addressable_store &lt;BR /&gt; cl_khr_gl_sharing &lt;BR /&gt; Has AMD Blas = No &lt;BR /&gt; Has AMD Fft = No &lt;BR /&gt; Preferred vector width char = 4 &lt;BR /&gt; Preferred vector width short = 4 &lt;BR /&gt; Preferred vector width int = 4 &lt;BR /&gt; Preferred vector width long = 0 &lt;BR /&gt; Preferred vector width float = 4 &lt;BR /&gt; Preferred vector width double = 0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why this error occured?&lt;/P&gt;&lt;P&gt;and what should I do?&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Jul 2020 02:46:14 GMT</pubDate>
    <dc:creator>gustcool2</dc:creator>
    <dc:date>2020-07-02T02:46:14Z</dc:date>
    <item>
      <title>i.mx6q opencv opencl error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6q-opencv-opencl-error/m-p/1053939#M155056</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using OpenCV 4.3 on i.mx6 quad plus.&lt;/P&gt;&lt;P&gt;And I used OpenCL in OpenCV.&lt;/P&gt;&lt;P&gt;but got error&lt;/P&gt;&lt;P&gt;======== error ========&lt;/P&gt;&lt;P&gt;OpenCL error CL_INVALID_WORK_GROUP_SIZE (-54) during call: clEnqueueNDRangeKerneA&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;======== platform =========&lt;/P&gt;&lt;P&gt;imx6qpsabresd:~/DSMS# opencv_version --opencl &lt;BR /&gt;4.3.0 &lt;BR /&gt;OpenCL Platforms: &lt;BR /&gt; Vivante OpenCL Platform &lt;BR /&gt; iGPU: Vivante OpenCL Device GC3000.5450.0000 (OpenCL 1.1 ) &lt;BR /&gt;Current OpenCL device: &lt;BR /&gt; Type = iGPU &lt;BR /&gt; Name = Vivante OpenCL Device GC3000.5450.0000 &lt;BR /&gt; Version = OpenCL 1.1 &lt;BR /&gt; Driver version = OpenCL 1.1 V6.2.2.93313 &lt;BR /&gt; Address bits = 32 &lt;BR /&gt; Compute units = 4 &lt;BR /&gt; Max work group size = 1024 &lt;BR /&gt; Local memory size = 1 KB &lt;BR /&gt; Max memory allocation size = 128 MB &lt;BR /&gt; Double support = No &lt;BR /&gt; Host unified memory = Yes &lt;BR /&gt; Device extensions: &lt;BR /&gt; cl_khr_byte_addressable_store &lt;BR /&gt; cl_khr_gl_sharing &lt;BR /&gt; Has AMD Blas = No &lt;BR /&gt; Has AMD Fft = No &lt;BR /&gt; Preferred vector width char = 4 &lt;BR /&gt; Preferred vector width short = 4 &lt;BR /&gt; Preferred vector width int = 4 &lt;BR /&gt; Preferred vector width long = 0 &lt;BR /&gt; Preferred vector width float = 4 &lt;BR /&gt; Preferred vector width double = 0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why this error occured?&lt;/P&gt;&lt;P&gt;and what should I do?&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jul 2020 02:46:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6q-opencv-opencl-error/m-p/1053939#M155056</guid>
      <dc:creator>gustcool2</dc:creator>
      <dc:date>2020-07-02T02:46:14Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6q opencv opencl error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6q-opencv-opencl-error/m-p/1053940#M155057</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;maybe you can refer to the document as below:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-93984"&gt;https://community.nxp.com/docs/DOC-93984&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jul 2020 07:37:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6q-opencv-opencl-error/m-p/1053940#M155057</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2020-07-02T07:37:46Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6q opencv opencl error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6q-opencv-opencl-error/m-p/1053941#M155058</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How many dimensions are you using ? also, what is the size of your local and global work group ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jul 2020 17:30:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6q-opencv-opencl-error/m-p/1053941#M155058</guid>
      <dc:creator>andre_silva</dc:creator>
      <dc:date>2020-07-22T17:30:12Z</dc:date>
    </item>
  </channel>
</rss>