<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Treck TCP/IP in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Treck-TCP-IP/m-p/1053835#M155041</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The TCP/IP library is used but it´s not from trek.But It can be implemented. Implements routing operations for TCP/UDP&lt;BR /&gt;connections:&lt;BR /&gt;− IPv4 with and without NAT&lt;BR /&gt;− IPv6&lt;BR /&gt;− VLAN tag insertion and removal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Jul 2020 13:28:45 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2020-07-03T13:28:45Z</dc:date>
    <item>
      <title>Treck TCP/IP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Treck-TCP-IP/m-p/1053834#M155040</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; Recently, there has been a vulnerability issue in the Treck TCP/IP protocol library. Will the NXP i.MX8MM I use, the officially improved demo image and the cross-compilation chain tool have any impact? Is the Treck TCP/IP protocol library used?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;A href="https://www.jsof-tech.com/ripple20/" target="test_blank"&gt;https://www.jsof-tech.com/ripple20/&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jul 2020 00:43:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Treck-TCP-IP/m-p/1053834#M155040</guid>
      <dc:creator>story</dc:creator>
      <dc:date>2020-07-02T00:43:27Z</dc:date>
    </item>
    <item>
      <title>Re: Treck TCP/IP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Treck-TCP-IP/m-p/1053835#M155041</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The TCP/IP library is used but it´s not from trek.But It can be implemented. Implements routing operations for TCP/UDP&lt;BR /&gt;connections:&lt;BR /&gt;− IPv4 with and without NAT&lt;BR /&gt;− IPv6&lt;BR /&gt;− VLAN tag insertion and removal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jul 2020 13:28:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Treck-TCP-IP/m-p/1053835#M155041</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2020-07-03T13:28:45Z</dc:date>
    </item>
    <item>
      <title>Re: Treck TCP/IP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Treck-TCP-IP/m-p/1053836#M155042</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we have same doubt about Tcp/ip library.&lt;BR /&gt;"Does MQX TCP/IP stack have this vulnerability"&lt;BR /&gt;we are using K60 micro controller for network connectivity&lt;BR /&gt;please confirm on this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&amp;nbsp;&lt;/P&gt;&lt;P&gt;Saikiran.M&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Aug 2020 09:04:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Treck-TCP-IP/m-p/1053836#M155042</guid>
      <dc:creator>amsec</dc:creator>
      <dc:date>2020-08-04T09:04:45Z</dc:date>
    </item>
  </channel>
</rss>