<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx8qx SDK in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8qx-SDK/m-p/1052602#M154891</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please try the below DISTRO.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DISTRO=fsl-imx-fb MACHINE=imx8qxpmek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 09 May 2020 17:24:25 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2020-05-09T17:24:25Z</dc:date>
    <item>
      <title>imx8qx SDK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qx-SDK/m-p/1052601#M154890</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;I built an image for iMX8QXPMEK machine. I'm tryng to add SDK but I'm having the following errors:&lt;/P&gt;&lt;P&gt;also I tried bitbake core-image-minimal -c populate_sdk, but got the same errors.&lt;/P&gt;&lt;P&gt;I'm working on Ubuntu 18.04.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~/imx-yocto-bsp/build-wayland$ bitbake imx-image-core -c populate_sdk&lt;BR /&gt;Loading cache: 100% |############################################| Time: 0:00:01&lt;BR /&gt;Loaded 4067 entries from dependency cache.&lt;BR /&gt;NOTE: Resolving any missing task queue dependencies&lt;/P&gt;&lt;P&gt;Build Configuration:&lt;BR /&gt;BB_VERSION = "1.44.0"&lt;BR /&gt;BUILD_SYS = "x86_64-linux"&lt;BR /&gt;NATIVELSBSTRING = "ubuntu-18.04"&lt;BR /&gt;TARGET_SYS = "aarch64-poky-linux"&lt;BR /&gt;MACHINE = "imx8qxpmek"&lt;BR /&gt;DISTRO = "fsl-imx-wayland"&lt;BR /&gt;DISTRO_VERSION = "5.4-zeus"&lt;BR /&gt;TUNE_FEATURES = "aarch64"&lt;BR /&gt;TARGET_FPU = ""&lt;BR /&gt;meta &lt;BR /&gt;meta-poky = "HEAD:0275e68b0576cdefc19718e4b1977044f9f43f48"&lt;BR /&gt;meta-oe &lt;BR /&gt;meta-multimedia &lt;BR /&gt;meta-python = "HEAD:aad5b3d070cd8c58828b0975cf861d8ebc90f460"&lt;BR /&gt;meta-freescale = "HEAD:0be39721cea6e04c589a419f4bb07fabd0da6704"&lt;BR /&gt;meta-freescale-3rdparty = "HEAD:aea3771baa77e74762358ceb673d407e36637e5f"&lt;BR /&gt;meta-freescale-distro = "HEAD:ca27d12e4964d1336e662bcc60184bbff526c857"&lt;BR /&gt;meta-bsp &lt;BR /&gt;meta-sdk &lt;BR /&gt;meta-ml = "HEAD:435f5e984856a943986491fddd061734a0b9eba5"&lt;BR /&gt;meta-browser = "HEAD:5f365ef0f842ba4651efe88787cf9c63bc8b6cb3"&lt;BR /&gt;meta-rust = "HEAD:5cda04c7c2158fc982502ca1e7893f71e4ca1729"&lt;BR /&gt;meta-gnome &lt;BR /&gt;meta-networking &lt;BR /&gt;meta-filesystems = "HEAD:aad5b3d070cd8c58828b0975cf861d8ebc90f460"&lt;BR /&gt;meta-qt5 = "HEAD:432ad2aa6c3a13253fefc909faba368851d21fb1"&lt;/P&gt;&lt;P&gt;Initialising tasks: 100% |#######################################| Time: 0:00:02&lt;BR /&gt;Sstate summary: Wanted 5 Found 0 Missed 5 Current 1397 (0% match, 99% complete)&lt;BR /&gt;NOTE: Executing Tasks&lt;BR /&gt;NOTE: Setscene tasks completed&lt;BR /&gt;ERROR: nativesdk-qemu-4.1.0-r0 do_compile: oe_runmake failed&lt;BR /&gt;ERROR: nativesdk-qemu-4.1.0-r0 do_compile: Execution of '/home/jose/imx-yocto-bsp/build-wayland/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-qemu/4.1.0-r0/temp/run.do_compile.3036' failed with exit code 1:&lt;BR /&gt;make[1]: Entering directory '/home/jose/imx-yocto-bsp/build-wayland/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-qemu/4.1.0-r0/qemu-4.1.0/slirp'&lt;BR /&gt;make[1]: Nothing to be done for 'all'.&lt;BR /&gt;make[1]: Leaving directory '/home/jose/imx-yocto-bsp/build-wayland/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-qemu/4.1.0-r0/qemu-4.1.0/slirp'&lt;BR /&gt; CC mipsel-softmmu/arch_init.o&lt;BR /&gt;/home/jose/imx-yocto-bsp/build-wayland/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-qemu/4.1.0-r0/qemu-4.1.0/arch_init.c:90:28: error: 'QEMU_ARCH' undeclared here (not in a function); did you mean 'QEMU_RCU_H'?&lt;BR /&gt; 90 | const uint32_t arch_type = QEMU_ARCH;&lt;BR /&gt; | ^~~~~~~~~&lt;BR /&gt; | QEMU_RCU_H&lt;BR /&gt;/home/jose/imx-yocto-bsp/build-wayland/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-qemu/4.1.0-r0/qemu-4.1.0/arch_init.c: In function 'qmp_query_target':&lt;BR /&gt;/home/jose/imx-yocto-bsp/build-wayland/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-qemu/4.1.0-r0/qemu-4.1.0/arch_init.c:115:56: error: 'TARGET_NAME' undeclared (first use in this function)&lt;BR /&gt; 115 | info-&amp;gt;arch = qapi_enum_parse(&amp;amp;SysEmuTarget_lookup, TARGET_NAME, -1,&lt;BR /&gt; | ^~~~~~~~~~~&lt;BR /&gt;/home/jose/imx-yocto-bsp/build-wayland/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-qemu/4.1.0-r0/qemu-4.1.0/arch_init.c:115:56: note: each undeclared identifier is reported only once for each function it appears in&lt;BR /&gt;/home/jose/imx-yocto-bsp/build-wayland/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-qemu/4.1.0-r0/qemu-4.1.0/rules.mak:69: recipe for target 'arch_init.o' failed&lt;BR /&gt;make[1]: *** [arch_init.o] Error 1&lt;BR /&gt;Makefile:472: recipe for target 'mipsel-softmmu/all' failed&lt;BR /&gt;make: *** [mipsel-softmmu/all] Error 2&lt;BR /&gt;WARNING: exit code 1 from a shell command.&lt;/P&gt;&lt;P&gt;ERROR: Logfile of failure stored in: /home/jose/imx-yocto-bsp/build-wayland/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-qemu/4.1.0-r0/temp/log.do_compile.3036&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 May 2020 22:07:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qx-SDK/m-p/1052601#M154890</guid>
      <dc:creator>josehdz</dc:creator>
      <dc:date>2020-05-06T22:07:41Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qx SDK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qx-SDK/m-p/1052602#M154891</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please try the below DISTRO.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DISTRO=fsl-imx-fb MACHINE=imx8qxpmek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 May 2020 17:24:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qx-SDK/m-p/1052602#M154891</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2020-05-09T17:24:25Z</dc:date>
    </item>
  </channel>
</rss>