<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: eMMC Not detected in yocto zeus in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-Not-detected-in-yocto-zeus/m-p/1051888#M154813</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nikhil&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try with different emmc parts, try to adjust drive strength as on below case&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/332110"&gt;eMMC 8GB to 4GB - crash on linux (yocto) boot&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Jun 2020 23:47:11 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2020-06-16T23:47:11Z</dc:date>
    <item>
      <title>eMMC Not detected in yocto zeus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-Not-detected-in-yocto-zeus/m-p/1051887#M154812</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am doing a porting exercise from yocto sumo to zeus version. We are facing issue in eMMC detection in this porting. I want to highlight the same configuration is working under yocto sumo, but not in yocto zeus. Below are the booting logs respectively.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sumo bootup logs:&lt;/P&gt;&lt;P&gt;U-Boot 2018.03-4.14.98-2.3.0+g0e20792 (Apr 04 2020 - 06:23:13 +0000)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6SX rev1.3 at 792MHz&lt;BR /&gt;CPU: Industrial temperature grade (-40C to 105C) at 45C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: Freescale i.MX6 SoloX SDB RevB Board&lt;BR /&gt;Board: MX6SX SABRE SDB rev@&lt;BR /&gt;DRAM: 1 GiB&lt;BR /&gt;PMIC: PFUZE100! DEV_ID=0x11 REV_ID=0x21&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2&lt;BR /&gt;Loading Environment from MMC... *** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;Failed (-5)&lt;BR /&gt;Display: Hannstar-XGA (1024x768)&lt;BR /&gt;Video: 1024x768x18&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc2(part 0) is current device&lt;BR /&gt;flash target is MMC:2&lt;BR /&gt;Net: &lt;BR /&gt;Warning: ethernet@02188000 (eth0) using random MAC address - d2:6c:09:5b:fe:dd&lt;BR /&gt;eth0: ethernet@02188000 [PRIME]&lt;BR /&gt;Warning: ethernet@021b4000 (eth1) using random MAC address - 66:3b:d9:8d:af:be&lt;BR /&gt;, eth1: ethernet@021b4000&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0 &lt;BR /&gt;********TP_19 not Pressed [0] : Normal mode********&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc2(part 0) is current device&lt;BR /&gt;** Unable to read file boot.scr **&lt;BR /&gt;7472632 bytes read in 214 ms (33.3 MiB/s)&lt;BR /&gt;Booting from mmc ...&lt;BR /&gt;50438 bytes read in 15 ms (3.2 MiB/s)&lt;BR /&gt;Kernel image @ 0x80800000 [ 0x000000 - 0x7205f8 ]&lt;BR /&gt;## Flattened Device Tree blob at 83000000&lt;BR /&gt; Booting using the fdt blob at 0x83000000&lt;BR /&gt; Using Device Tree in place at 83000000, end 8300f505&lt;BR /&gt;switch to ldo_bypass mode!&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;Booting Linux on physical CPU 0x0&lt;/P&gt;&lt;P&gt;================================================&lt;/P&gt;&lt;P&gt;Zeus bootup logs:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot 2019.04-lf-5.4.y_v2019.04+g228843cdf5 (May 30 2020 - 17:24:25 +0000)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6SX rev1.3 at 792MHz&lt;BR /&gt;CPU: Industrial temperature grade (-40C to 105C) at 43C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: Freescale i.MX6 SoloX SDB RevB Board&lt;BR /&gt;Board: MX6SX SABRE SDB rev@&lt;BR /&gt;DRAM: 1 GiB&lt;BR /&gt;PMIC: PFUZE100! DEV_ID=0x11 REV_ID=0x21&lt;BR /&gt;MMC: &lt;BR /&gt;Loading Environment from MMC... MMC Device 2 not found&lt;BR /&gt;*** Warning - No MMC card found, using default environment&lt;/P&gt;&lt;P&gt;Display: Hannstar-XGA (1024x768)&lt;BR /&gt;Video: 1024x768x18&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;No MMC device available&lt;BR /&gt;flash target is MMC:2&lt;BR /&gt;MMC Device 2 not found&lt;BR /&gt;invalid mmc device 2&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc2(part 0) is current device&lt;BR /&gt;flash target is MMC:2&lt;BR /&gt;Net: &lt;BR /&gt;Warning: ethernet@02188000 (eth0) using random MAC address - 2e:38:9e:24:b0:7c&lt;BR /&gt;eth0: ethernet@02188000 [PRIME]&lt;BR /&gt;Warning: ethernet@021b4000 (eth1) using random MAC address - ba:6e:8b:bd:30:cf&lt;BR /&gt;, eth1: ethernet@021b4000&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0 &lt;BR /&gt;********TP_19 not Pressed [0] : Normal mode********&lt;BR /&gt;No MMC device available&lt;BR /&gt;No MMC device available&lt;BR /&gt;Booting from net ...&lt;BR /&gt;ethernet@02188000 Waiting for PHY auto negotiation to complete....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone please point out where i can lagging, the same configuration worked in sumo but not in zeus.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Nikhil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jun 2020 17:14:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/eMMC-Not-detected-in-yocto-zeus/m-p/1051887#M154812</guid>
      <dc:creator>nikhil_sahu2</dc:creator>
      <dc:date>2020-06-16T17:14:46Z</dc:date>
    </item>
    <item>
      <title>Re: eMMC Not detected in yocto zeus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-Not-detected-in-yocto-zeus/m-p/1051888#M154813</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nikhil&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try with different emmc parts, try to adjust drive strength as on below case&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/332110"&gt;eMMC 8GB to 4GB - crash on linux (yocto) boot&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jun 2020 23:47:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/eMMC-Not-detected-in-yocto-zeus/m-p/1051888#M154813</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-06-16T23:47:11Z</dc:date>
    </item>
  </channel>
</rss>