<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Unused supplies on PF0100 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Unused-supplies-on-PF0100/m-p/223839#M15463</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I've made a construction with iMX6 solo based on the Sabre SD development board. It looks like I'm not going to need some regulators from the PF0100, for instance VGEN1 and VGEN2. I assume their outputs should just be NC then? Also, this implies that I do not need to connect any supply to VIN1 (which powers VGEN1 and VGEN2). Is this correct? Can I just leave VIN1 unconnected and connect VIN2 and VIN3 only?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Emil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Feb 2014 10:38:24 GMT</pubDate>
    <dc:creator>emil</dc:creator>
    <dc:date>2014-02-11T10:38:24Z</dc:date>
    <item>
      <title>Unused supplies on PF0100</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unused-supplies-on-PF0100/m-p/223839#M15463</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I've made a construction with iMX6 solo based on the Sabre SD development board. It looks like I'm not going to need some regulators from the PF0100, for instance VGEN1 and VGEN2. I assume their outputs should just be NC then? Also, this implies that I do not need to connect any supply to VIN1 (which powers VGEN1 and VGEN2). Is this correct? Can I just leave VIN1 unconnected and connect VIN2 and VIN3 only?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Emil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Feb 2014 10:38:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unused-supplies-on-PF0100/m-p/223839#M15463</guid>
      <dc:creator>emil</dc:creator>
      <dc:date>2014-02-11T10:38:24Z</dc:date>
    </item>
    <item>
      <title>Re: Unused supplies on PF0100</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unused-supplies-on-PF0100/m-p/223840#M15464</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please refer to Table 1 (MMPF0100 Pin Connection Guidelines) of AN4717 &lt;/P&gt;&lt;P&gt;(Schematic Guidelines for the MMPF0100).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/analog/doc/app_note/AN4717.pdf"&gt;http://cache.freescale.com/files/analog/doc/app_note/AN4717.pdf&lt;/A&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Feb 2014 11:23:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unused-supplies-on-PF0100/m-p/223840#M15464</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2014-02-11T11:23:39Z</dc:date>
    </item>
  </channel>
</rss>