<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックmfgtool, No Device Connected.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/mfgtool-No-Device-Connected/m-p/1049738#M154562</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have an i.mx6qp sabred board and I want to download it using mfgtool.&lt;BR /&gt;However, the PC does not recognize the device.&lt;BR /&gt;SW6 dip switch is set to 00001100.&lt;BR /&gt;When a USB OTB connector is connected to a PC, it is recognized as SE Blank ARIK HID.&lt;BR /&gt;If you try to force reinstallation with mfgtools \ Drivers \ iMX_BulkIO_Driver \ imxusb.inf, the installation will fail because it is not 64-bit compatible.&lt;BR /&gt;The MFG tool version is 2.7.0.&lt;BR /&gt;What should I do?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 May 2020 08:44:46 GMT</pubDate>
    <dc:creator>openclosed</dc:creator>
    <dc:date>2020-05-06T08:44:46Z</dc:date>
    <item>
      <title>mfgtool, No Device Connected.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mfgtool-No-Device-Connected/m-p/1049738#M154562</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have an i.mx6qp sabred board and I want to download it using mfgtool.&lt;BR /&gt;However, the PC does not recognize the device.&lt;BR /&gt;SW6 dip switch is set to 00001100.&lt;BR /&gt;When a USB OTB connector is connected to a PC, it is recognized as SE Blank ARIK HID.&lt;BR /&gt;If you try to force reinstallation with mfgtools \ Drivers \ iMX_BulkIO_Driver \ imxusb.inf, the installation will fail because it is not 64-bit compatible.&lt;BR /&gt;The MFG tool version is 2.7.0.&lt;BR /&gt;What should I do?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 May 2020 08:44:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mfgtool-No-Device-Connected/m-p/1049738#M154562</guid>
      <dc:creator>openclosed</dc:creator>
      <dc:date>2020-05-06T08:44:46Z</dc:date>
    </item>
    <item>
      <title>Re: mfgtool, No Device Connected.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mfgtool-No-Device-Connected/m-p/1049739#M154563</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is your board win7 or win10 system? And which version BSP are you using?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 May 2020 08:52:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mfgtool-No-Device-Connected/m-p/1049739#M154563</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2020-05-06T08:52:57Z</dc:date>
    </item>
  </channel>
</rss>