<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX6 and QT 5 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-and-QT-5/m-p/223800#M15454</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There's a small test program that is compiled during configure stage to test for OpenGL library presence. You may try to compile it manually and see why it fails to compile. Usually it is missing library for the GPU, as there's a few of them needed to be included.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Sep 2013 12:59:17 GMT</pubDate>
    <dc:creator>VladanJovanovic</dc:creator>
    <dc:date>2013-09-11T12:59:17Z</dc:date>
    <item>
      <title>IMX6 and QT 5</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-and-QT-5/m-p/223799#M15453</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, i hope someone here can help me. I have a Problem by the installation from QT.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Warning: Disabling pkg-config since &lt;SPAN class="caps"&gt;PKG&lt;/SPAN&gt;_CONFIG_LIBDIR is not set.&lt;BR /&gt; Note: &lt;SPAN class="caps"&gt;PKG&lt;/SPAN&gt;_CONFIG_SYSROOT_DIR automatically set to /home/udcu/LTIB/litb/rootfs&lt;BR /&gt; The OpenGL ES 2.0 functionality test failed! You might need to modify the include and library search paths by editing &lt;SPAN class="caps"&gt;QMAKE&lt;/SPAN&gt;_INCDIR_OPENGL_ES2, &lt;SPAN class="caps"&gt;QMAKE&lt;/SPAN&gt;_LIBDIR_OPENGL_ES2 and &lt;SPAN class="caps"&gt;QMAKE&lt;/SPAN&gt;_LIBS_OPENGL_ES2 in /home/udcu/qt5/qtbase/mkspecs/devices/linux-imx6-g++.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Sep 2013 12:12:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-and-QT-5/m-p/223799#M15453</guid>
      <dc:creator>conti_rob</dc:creator>
      <dc:date>2013-09-10T12:12:38Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 and QT 5</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-and-QT-5/m-p/223800#M15454</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There's a small test program that is compiled during configure stage to test for OpenGL library presence. You may try to compile it manually and see why it fails to compile. Usually it is missing library for the GPU, as there's a few of them needed to be included.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Sep 2013 12:59:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-and-QT-5/m-p/223800#M15454</guid>
      <dc:creator>VladanJovanovic</dc:creator>
      <dc:date>2013-09-11T12:59:17Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 and QT 5</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-and-QT-5/m-p/223801#M15455</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Barth&lt;/P&gt;&lt;P&gt;Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel &lt;/P&gt;&lt;P&gt;free to reply with an update to this discussion.&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Feb 2014 07:42:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-and-QT-5/m-p/223801#M15455</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-02-21T07:42:04Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 and QT 5</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-and-QT-5/m-p/223802#M15456</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Barth&lt;/P&gt;&lt;P&gt;This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Feb 2014 07:49:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-and-QT-5/m-p/223802#M15456</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-02-26T07:49:24Z</dc:date>
    </item>
  </channel>
</rss>