<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: USB Camera C270 validation in Android</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-Camera-C270-validation-in-Android/m-p/1049361#M154506</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="291957" data-username="abdulredwan" href="https://community.nxp.com/people/abdulredwan"&gt;Abdul &lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It means that USB camera is not opened in default demo image.&lt;/P&gt;&lt;P&gt;you can do it like below, and re-compile android images via android source code and bsp.&lt;/P&gt;&lt;P&gt;---------------&lt;/P&gt;&lt;P&gt;Set it in init.rc like below:&lt;/P&gt;&lt;P&gt;setprop back_camera_name uvc&lt;BR /&gt;or &lt;BR /&gt;setprop front_camera_name uvc&lt;/P&gt;&lt;P&gt;---------------&lt;/P&gt;&lt;P&gt;then program you android images into eMMC / SD card.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope above innformation is helpful for you.&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;P&gt;B.R,&lt;/P&gt;&lt;P&gt;weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Aug 2020 08:09:37 GMT</pubDate>
    <dc:creator>weidong_sun</dc:creator>
    <dc:date>2020-08-21T08:09:37Z</dc:date>
    <item>
      <title>USB Camera C270 validation in Android</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Camera-C270-validation-in-Android/m-p/1049360#M154505</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi NXP Team,&lt;/P&gt;&lt;P&gt;We are trying to evaluate USB Camera C270 with Android 9 in SabreSD platform as mentioned in the Release notes.&amp;nbsp;But when we tested the prebuilt&amp;nbsp;(&lt;A href="https://www.nxp.com/webapp/sps/download/license.jsp?colCode=P9.0.0_2.2.0_GA_DEMO_MX6SD&amp;amp;appType=file1&amp;amp;DOWNLOAD_ID=null"&gt;https://www.nxp.com/webapp/sps/download/license.jsp?colCode=P9.0.0_2.2.0_GA_DEMO_MX6SD&amp;amp;appType=file1&amp;amp;DOWNLOAD_ID=null&lt;/A&gt;)&amp;nbsp;it doesnt work. Any pointers here&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We could see UVC logs from kernel&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver uvcvideo&lt;BR /&gt;USB Video Class driver (1.1.1)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope usb camera works with default camera app&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;AMR&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Aug 2020 14:26:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Camera-C270-validation-in-Android/m-p/1049360#M154505</guid>
      <dc:creator>abdulredwan</dc:creator>
      <dc:date>2020-08-20T14:26:23Z</dc:date>
    </item>
    <item>
      <title>Re: USB Camera C270 validation in Android</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Camera-C270-validation-in-Android/m-p/1049361#M154506</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="291957" data-username="abdulredwan" href="https://community.nxp.com/people/abdulredwan"&gt;Abdul &lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It means that USB camera is not opened in default demo image.&lt;/P&gt;&lt;P&gt;you can do it like below, and re-compile android images via android source code and bsp.&lt;/P&gt;&lt;P&gt;---------------&lt;/P&gt;&lt;P&gt;Set it in init.rc like below:&lt;/P&gt;&lt;P&gt;setprop back_camera_name uvc&lt;BR /&gt;or &lt;BR /&gt;setprop front_camera_name uvc&lt;/P&gt;&lt;P&gt;---------------&lt;/P&gt;&lt;P&gt;then program you android images into eMMC / SD card.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope above innformation is helpful for you.&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;P&gt;B.R,&lt;/P&gt;&lt;P&gt;weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Aug 2020 08:09:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Camera-C270-validation-in-Android/m-p/1049361#M154506</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2020-08-21T08:09:37Z</dc:date>
    </item>
  </channel>
</rss>