<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to configure LPOS 3.1 secure OS for NAND flash? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-configure-LPOS-3-1-secure-OS-for-NAND-flash/m-p/1047181#M154225</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guyss,&lt;BR /&gt;I am having a customize imx6ul board with NAND flash memory and no sd card. I want to port the LPOS 3.1 secure OS on the custom board. The LPOS 3.1 secure OS is written and configured for SD card boot. How should I customize the source code in order to boot from NAND flash?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 31 Jul 2020 05:28:24 GMT</pubDate>
    <dc:creator>nikhil_anjane</dc:creator>
    <dc:date>2020-07-31T05:28:24Z</dc:date>
    <item>
      <title>How to configure LPOS 3.1 secure OS for NAND flash?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-configure-LPOS-3-1-secure-OS-for-NAND-flash/m-p/1047181#M154225</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guyss,&lt;BR /&gt;I am having a customize imx6ul board with NAND flash memory and no sd card. I want to port the LPOS 3.1 secure OS on the custom board. The LPOS 3.1 secure OS is written and configured for SD card boot. How should I customize the source code in order to boot from NAND flash?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Jul 2020 05:28:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-configure-LPOS-3-1-secure-OS-for-NAND-flash/m-p/1047181#M154225</guid>
      <dc:creator>nikhil_anjane</dc:creator>
      <dc:date>2020-07-31T05:28:24Z</dc:date>
    </item>
  </channel>
</rss>