<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to make jpegs with hardware acceleration in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-make-jpegs-with-hardware-acceleration/m-p/1047023#M154209</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi NXP community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am using a MX8MQEVK Developer Board and i want to make jpegs from yuyv Buffer with hardware support.&lt;BR /&gt;So i tried encoder_test from the unit tests and this is not working yet. Which dev node should i use?&lt;/P&gt;&lt;P&gt;Isn't it also possible to use VPU with vpu_wrapper? And where is the libfile located?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks in advance...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Daniel Grünewald&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 May 2020 10:44:19 GMT</pubDate>
    <dc:creator>sl2</dc:creator>
    <dc:date>2020-05-20T10:44:19Z</dc:date>
    <item>
      <title>How to make jpegs with hardware acceleration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-make-jpegs-with-hardware-acceleration/m-p/1047023#M154209</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi NXP community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am using a MX8MQEVK Developer Board and i want to make jpegs from yuyv Buffer with hardware support.&lt;BR /&gt;So i tried encoder_test from the unit tests and this is not working yet. Which dev node should i use?&lt;/P&gt;&lt;P&gt;Isn't it also possible to use VPU with vpu_wrapper? And where is the libfile located?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks in advance...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Daniel Grünewald&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 May 2020 10:44:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-make-jpegs-with-hardware-acceleration/m-p/1047023#M154209</guid>
      <dc:creator>sl2</dc:creator>
      <dc:date>2020-05-20T10:44:19Z</dc:date>
    </item>
    <item>
      <title>Re: How to make jpegs with hardware acceleration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-make-jpegs-with-hardware-acceleration/m-p/1047024#M154210</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For encoder supported only VP8 and H.264 as described in Table Supported Standards,&lt;/P&gt;&lt;P&gt;Profiles and Levels i.MX8M Reference Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 May 2020 14:07:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-make-jpegs-with-hardware-acceleration/m-p/1047024#M154210</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2020-05-21T14:07:04Z</dc:date>
    </item>
  </channel>
</rss>