<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic  imx8mini GPIO in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mini-GPIO/m-p/1045263#M153952</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your prompt reply Yuri.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using a Variscite Dev Kit, which we need more GPIO's. We would like to change Pad AD13 on the IMX8M-MINI (MIMX8MM6DVTLZAA) to a GPIO Input with high impedance, as we would like to pull this up to 3V3. Variscite in their BSP is using this pad for SAI5_RXD2 and we would like to change it to a GPIO. Can you pls advise the register/changes needed in order to achieve this?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Aug 2020 05:43:36 GMT</pubDate>
    <dc:creator>bobwang</dc:creator>
    <dc:date>2020-08-18T05:43:36Z</dc:date>
    <item>
      <title>imx8mini GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mini-GPIO/m-p/1045263#M153952</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your prompt reply Yuri.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using a Variscite Dev Kit, which we need more GPIO's. We would like to change Pad AD13 on the IMX8M-MINI (MIMX8MM6DVTLZAA) to a GPIO Input with high impedance, as we would like to pull this up to 3V3. Variscite in their BSP is using this pad for SAI5_RXD2 and we would like to change it to a GPIO. Can you pls advise the register/changes needed in order to achieve this?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Aug 2020 05:43:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mini-GPIO/m-p/1045263#M153952</guid>
      <dc:creator>bobwang</dc:creator>
      <dc:date>2020-08-18T05:43:36Z</dc:date>
    </item>
    <item>
      <title>Re:  imx8mini GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mini-GPIO/m-p/1045264#M153953</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;Configuring a pad for a specific functionality requires the following actions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;Check in the Device Tree&amp;nbsp; if the pad is used by other peripheral modules, because a pad can be configured only once in device. Such functionality has to be "disabled" in order to avoid pins conflict.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;Check what functionalities can be export the targeted pad in&amp;nbsp;&lt;STRONG&gt;include/dt-bindings/pinctrl/pins-imx8mm.h:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Macros are defined using the convention documented &lt;A class="" data-content-finding="Community" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fsource.codeaurora.org%2Fexternal%2Fimx%2Flinux-imx%2Ftree%2FDocumentation%2Fdevicetree%2Fbindings%2Fpinctrl%2Ffsl%2Cimx8mq-pinctrl.txt%3Fh%3Dimx_4.19.35_1.1.0" rel="nofollow" target="_blank"&gt;here&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;Besides, this type of macro, a sixth value, the pad configuration has to be added for full pinmux setup. The pad configuration (&lt;STRONG&gt;IOMUXC_SW_PAD_CTL_PAD_*&lt;/STRONG&gt;) is done in order to select Internal Pull Up Resistors, Hysteresis Enable, Internal Pull Down Resistors, Open Drain Enable, Slew Rate and Drive Strength.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; I've sent You more information about GPIO directly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Aug 2020 04:25:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mini-GPIO/m-p/1045264#M153953</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2020-08-19T04:25:51Z</dc:date>
    </item>
  </channel>
</rss>