<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Question on i.MX6 LVDS setting</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Question-on-i-MX6-LVDS-setting/m-p/1045127#M153933</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, it is possible. Please refer to&amp;nbsp;section&amp;nbsp;39.6.1 LDB Control Register (LDB_CTRL)&amp;nbsp;for register settings.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/116165i1FE2F33AFD6F46A3/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Table 39-5 provides different use-cases as Single-channel 0/1, Separate channel, Dual Channel, and split&amp;nbsp;channel. And above register settings help you in the above use-cases.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mrudang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 17 Jul 2020 08:06:18 GMT</pubDate>
    <dc:creator>mrudangshelat1</dc:creator>
    <dc:date>2020-07-17T08:06:18Z</dc:date>
    <item>
      <title>Question on i.MX6 LVDS setting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-on-i-MX6-LVDS-setting/m-p/1045124#M153930</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to "39.5.1 Mapping of Input Data Busses" in Reference Manual of i.MX6 Quad, when using LVDS channel 1, DI0 in single channel mode is disabled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/115849i1DE842DDE7E527B7/image-size/large?v=v2&amp;amp;px=999" title="table39-5.png" alt="table39-5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The question is: what does this mean?&lt;/P&gt;&lt;P&gt;Does it mean when using LVDS ch1, only IPU*-DI1 can be used (and IPU*-DI0 is not usable)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jul 2020 05:54:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-on-i-MX6-LVDS-setting/m-p/1045124#M153930</guid>
      <dc:creator>t_kuha</dc:creator>
      <dc:date>2020-07-15T05:54:48Z</dc:date>
    </item>
    <item>
      <title>Re: Question on i.MX6 LVDS setting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-on-i-MX6-LVDS-setting/m-p/1045125#M153931</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As per Reference Manual section 9.3-&amp;nbsp;&lt;SPAN class=""&gt;LVDS Display Bridge (LDB),&amp;nbsp;&lt;SPAN class=""&gt;LVDS Display Bridge (LDB) will be used to connect the IPU (Image Processing Unit) to the External LVDS Display Interface.&lt;/SPAN&gt; &lt;BR style="font-weight: normal;" /&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt; &lt;SPAN class=""&gt;There are 2 LVDS channels. These inputs are used to communicate RGB data and&amp;nbsp;controls to external LCD displays with the LVDS interface or through LVDS receivers.&amp;nbsp;The LVDS ports may be used as follows:&lt;BR /&gt;• One single-channel output&lt;BR /&gt;• One dual-channel output: single input, split to two output channels&lt;BR /&gt;• Two identical outputs: single input sent to both output channels&lt;BR /&gt;• Two independent outputs: two inputs sent, each, to a different output channel&lt;/SPAN&gt; &lt;BR style="font-weight: normal;" /&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Please refer section&amp;nbsp;&lt;SPAN class=""&gt;39.6.1 LDB Control Register (LDB_CTRL)&lt;/SPAN&gt;&amp;nbsp;for register settings.&lt;BR style="font-weight: normal;" /&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;It means you can use both the channel parallel mode. Let us know for which application or purpose you want to use both.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Mrudang&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jul 2020 09:42:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-on-i-MX6-LVDS-setting/m-p/1045125#M153931</guid>
      <dc:creator>mrudangshelat1</dc:creator>
      <dc:date>2020-07-15T09:42:47Z</dc:date>
    </item>
    <item>
      <title>Re: Question on i.MX6 LVDS setting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-on-i-MX6-LVDS-setting/m-p/1045126#M153932</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Mrudang,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the response.&lt;/P&gt;&lt;P&gt;What I want to know is whether DI0 can be used as the input for LVDS CH1 when it is used in "&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;STRONG&gt;One single-channel output.&lt;/STRONG&gt;"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;(I tried to input RGB data from DI0 to LVDS CH1 without apparent problems, but then what "&lt;STRONG&gt;disabled&lt;/STRONG&gt;" in Table 39-5 mean?)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jul 2020 02:38:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-on-i-MX6-LVDS-setting/m-p/1045126#M153932</guid>
      <dc:creator>t_kuha</dc:creator>
      <dc:date>2020-07-16T02:38:05Z</dc:date>
    </item>
    <item>
      <title>Re: Question on i.MX6 LVDS setting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-on-i-MX6-LVDS-setting/m-p/1045127#M153933</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, it is possible. Please refer to&amp;nbsp;section&amp;nbsp;39.6.1 LDB Control Register (LDB_CTRL)&amp;nbsp;for register settings.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/116165i1FE2F33AFD6F46A3/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Table 39-5 provides different use-cases as Single-channel 0/1, Separate channel, Dual Channel, and split&amp;nbsp;channel. And above register settings help you in the above use-cases.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mrudang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jul 2020 08:06:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-on-i-MX6-LVDS-setting/m-p/1045127#M153933</guid>
      <dc:creator>mrudangshelat1</dc:creator>
      <dc:date>2020-07-17T08:06:18Z</dc:date>
    </item>
    <item>
      <title>Re: Question on i.MX6 LVDS setting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-on-i-MX6-LVDS-setting/m-p/1045128#M153934</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class=""&gt;Mrudang&lt;/SPAN&gt; mentioned the LVDS have the ways use you can see in our RM Table39-5. Recommend you to use following our RM, do not change the order. DI0 to LVDS0 and&amp;nbsp; DI1 to LVDS1.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/116176i5E25236CCAF42589/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jul 2020 09:15:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-on-i-MX6-LVDS-setting/m-p/1045128#M153934</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2020-07-17T09:15:14Z</dc:date>
    </item>
    <item>
      <title>Re: Question on i.MX6 LVDS setting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-on-i-MX6-LVDS-setting/m-p/1045129#M153935</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Mrudang and Rita,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the answer.&lt;/P&gt;&lt;P&gt;I now understand that although it is technically posiible to use IPU* DI0 for LVDS CH1 in single channle output mode,&amp;nbsp;&lt;/P&gt;&lt;P&gt;it is not a recommended use case.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jul 2020 00:46:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-on-i-MX6-LVDS-setting/m-p/1045129#M153935</guid>
      <dc:creator>t_kuha</dc:creator>
      <dc:date>2020-07-20T00:46:59Z</dc:date>
    </item>
    <item>
      <title>Re: Question on i.MX6 LVDS setting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-on-i-MX6-LVDS-setting/m-p/1647096#M205517</link>
      <description>&lt;P&gt;Hi, do you have any recommendations for the 2 channel RGB to LVDS interface ICs?&amp;nbsp; Thanks.&lt;/P&gt;</description>
      <pubDate>Tue, 09 May 2023 10:42:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-on-i-MX6-LVDS-setting/m-p/1647096#M205517</guid>
      <dc:creator>kiranpatel</dc:creator>
      <dc:date>2023-05-09T10:42:09Z</dc:date>
    </item>
  </channel>
</rss>