<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックfirmware-imx build failure</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/firmware-imx-build-failure/m-p/1044530#M153813</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have seen this for the past yer, but do not see a clear solution.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;while running a build for poky and v3.14.79. it fails at:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ERROR: firmware-imx-1_5.4-r0 do_fetch: Fetcher failure: Fetch command export DBUS_SESSION_BUS_ADDRESS="unix:abstract=/tmp/dbus-A8plQGBIyD"; export SSH_AUTH_SOCK="/run/user/1001/keyring/ssh"; export PATH="/home/gfine/bi_buildcache/132/tmp/sysroots-uninative/x86_64-linux/usr/bin:/opt/dey-2.2/sources/poky/scripts:/home/gfine/bi_buildcache/132/tmp/sysroots/x86_64-linux/usr/bin/allarch-dey-linux:/home/gfine/bi_buildcache/132/tmp/sysroots/ibwarmer/usr/bin/crossscripts:/home/gfine/bi_buildcache/132/tmp/sysroots/x86_64-linux/usr/sbin:/home/gfine/bi_buildcache/132/tmp/sysroots/x86_64-linux/usr/bin:/home/gfine/bi_buildcache/132/tmp/sysroots/x86_64-linux/sbin:/home/gfine/bi_buildcache/132/tmp/sysroots/x86_64-linux/bin:/opt/dey-2.2/sources/poky/scripts:/opt/dey-2.2/sources/poky/bitbake/bin:/home/gfine/.cargo/bin:/home/gfine/bin:/home/gfine/.local/bin:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/usr/local/games:/snap/bin"; export HOME="/home/gfine"; LANG=C git -c core.fsyncobjectfiles=0 clone --bare --mirror git://git.freescale.com/imx/imx-firmware.git /home/gfine/bi_buildcache/132/downloads/git2/git.freescale.com.imx.imx-firmware.git --progress failed with exit code 128, output:&lt;BR /&gt;Cloning into bare repository '/home/gfine/bi_buildcache/132/downloads/git2/git.freescale.com.imx.imx-firmware.git'...&lt;BR /&gt;fatal: Unable to look up git.freescale.com (port 9418) (No address associated with hostname)&lt;/P&gt;&lt;P&gt;ERROR: firmware-imx-1_5.4-r0 do_fetch: Fetcher failure for URL: 'git://git.freescale.com/imx/imx-firmware.git;branch=master;destsuffix=/home/gfine/bi_buildcache/132/tmp/work/all-dey-linux/firmware-imx/1_5.4-r0/firmware-imx-5.4/git'. Unable to fetch URL from any source.&lt;BR /&gt;ERROR: firmware-imx-1_5.4-r0 do_fetch: Function failed: base_do_fetch&lt;BR /&gt;ERROR: Logfile of failure stored in: /home/gfine/bi_buildcache/132/tmp/work/all-dey-linux/firmware-imx/1_5.4-r0/temp/log.do_fetch.11389&lt;BR /&gt;ERROR: Task (/opt/dey-2.2/sources/meta-freescale/recipes-bsp/firmware-imx/firmware-imx_5.4.bb:do_fetch) failed with exit code '1'&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I do see suggestions to use&amp;nbsp;"&lt;A class="link-titled" href="https://source.codeaurora.org/external" title="https://source.codeaurora.org/external"&gt;Code Aurora git repositories&lt;/A&gt;&amp;nbsp;"&amp;nbsp;(instead of freescale.com)&amp;nbsp; but it fails in the same fashion.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here is what I used in firmware.imx :&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SRC_URI = "${FSL_MIRROR}/firmware-imx-${PV}.bin;fsl-eula=true \&lt;BR /&gt;&amp;nbsp;https://source.codeaurora.org/external/imx/imx-firmware.git;branch=${SRCBRANCH};destsuffix=${S}/git "&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone give me the correct solution?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers, Glen&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 May 2020 22:16:06 GMT</pubDate>
    <dc:creator>glenfine</dc:creator>
    <dc:date>2020-05-19T22:16:06Z</dc:date>
    <item>
      <title>firmware-imx build failure</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/firmware-imx-build-failure/m-p/1044530#M153813</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have seen this for the past yer, but do not see a clear solution.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;while running a build for poky and v3.14.79. it fails at:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ERROR: firmware-imx-1_5.4-r0 do_fetch: Fetcher failure: Fetch command export DBUS_SESSION_BUS_ADDRESS="unix:abstract=/tmp/dbus-A8plQGBIyD"; export SSH_AUTH_SOCK="/run/user/1001/keyring/ssh"; export PATH="/home/gfine/bi_buildcache/132/tmp/sysroots-uninative/x86_64-linux/usr/bin:/opt/dey-2.2/sources/poky/scripts:/home/gfine/bi_buildcache/132/tmp/sysroots/x86_64-linux/usr/bin/allarch-dey-linux:/home/gfine/bi_buildcache/132/tmp/sysroots/ibwarmer/usr/bin/crossscripts:/home/gfine/bi_buildcache/132/tmp/sysroots/x86_64-linux/usr/sbin:/home/gfine/bi_buildcache/132/tmp/sysroots/x86_64-linux/usr/bin:/home/gfine/bi_buildcache/132/tmp/sysroots/x86_64-linux/sbin:/home/gfine/bi_buildcache/132/tmp/sysroots/x86_64-linux/bin:/opt/dey-2.2/sources/poky/scripts:/opt/dey-2.2/sources/poky/bitbake/bin:/home/gfine/.cargo/bin:/home/gfine/bin:/home/gfine/.local/bin:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/usr/local/games:/snap/bin"; export HOME="/home/gfine"; LANG=C git -c core.fsyncobjectfiles=0 clone --bare --mirror git://git.freescale.com/imx/imx-firmware.git /home/gfine/bi_buildcache/132/downloads/git2/git.freescale.com.imx.imx-firmware.git --progress failed with exit code 128, output:&lt;BR /&gt;Cloning into bare repository '/home/gfine/bi_buildcache/132/downloads/git2/git.freescale.com.imx.imx-firmware.git'...&lt;BR /&gt;fatal: Unable to look up git.freescale.com (port 9418) (No address associated with hostname)&lt;/P&gt;&lt;P&gt;ERROR: firmware-imx-1_5.4-r0 do_fetch: Fetcher failure for URL: 'git://git.freescale.com/imx/imx-firmware.git;branch=master;destsuffix=/home/gfine/bi_buildcache/132/tmp/work/all-dey-linux/firmware-imx/1_5.4-r0/firmware-imx-5.4/git'. Unable to fetch URL from any source.&lt;BR /&gt;ERROR: firmware-imx-1_5.4-r0 do_fetch: Function failed: base_do_fetch&lt;BR /&gt;ERROR: Logfile of failure stored in: /home/gfine/bi_buildcache/132/tmp/work/all-dey-linux/firmware-imx/1_5.4-r0/temp/log.do_fetch.11389&lt;BR /&gt;ERROR: Task (/opt/dey-2.2/sources/meta-freescale/recipes-bsp/firmware-imx/firmware-imx_5.4.bb:do_fetch) failed with exit code '1'&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I do see suggestions to use&amp;nbsp;"&lt;A class="link-titled" href="https://source.codeaurora.org/external" title="https://source.codeaurora.org/external"&gt;Code Aurora git repositories&lt;/A&gt;&amp;nbsp;"&amp;nbsp;(instead of freescale.com)&amp;nbsp; but it fails in the same fashion.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here is what I used in firmware.imx :&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SRC_URI = "${FSL_MIRROR}/firmware-imx-${PV}.bin;fsl-eula=true \&lt;BR /&gt;&amp;nbsp;https://source.codeaurora.org/external/imx/imx-firmware.git;branch=${SRCBRANCH};destsuffix=${S}/git "&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone give me the correct solution?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers, Glen&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 May 2020 22:16:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/firmware-imx-build-failure/m-p/1044530#M153813</guid>
      <dc:creator>glenfine</dc:creator>
      <dc:date>2020-05-19T22:16:06Z</dc:date>
    </item>
    <item>
      <title>Re: firmware-imx build failure</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/firmware-imx-build-failure/m-p/1044531#M153814</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;you can refer to my document&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-346089"&gt;unable to connect to git.freescale.com&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;let me remind, if you download the package I uploaded, and put them to the downloads, need to keep the firmware.imx, don't change it to "&lt;A class="" data-content-finding="Community" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fsource.codeaurora.org%2Fexternal%2Fimx%2Fimx-firmware.git%3Bbranch%3D%24" rel="nofollow" target="_blank"&gt;https://source.codeaurora.org/external/imx/imx-firmware.git&lt;/A&gt;", still keep the git.freescale.com&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 May 2020 04:35:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/firmware-imx-build-failure/m-p/1044531#M153814</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2020-05-20T04:35:26Z</dc:date>
    </item>
    <item>
      <title>Re: firmware-imx build failure</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/firmware-imx-build-failure/m-p/1202228#M166773</link>
      <description>&lt;P&gt;Hi, &lt;SPAN class=""&gt;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/39586" target="_self"&gt;joanxie&lt;/A&gt;,&amp;nbsp;I need to get the download package, please send it to me. shenhzdl@gmail.com&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Dec 2020 06:04:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/firmware-imx-build-failure/m-p/1202228#M166773</guid>
      <dc:creator>Payton</dc:creator>
      <dc:date>2020-12-21T06:04:35Z</dc:date>
    </item>
    <item>
      <title>Re: firmware-imx build failure</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/firmware-imx-build-failure/m-p/1390173#M184803</link>
      <description>&lt;P&gt;hi,@&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/39586" target="_self"&gt;&lt;SPAN class=""&gt;joanxie&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp; &amp;nbsp; I need&amp;nbsp;firmware-imx-1_5.4-r0 ,&lt;EM&gt;&lt;SPAN class=""&gt;&lt;A target="_blank"&gt;thank&lt;/A&gt; &lt;A target="_blank"&gt;you!&amp;nbsp;&amp;nbsp;&lt;/A&gt;&lt;A target="_blank"&gt;my&lt;/A&gt; &lt;A target="_blank"&gt;email is li2390707440@outlook.com&lt;/A&gt;&lt;/SPAN&gt;&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 21 Dec 2021 12:26:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/firmware-imx-build-failure/m-p/1390173#M184803</guid>
      <dc:creator>小李</dc:creator>
      <dc:date>2021-12-21T12:26:27Z</dc:date>
    </item>
    <item>
      <title>Re: firmware-imx build failure</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/firmware-imx-build-failure/m-p/1420038#M187536</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi,&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/39586" target="_self"&gt;joanxie&lt;/A&gt;,&amp;nbsp;I need to get the download package, please send it to me. zjksn88@126.com&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 26 Feb 2022 11:17:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/firmware-imx-build-failure/m-p/1420038#M187536</guid>
      <dc:creator>xinxin1</dc:creator>
      <dc:date>2022-02-26T11:17:37Z</dc:date>
    </item>
    <item>
      <title>Re: firmware-imx build failure</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/firmware-imx-build-failure/m-p/1515199#M194571</link>
      <description>&lt;P&gt;&lt;SPAN&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/39586"&gt;@joanxie&lt;/a&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Hi,&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/39586" target="_self"&gt;joanxie&lt;/A&gt;,&amp;nbsp;I need to get &lt;SPAN&gt;&amp;nbsp;firmware-imx-1_5.4-r0&lt;/SPAN&gt;&amp;nbsp;package, please send it to me. lzz93929@gmail.com&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 01 Sep 2022 04:02:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/firmware-imx-build-failure/m-p/1515199#M194571</guid>
      <dc:creator>lzz1</dc:creator>
      <dc:date>2022-09-01T04:02:42Z</dc:date>
    </item>
  </channel>
</rss>