<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx8m mini flash img error in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8m-mini-flash-img-error/m-p/1044432#M153797</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Tang Wei,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are using a custom board, you would need to make adjustments as mentioned on the following threads:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/519435"&gt;https://community.nxp.com/thread/519435&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/521347"&gt;https://community.nxp.com/thread/521347&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the first, it talks about how to setup the information of your board, and on the second it talks about a specific problem when having USB type C settings on uboot for your board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps to shed some light on what may be the issue.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Jun 2020 22:19:48 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2020-06-02T22:19:48Z</dc:date>
    <item>
      <title>imx8m mini flash img error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8m-mini-flash-img-error/m-p/1044431#M153796</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I develop a custom board with imx8m mini ,when we execute the command&lt;/P&gt;&lt;P&gt;"sudo ./uuu_imx_android_flash.sh -f imx8mm -u ddr4 ",&lt;/P&gt;&lt;P&gt;the result is failed .it stop at the result&lt;/P&gt;&lt;P&gt;"3:13 1/ 1 [=================100%=================] SDP: boot -f u-boot-imx8mm-ddr4-evk-uuu.imx "&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we doubt whether it is because of the ddr4.&lt;/P&gt;&lt;P&gt;I noticed that the reference board using 2*16bit DDR4 for memory interface for 32bit data, and we used 16 bit DDR4 for memory for 16 bit data.&lt;BR /&gt;I wonder whether it is the cause of our problem.&lt;BR /&gt;Maybe we need to modify some code or configuration, Could you please give us some tips?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jun 2020 07:15:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8m-mini-flash-img-error/m-p/1044431#M153796</guid>
      <dc:creator>1269813285</dc:creator>
      <dc:date>2020-06-02T07:15:04Z</dc:date>
    </item>
    <item>
      <title>Re: imx8m mini flash img error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8m-mini-flash-img-error/m-p/1044432#M153797</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Tang Wei,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are using a custom board, you would need to make adjustments as mentioned on the following threads:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/519435"&gt;https://community.nxp.com/thread/519435&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/521347"&gt;https://community.nxp.com/thread/521347&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the first, it talks about how to setup the information of your board, and on the second it talks about a specific problem when having USB type C settings on uboot for your board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps to shed some light on what may be the issue.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jun 2020 22:19:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8m-mini-flash-img-error/m-p/1044432#M153797</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2020-06-02T22:19:48Z</dc:date>
    </item>
  </channel>
</rss>