<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx8mq Dual Lane DisplayPort in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Dual-Lane-DisplayPort/m-p/1043150#M153616</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;I had checked the above thread regarding display port before and just&amp;nbsp; changed to the driver in 5.4.24_2.1.0 and firmware-imx-8.8.bin but that does not fix the link training in dual lane mode for me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note that it looks like&amp;nbsp; training finished clock recovery but fails in the EQ phase. Is there any other data i can provide to diagnose the problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Aug 2020 08:19:40 GMT</pubDate>
    <dc:creator>guido_gunther</dc:creator>
    <dc:date>2020-08-19T08:19:40Z</dc:date>
    <item>
      <title>imx8mq Dual Lane DisplayPort</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Dual-Lane-DisplayPort/m-p/1043148#M153614</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm working with the mhdp/dcss driver based off of NXPs BSP and am using the 8.7 firmware from&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-imx-8.7.bin" title="https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/"&gt;https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-imx-8.7.bin&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While 4-Lane DisplayPort configurations work, dual lane configurations fail the link training like (i've added some printk to the training code in cdns-mhdp-common.c):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp; 61.093206] cdns-mhdp-imx 32c00000.hdmi: [drm:cdns_mhdp_train_link [cdns_mhdp_drmcore]] Training status: 0x4&lt;BR /&gt;&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 61.148744] cdns-mhdp-imx 32c00000.hdmi: [drm:cdns_mhdp_train_link [cdns_mhdp_drmcore]] Training status: 0x20&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp; 61.541297] cdns-mhdp-imx 32c00000.hdmi: [drm:cdns_mhdp_train_link [cdns_mhdp_drmcore]] Training status: 0x0&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 61.551221] cdns-mhdp-imx 32c00000.hdmi: [drm:cdns_mhdp_train_link [cdns_mhdp_drmcore]] *ERROR* training failed: -110&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 61.561890] cdns-mhdp-imx 32c00000.hdmi: [drm:cdns_mhdp_train_link [cdns_mhdp_drmcore]] *ERROR* Failed to start training -110&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 61.573294] cdns-mhdp-imx 32c00000.hdmi: [drm:cdns_dp_mode_set [cdns_mhdp_drmcore]] *ERROR* Failed link train -110&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So the training can finish clock recovery but gives up with&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;EQ_PHASE_FAILED&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Are there any special settings required to switch to 2 lane mode. Can someone confirm this should work ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The reference manual does not give any details on how to configure two lane mode. I can see that the number of lanes is passed down to the phy and used in&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;cdns_mhdp_set_host_cap()&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I assume it should not affect the LANES_CONFIG register, right?&lt;/P&gt;&lt;P&gt;Can you please specify the details of correct PHY and HDMITX setup for two lane DP mode on the imx8mq?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Aug 2020 13:45:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Dual-Lane-DisplayPort/m-p/1043148#M153614</guid>
      <dc:creator>guido_gunther</dc:creator>
      <dc:date>2020-08-18T13:45:22Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mq Dual Lane DisplayPort</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Dual-Lane-DisplayPort/m-p/1043149#M153615</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Guido&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at similar issue on&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/message/1284068?commentID=1284068#comment-1284068" title="https://community.nxp.com/message/1284068?commentID=1284068#comment-1284068"&gt;https://community.nxp.com/message/1284068?commentID=1284068#comment-1284068&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;as for "8.7 firmware"&amp;nbsp; - (it is mentioned in Table 3. BSP and Multimedia standard packages&lt;/P&gt;&lt;P&gt;attached Release Notes) it was used in old linux releases and there are DP issues described in&lt;/P&gt;&lt;P&gt;Table 14. Known issues and workarounds for i.MX 8 Family SoC Release Notes&lt;/P&gt;&lt;P&gt;All documentation:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=In-Depth_Tab" title="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=In-Depth_Tab"&gt;Embedded Linux for i.MX Applications Processors | NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Recommended to use latest Linux 5.4.24_2.1.0&amp;nbsp; (firmware-imx-8.8.bin) where seems these were fixed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Aug 2020 01:44:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Dual-Lane-DisplayPort/m-p/1043149#M153615</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-08-19T01:44:37Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mq Dual Lane DisplayPort</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Dual-Lane-DisplayPort/m-p/1043150#M153616</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;I had checked the above thread regarding display port before and just&amp;nbsp; changed to the driver in 5.4.24_2.1.0 and firmware-imx-8.8.bin but that does not fix the link training in dual lane mode for me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note that it looks like&amp;nbsp; training finished clock recovery but fails in the EQ phase. Is there any other data i can provide to diagnose the problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Aug 2020 08:19:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Dual-Lane-DisplayPort/m-p/1043150#M153616</guid>
      <dc:creator>guido_gunther</dc:creator>
      <dc:date>2020-08-19T08:19:40Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mq Dual Lane DisplayPort</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Dual-Lane-DisplayPort/m-p/1043151#M153617</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Guido&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;could you try to test on NXP i.MX8MQ EVK board with NXP Linux from&lt;/P&gt;&lt;P&gt;source.codeaurora.org/external/imx/linux-imx&amp;nbsp; repository&lt;/P&gt;&lt;P&gt;imx8mq-evk-dp.dts&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mq-evk-dp.dts?h=imx_5.4.24_2.1.0" title="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mq-evk-dp.dts?h=imx_5.4.24_2.1.0"&gt;imx8mq-evk-dp.dts\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;All linux documentation:&lt;/P&gt;&lt;P&gt;&lt;A data-content-finding="Community" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdesign%2Fsoftware%2Fembedded-software%2Fi-mx-software%2Fembedded-linux-for-i-mx-applications-processors%3AIMXLINUX%3Ftab%3DIn-Depth_Tab" rel="nofollow" target="_blank"&gt;Embedded Linux for i.MX Applications Processors | NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Aug 2020 11:18:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Dual-Lane-DisplayPort/m-p/1043151#M153617</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-08-19T11:18:38Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mq Dual Lane DisplayPort</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Dual-Lane-DisplayPort/m-p/1043152#M153618</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;I can't test with the EVK since the one i have only drives HDMI so i have to use our board for that. The mhdp/dcss driver corresponds to this branch &lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/log/?h=imx_5.4.24_2.1.0" title="https://source.codeaurora.org/external/imx/linux-imx/log/?h=imx_5.4.24_2.1.0"&gt;linux-imx - i.MX Linux kernel&lt;/A&gt; and the DT bits look like what you linked to:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;```&lt;/P&gt;&lt;P&gt;&amp;amp;dcss {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; status = "okay";&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; port@0 {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; dcss_out: endpoint {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; remote-endpoint = &amp;lt;&amp;amp;hdmi_in&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; };&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; };&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;amp;hdmi {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; compatible = "cdn,imx8mq-dp";&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; lane-mapping = &amp;lt;0xc6&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; status = "okay";&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; port@1 {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; hdmi_in: endpoint {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; remote-endpoint = &amp;lt;&amp;amp;dcss_out&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; };&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; };&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;```&lt;/P&gt;&lt;P&gt;As i wrote above 4 lane DP works so i suspect either a firmware or driver issue.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Aug 2020 08:39:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Dual-Lane-DisplayPort/m-p/1043152#M153618</guid>
      <dc:creator>guido_gunther</dc:creator>
      <dc:date>2020-08-20T08:39:10Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mq Dual Lane DisplayPort</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Dual-Lane-DisplayPort/m-p/1043153#M153619</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Hi Guido&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;dual lane eDP (LTK156D30A004) was verified by boundary devices&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;A class="link-titled" href="https://boundarydevices.com/edp-display-support-on-nitrogen8m/" title="https://boundarydevices.com/edp-display-support-on-nitrogen8m/"&gt;https://boundarydevices.com/edp-display-support-on-nitrogen8m/&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;A class="link-titled" href="https://github.com/boundarydevices/linux-imx6/blob/boundary-imx_4.14.x_2.0.0_ga/arch/arm64/boot/dts/freescale/imx8mq-nitrogen8m-edp.dts" title="https://github.com/boundarydevices/linux-imx6/blob/boundary-imx_4.14.x_2.0.0_ga/arch/arm64/boot/dts/freescale/imx8mq-nitrogen8m-edp.dts"&gt;linux-imx6/imx8mq-nitrogen8m-edp.dts at boundary-imx_4.14.x_2.0.0_ga · boundarydevices/linux-imx6 · GitHub&lt;/A&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Seems you used only driver and firmware from&amp;nbsp;source.codeaurora.org/external/imx/linux-imx&amp;nbsp; repository,&lt;/P&gt;&lt;P&gt;not whole linux image, right ? For such kind of development may be suggested to proceed with help of&lt;/P&gt;&lt;P&gt;NXP Professional Services:&lt;BR /&gt;&lt;A class="link-titled" href="https://www.nxp.com/support/support/nxp-engineering-services/professional-engineering-services:PROFESSIONAL-ENGINEERING-SERVICES" title="https://www.nxp.com/support/support/nxp-engineering-services/professional-engineering-services:PROFESSIONAL-ENGINEERING-SERVICES"&gt;Professional Engineering Services | NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Aug 2020 10:34:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Dual-Lane-DisplayPort/m-p/1043153#M153619</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-08-20T10:34:09Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mq Dual Lane DisplayPort</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Dual-Lane-DisplayPort/m-p/1658602#M206665</link>
      <description>&lt;P&gt;Hey &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/104289"&gt;@guido_gunther&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Did you resolve your issue with the two-lane link training? Auxiliary communication works, we receive edid, so the dp firmware is running and included in the uuu-programming script. The lane mapping is correct (c6), and link training says it succeeds. However, transmission does not seem to occur as we get no picture.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sam&lt;/P&gt;</description>
      <pubDate>Thu, 08 Jun 2023 18:49:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Dual-Lane-DisplayPort/m-p/1658602#M206665</guid>
      <dc:creator>smusserRosen</dc:creator>
      <dc:date>2023-06-08T18:49:23Z</dc:date>
    </item>
  </channel>
</rss>