<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MIPI DSI HFP stability in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-HFP-stability/m-p/1042346#M153535</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have trying to connect a 800x480 RGB TFT to an imx8m mini using a bridge chip.&amp;nbsp; I have tried 2 different bridge vendors ic's and both show the same issue.&amp;nbsp; The horizontal front porch is not consistent from line to line.&amp;nbsp; I am seeing a variation of up to 7x pixel clocks per line.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the attachment I am triggering on the rising edge of data enable.&amp;nbsp; The horizontal sync is stable, and you can see this issue in the falling edge of data enable for the previous frame.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have&amp;nbsp;tried all MIPI DSI flag combinations in the linux driver without success.&amp;nbsp; I&amp;nbsp;am currently using Video mode without burst and MIPI_DSI_MODE_VIDEO_SYNC_PULSE.&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;Adjusting these&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;flags change the jitter, but not remove it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there some setting that I'm missing?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 14 Jun 2020 19:10:42 GMT</pubDate>
    <dc:creator>mark_vogt1</dc:creator>
    <dc:date>2020-06-14T19:10:42Z</dc:date>
    <item>
      <title>MIPI DSI HFP stability</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-HFP-stability/m-p/1042346#M153535</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have trying to connect a 800x480 RGB TFT to an imx8m mini using a bridge chip.&amp;nbsp; I have tried 2 different bridge vendors ic's and both show the same issue.&amp;nbsp; The horizontal front porch is not consistent from line to line.&amp;nbsp; I am seeing a variation of up to 7x pixel clocks per line.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the attachment I am triggering on the rising edge of data enable.&amp;nbsp; The horizontal sync is stable, and you can see this issue in the falling edge of data enable for the previous frame.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have&amp;nbsp;tried all MIPI DSI flag combinations in the linux driver without success.&amp;nbsp; I&amp;nbsp;am currently using Video mode without burst and MIPI_DSI_MODE_VIDEO_SYNC_PULSE.&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;Adjusting these&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;flags change the jitter, but not remove it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there some setting that I'm missing?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 14 Jun 2020 19:10:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-HFP-stability/m-p/1042346#M153535</guid>
      <dc:creator>mark_vogt1</dc:creator>
      <dc:date>2020-06-14T19:10:42Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI DSI HFP stability</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-HFP-stability/m-p/1042347#M153536</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;such configuration seems is working fine on DART-MX8MMini board:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/varigit/linux-imx/blob/imx_4.19.35_1.1.0_var01/arch/arm64/boot/dts/freescale/fsl-imx8mm-var-dart.dts" title="https://github.com/varigit/linux-imx/blob/imx_4.19.35_1.1.0_var01/arch/arm64/boot/dts/freescale/fsl-imx8mm-var-dart.dts"&gt;linux-imx/fsl-imx8mm-var-dart.dts at imx_4.19.35_1.1.0_var01 · varigit/linux-imx · GitHub&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.variscite.com/product/system-on-module-som/cortex-a53-krait/dart-mx8m-mini-nxp-i-mx8m-mini/" title="https://www.variscite.com/product/system-on-module-som/cortex-a53-krait/dart-mx8m-mini-nxp-i-mx8m-mini/"&gt;DART-MX8M-MINI : NXP i.MX8M Mini ARM SoM (System on Module) | Variscite&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;other bridge example&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/TechNexion-customization/linux-imx-tn/blob/tn-imx_4.14.98_2.0.0_ga-wip-mipi2lvds/arch/arm64/boot/dts/freescale/imx8mm-pico-pi-sn65dsi84-hj070na.dts" title="https://github.com/TechNexion-customization/linux-imx-tn/blob/tn-imx_4.14.98_2.0.0_ga-wip-mipi2lvds/arch/arm64/boot/dts/freescale/imx8mm-pico-pi-sn65dsi84-hj070na.dts"&gt;linux-imx-tn/imx8mm-pico-pi-sn65dsi84-hj070na.dts at tn-imx_4.14.98_2.0.0_ga-wip-mipi2lvds · TechNexion-customization/li…&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.technexion.com/products/system-on-modules/pico/pico-compute-modules/detail/PICO-IMX8M-MINI" title="https://www.technexion.com/products/system-on-modules/pico/pico-compute-modules/detail/PICO-IMX8M-MINI"&gt;https://www.technexion.com/products/system-on-modules/pico/pico-compute-modules/detail/PICO-IMX8M-MINI&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jun 2020 00:55:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-DSI-HFP-stability/m-p/1042347#M153536</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-06-17T00:55:54Z</dc:date>
    </item>
  </channel>
</rss>