<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX8MQ PCIe Tx and Rx Swapping</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MQ-PCIe-Tx-and-Rx-Swapping/m-p/1040614#M153292</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi NXP Team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are working for communication between two i.MX8MQ processors using the PCIe link. For the same, we are planning to do below connections from the hardware.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/108731i13AE0A51A5ED3FCE/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;To support the above connections we are required to swap the Tx and Rx lines of one port of PCIe.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the i.MX8MQ Processor is there any configuration available where we can swap the TX and RX signals on the pins? (Similar to what is being supported for the UART Tx/Rx swapping?)&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 Jun 2020 13:04:04 GMT</pubDate>
    <dc:creator>harshitshah</dc:creator>
    <dc:date>2020-06-01T13:04:04Z</dc:date>
    <item>
      <title>i.MX8MQ PCIe Tx and Rx Swapping</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MQ-PCIe-Tx-and-Rx-Swapping/m-p/1040614#M153292</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi NXP Team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are working for communication between two i.MX8MQ processors using the PCIe link. For the same, we are planning to do below connections from the hardware.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/108731i13AE0A51A5ED3FCE/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;To support the above connections we are required to swap the Tx and Rx lines of one port of PCIe.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the i.MX8MQ Processor is there any configuration available where we can swap the TX and RX signals on the pins? (Similar to what is being supported for the UART Tx/Rx swapping?)&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Jun 2020 13:04:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MQ-PCIe-Tx-and-Rx-Swapping/m-p/1040614#M153292</guid>
      <dc:creator>harshitshah</dc:creator>
      <dc:date>2020-06-01T13:04:04Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8MQ PCIe Tx and Rx Swapping</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MQ-PCIe-Tx-and-Rx-Swapping/m-p/1040615#M153293</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Harshit&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;In the i.MX8MQ Processor is there any configuration available where we can swap the TX and RX signals on the pins?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am afraid it is not supported in hardware, sorry.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Jun 2020 23:26:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MQ-PCIe-Tx-and-Rx-Swapping/m-p/1040615#M153293</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-06-01T23:26:33Z</dc:date>
    </item>
  </channel>
</rss>