<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX6Q Linux MIPI LCD + HDMI</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-Linux-MIPI-LCD-HDMI/m-p/1040520#M153291</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;BSP L3.14.52 is too old. Please try the newer version of BSP. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 17 Apr 2020 18:46:29 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2020-04-17T18:46:29Z</dc:date>
    <item>
      <title>IMX6Q Linux MIPI LCD + HDMI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-Linux-MIPI-LCD-HDMI/m-p/1040519#M153290</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i want to use mipi LCD + HDMI&amp;nbsp;&lt;/P&gt;&lt;P&gt;mipi LCD :1024x600&amp;nbsp;&lt;/P&gt;&lt;P&gt;HDMI 1920x1080&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;device tree:&amp;nbsp;&lt;/P&gt;&lt;P&gt;mxcfb1: fb@0 {&lt;BR /&gt; compatible = "fsl,mxc_sdc_fb";&lt;BR /&gt; disp_dev = "mipi_dsi";&lt;BR /&gt; interface_pix_fmt = "RGB24"; &lt;BR /&gt; mode_str = "ST7701S-WVGA";&lt;BR /&gt; default_bpp = &amp;lt;24&amp;gt;;&lt;BR /&gt; int_clk = &amp;lt;0&amp;gt;;&lt;BR /&gt; late_init = &amp;lt;0&amp;gt;;&lt;BR /&gt; status = "disabled";&lt;BR /&gt; };&lt;/P&gt;&lt;P&gt;mxcfb2: fb@1 {&lt;BR /&gt; compatible = "fsl,mxc_sdc_fb";&lt;BR /&gt; disp_dev = "hdmi";&lt;BR /&gt; interface_pix_fmt = "RGB24";&lt;BR /&gt; mode_str ="1920x1080M@60";&lt;BR /&gt; default_bpp = &amp;lt;24&amp;gt;;&lt;BR /&gt; int_clk = &amp;lt;0&amp;gt;;&lt;BR /&gt; late_init = &amp;lt;0&amp;gt;;&lt;BR /&gt; status = "disabled";&lt;BR /&gt; };&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;amp;hdmi_core {&lt;BR /&gt; ipu_id = &amp;lt;0&amp;gt;;&lt;BR /&gt; disp_id = &amp;lt;0&amp;gt;;&lt;BR /&gt; status = "okay";&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&amp;amp;mipi_csi {&lt;BR /&gt; status = "okay";&lt;BR /&gt; ipu_id = &amp;lt;0&amp;gt;;&lt;BR /&gt; csi_id = &amp;lt;1&amp;gt;;&lt;BR /&gt; v_channel = &amp;lt;0&amp;gt;;&lt;BR /&gt; lanes = &amp;lt;2&amp;gt;;&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;i add&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;video=mxcfb0:dev=mipi_dsi,ST7701S-WVGA,if=RGB24 video=mxcfb1:dev=hdmi,1920x1080M@60,bpp=32,if=RGB24&lt;/P&gt;&lt;P&gt;into uboot env&lt;/P&gt;&lt;P&gt;------------&lt;/P&gt;&lt;P&gt;the result is MIPI can display but HDMI can't.&lt;/P&gt;&lt;P&gt;&amp;nbsp;cat /sys/class/graphics/fb0/mode&amp;nbsp; ==&amp;gt;&amp;gt; U:1024x600p-60&lt;BR /&gt;cat /sys/class/graphics/fb2/mode&amp;nbsp; &amp;nbsp;==&amp;gt;&amp;gt;&amp;nbsp; U:1920x1080p-60&lt;/P&gt;&lt;P&gt;i use kernel version is : 3.14.52&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone encountered such&amp;nbsp; problem?&amp;nbsp;&lt;/P&gt;&lt;P&gt;it was&amp;nbsp;&lt;SPAN&gt;ipu_id&amp;nbsp; problem ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Hope someone can help me .&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Apr 2020 02:04:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-Linux-MIPI-LCD-HDMI/m-p/1040519#M153290</guid>
      <dc:creator>chenjt</dc:creator>
      <dc:date>2020-04-16T02:04:33Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q Linux MIPI LCD + HDMI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-Linux-MIPI-LCD-HDMI/m-p/1040520#M153291</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;BSP L3.14.52 is too old. Please try the newer version of BSP. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Apr 2020 18:46:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-Linux-MIPI-LCD-HDMI/m-p/1040520#M153291</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2020-04-17T18:46:29Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q Linux MIPI LCD + HDMI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-Linux-MIPI-LCD-HDMI/m-p/1313476#M177488</link>
      <description>&lt;P&gt;I use kernel version is : 4.1.15.This version also can not realize Mipi and HDMI displayed simultaneously by modifying the device tree.&lt;BR /&gt;was ipu_id and disp_id 's problem ?&lt;BR /&gt;Is there anything else that needs to be modified?&lt;/P&gt;</description>
      <pubDate>Tue, 27 Jul 2021 01:34:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-Linux-MIPI-LCD-HDMI/m-p/1313476#M177488</guid>
      <dc:creator>wjy</dc:creator>
      <dc:date>2021-07-27T01:34:17Z</dc:date>
    </item>
  </channel>
</rss>