<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: IMX8MM: RPMsg between A core and M4</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-RPMsg-between-A-core-and-M4/m-p/1038161#M152987</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For the tests you can play with RPMsg test program included into unit-test of our Linux.&lt;BR /&gt;Please refer to chapter 2.8.5 "Running i.MX RPMsg Test Programs" of 2.8.5 of i.MX Linux Reference Manual included to this bundle:&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/supporting-information/fsl-yocto-L4.9.123_2.3.0_mx8mm.zip" target="test_blank"&gt;https://www.nxp.com/docs/en/supporting-information/fsl-yocto-L4.9.123_2.3.0_mx8mm.zip&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Mar 2020 03:58:42 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2020-03-04T03:58:42Z</dc:date>
    <item>
      <title>IMX8MM: RPMsg between A core and M4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-RPMsg-between-A-core-and-M4/m-p/1038160#M152986</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;I am using a IMX8MM in my project and running android 9 on this. In the project, we plan to have some GPIO function working on M4, and there will be some communications between A core and M4.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;I have download the RPMsg-lite sample for reference, but I still have no idea what's the mechanism for avoiding resources overlap on both A core and M4. Is the multicore manager responsible for the resource allocation and monitoring between multiple core? If it is, where can I find the sample code? (I only found RPMsg-lite under the multicore example folder)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Mar 2020 08:12:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-RPMsg-between-A-core-and-M4/m-p/1038160#M152986</guid>
      <dc:creator>roger_chang</dc:creator>
      <dc:date>2020-03-03T08:12:40Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MM: RPMsg between A core and M4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-RPMsg-between-A-core-and-M4/m-p/1038161#M152987</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For the tests you can play with RPMsg test program included into unit-test of our Linux.&lt;BR /&gt;Please refer to chapter 2.8.5 "Running i.MX RPMsg Test Programs" of 2.8.5 of i.MX Linux Reference Manual included to this bundle:&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/supporting-information/fsl-yocto-L4.9.123_2.3.0_mx8mm.zip" target="test_blank"&gt;https://www.nxp.com/docs/en/supporting-information/fsl-yocto-L4.9.123_2.3.0_mx8mm.zip&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Mar 2020 03:58:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MM-RPMsg-between-A-core-and-M4/m-p/1038161#M152987</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2020-03-04T03:58:42Z</dc:date>
    </item>
  </channel>
</rss>