<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: UBIFS mount fails in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/UBIFS-mount-fails/m-p/1036798#M152868</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Weidong,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ours is MLC NAND Flash. In that case is not posbbile to boot the kernel from the rootfs ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Deepanraj.A&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Mar 2020 07:37:28 GMT</pubDate>
    <dc:creator>deepanrajanbara</dc:creator>
    <dc:date>2020-03-03T07:37:28Z</dc:date>
    <item>
      <title>UBIFS mount fails</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UBIFS-mount-fails/m-p/1036796#M152866</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually i have implemented imx6ull kernel version 4.14.98 for our custom board. In which NAND is the Boot media.&lt;/P&gt;&lt;P&gt;I wanted to keep my kernel and dtb in my UBIFS instead of flashing them to a separate raw partition. Since we wanted to do OTA for the device. When booting the Uboot, i am getting a error. Please help us debug the error. We are flashing the .ubimg file after flashing the uboot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ubi0: detaching mtd1&lt;BR /&gt;ubi0: mtd1 is detached&lt;BR /&gt;ubi0: attaching mtd1&lt;BR /&gt;ubi0: scanning is finished&lt;BR /&gt;ubi0: attached mtd1 (name "mtd=1", size 496 MiB)&lt;BR /&gt;ubi0: PEB size: 262144 bytes (256 KiB), LEB size: 253952 bytes&lt;BR /&gt;ubi0: min./max. I/O unit sizes: 4096/4096, sub-page size 4096&lt;BR /&gt;ubi0: VID header offset: 4096 (aligned 4096), data offset: 8192&lt;BR /&gt;ubi0: good PEBs: 1976, bad PEBs: 8, corrupted PEBs: 0&lt;BR /&gt;ubi0: user volume: 5, internal volumes: 1, max. volumes count: 128&lt;BR /&gt;ubi0: max/mean erase counter: 2/0, WL threshold: 4096, image sequence number: 618423331&lt;BR /&gt;ubi0: available PEBs: 2, total reserved PEBs: 1974, PEBs reserved for bad PEB handling: 32&lt;BR /&gt;UBIFS assert failed in ubifs_change_lp at 540&lt;BR /&gt;UBIFS assert failed in ubifs_release_lprops at 278&lt;BR /&gt;UBIFS assert failed in ubifs_change_lp at 540&lt;BR /&gt;UBIFS assert failed in ubifs_release_lprops at 278&lt;BR /&gt;UBIFS error (ubi0:0 pid 0): ubifs_read_node: bad node type (255 but expected 9)&lt;BR /&gt;UBIFS error (ubi0:0 pid 0): ubifs_read_node: bad node at LEB 125:249352, LEB mapping status 0&lt;BR /&gt;Not a node, first 24 bytes:UBIFS error (ubi0:0 pid 0): ubifs_iget: failed to read inode 1, error -22&lt;BR /&gt;Error reading superblock on volume 'ubi0:rootfsa' errno=-22!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Deepanraj&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Mar 2020 12:17:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UBIFS-mount-fails/m-p/1036796#M152866</guid>
      <dc:creator>deepanrajanbara</dc:creator>
      <dc:date>2020-03-02T12:17:57Z</dc:date>
    </item>
    <item>
      <title>Re: UBIFS mount fails</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UBIFS-mount-fails/m-p/1036797#M152867</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Deepanraj,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Starting from 4.14.98 bsp or later, ubifs doesn't support MLC NAND Flash, but SLC is no problem. So please check your NAND Flash, please!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope the information is helpful for you!&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Mar 2020 01:43:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UBIFS-mount-fails/m-p/1036797#M152867</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2020-03-03T01:43:35Z</dc:date>
    </item>
    <item>
      <title>Re: UBIFS mount fails</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UBIFS-mount-fails/m-p/1036798#M152868</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Weidong,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ours is MLC NAND Flash. In that case is not posbbile to boot the kernel from the rootfs ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Deepanraj.A&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Mar 2020 07:37:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UBIFS-mount-fails/m-p/1036798#M152868</guid>
      <dc:creator>deepanrajanbara</dc:creator>
      <dc:date>2020-03-03T07:37:28Z</dc:date>
    </item>
  </channel>
</rss>