<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックPMIC selection for i.MX6ULL</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-selection-for-i-MX6ULL/m-p/1036632#M152828</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on a new design using the i.MX6ULL and intending to use the PF3001 for the PMIC as I don't need the additional features in the PF3000.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone please confirm that the PF3001 is compatible with the i.MX6ULL? The data sheet for the PF3001 only confirms that the i.MX6UL is supported, and doesn't mention the i.MX6ULL.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ben&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 02 Mar 2020 13:38:02 GMT</pubDate>
    <dc:creator>ben_jones</dc:creator>
    <dc:date>2020-03-02T13:38:02Z</dc:date>
    <item>
      <title>PMIC selection for i.MX6ULL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-selection-for-i-MX6ULL/m-p/1036632#M152828</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on a new design using the i.MX6ULL and intending to use the PF3001 for the PMIC as I don't need the additional features in the PF3000.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone please confirm that the PF3001 is compatible with the i.MX6ULL? The data sheet for the PF3001 only confirms that the i.MX6UL is supported, and doesn't mention the i.MX6ULL.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ben&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Mar 2020 13:38:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PMIC-selection-for-i-MX6ULL/m-p/1036632#M152828</guid>
      <dc:creator>ben_jones</dc:creator>
      <dc:date>2020-03-02T13:38:02Z</dc:date>
    </item>
    <item>
      <title>Re: PMIC selection for i.MX6ULL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-selection-for-i-MX6ULL/m-p/1036633#M152829</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ben,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can see the i.MX 6ULL as a derivation from i.MX 6UL. I would suggest you to&amp;nbsp;check the migration guide from i.MX 6UL to i.MX 6ULL:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN5350.pdf"&gt;Migrating from i.MX 6UL to i.MX 6ULL&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can use the PF3001 datasheet to help you selecting a PMIC for your processor (&lt;EM&gt;Table 1. Orderable part variations&lt;/EM&gt;):&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/data-sheet/PF3001.pdf"&gt;PF3001 datasheet&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope the information was helpful!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Mar 2020 17:37:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PMIC-selection-for-i-MX6ULL/m-p/1036633#M152829</guid>
      <dc:creator>nxf54947</dc:creator>
      <dc:date>2020-03-03T17:37:36Z</dc:date>
    </item>
  </channel>
</rss>